<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックgPTP example not running on S32g399</title>
    <link>https://community.nxp.com/t5/S32G/gPTP-example-not-running-on-S32g399/m-p/2305076#M15928</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I have built gPTP_S32G_1.1.0 with:&lt;BR /&gt;&lt;BR /&gt;S32 RTD version SW32G_RTD_4.4_5.0.0_QLP03_D2505 S32G&lt;BR /&gt;PFE MCAL driver PFE_DRV_MCAL_S32G_RTM_1_6_0_D2505&lt;BR /&gt;S32G PFE Firmware PFE-FW_S32G_1.11.0&lt;BR /&gt;&lt;BR /&gt;I ran make generate and then make which created elf in /output_AED-E_RDB3&lt;BR /&gt;I have loaded this elf as a project from executable in S32 DS which created a DEBUG_RAM configuration.&lt;BR /&gt;&lt;BR /&gt;I have noticed that the application does not go beyond&amp;nbsp; and&amp;nbsp;Mcu_GetPllStatus() call in&amp;nbsp;DriversInitialization(). Upon pausing the execution I found out that the execution is stuck on PLL lock in&amp;nbsp;Clock_Ip_CompletePlldigRdivMfiMfnSdmenSsscgbypSpreadctlStepnoStepsize()&lt;BR /&gt;&lt;BR /&gt;I have made no changes of my own other than fixing the makefile to pick correct paths. It built without errors and I just flashed it with S32 Debugger.&lt;BR /&gt;&lt;BR /&gt;Please let me know how to fix this and how to validate gPTP application in AED-E mode. Thanks,&lt;/P&gt;</description>
    <pubDate>Tue, 03 Feb 2026 08:30:59 GMT</pubDate>
    <dc:creator>rizwan_at_disruptdotcom</dc:creator>
    <dc:date>2026-02-03T08:30:59Z</dc:date>
    <item>
      <title>gPTP example not running on S32g399</title>
      <link>https://community.nxp.com/t5/S32G/gPTP-example-not-running-on-S32g399/m-p/2305076#M15928</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I have built gPTP_S32G_1.1.0 with:&lt;BR /&gt;&lt;BR /&gt;S32 RTD version SW32G_RTD_4.4_5.0.0_QLP03_D2505 S32G&lt;BR /&gt;PFE MCAL driver PFE_DRV_MCAL_S32G_RTM_1_6_0_D2505&lt;BR /&gt;S32G PFE Firmware PFE-FW_S32G_1.11.0&lt;BR /&gt;&lt;BR /&gt;I ran make generate and then make which created elf in /output_AED-E_RDB3&lt;BR /&gt;I have loaded this elf as a project from executable in S32 DS which created a DEBUG_RAM configuration.&lt;BR /&gt;&lt;BR /&gt;I have noticed that the application does not go beyond&amp;nbsp; and&amp;nbsp;Mcu_GetPllStatus() call in&amp;nbsp;DriversInitialization(). Upon pausing the execution I found out that the execution is stuck on PLL lock in&amp;nbsp;Clock_Ip_CompletePlldigRdivMfiMfnSdmenSsscgbypSpreadctlStepnoStepsize()&lt;BR /&gt;&lt;BR /&gt;I have made no changes of my own other than fixing the makefile to pick correct paths. It built without errors and I just flashed it with S32 Debugger.&lt;BR /&gt;&lt;BR /&gt;Please let me know how to fix this and how to validate gPTP application in AED-E mode. Thanks,&lt;/P&gt;</description>
      <pubDate>Tue, 03 Feb 2026 08:30:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/gPTP-example-not-running-on-S32g399/m-p/2305076#M15928</guid>
      <dc:creator>rizwan_at_disruptdotcom</dc:creator>
      <dc:date>2026-02-03T08:30:59Z</dc:date>
    </item>
    <item>
      <title>Re: gPTP example not running on S32g399</title>
      <link>https://community.nxp.com/t5/S32G/gPTP-example-not-running-on-S32g399/m-p/2305689#M15938</link>
      <description>&lt;P&gt;Hi,&lt;SPAN&gt;rizwan_at_disru&lt;/SPAN&gt;&lt;WBR /&gt;&lt;SPAN&gt;ptdotcom&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Do you use the RDB3 board or customer board?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Wed, 04 Feb 2026 04:13:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/gPTP-example-not-running-on-S32g399/m-p/2305689#M15938</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2026-02-04T04:13:25Z</dc:date>
    </item>
    <item>
      <title>Re: gPTP example not running on S32g399</title>
      <link>https://community.nxp.com/t5/S32G/gPTP-example-not-running-on-S32g399/m-p/2305731#M15939</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/236188"&gt;@Joey_z&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using a GLDBOX3:&amp;nbsp;&lt;A href="https://www.nxp.com/part/S32G-VNP-GLDBOX3" target="_blank"&gt;https://www.nxp.com/part/S32G-VNP-GLDBOX3&lt;/A&gt;&lt;/P&gt;&lt;P&gt;If there are changes required to get this application run on this board then please describe those changes that I can try. Alternatively if there is an application note to adapt the gPTP application for this board, that should also work.&lt;BR /&gt;&lt;BR /&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Wed, 04 Feb 2026 06:17:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/gPTP-example-not-running-on-S32g399/m-p/2305731#M15939</guid>
      <dc:creator>rizwan_at_disruptdotcom</dc:creator>
      <dc:date>2026-02-04T06:17:43Z</dc:date>
    </item>
    <item>
      <title>Re: gPTP example not running on S32g399</title>
      <link>https://community.nxp.com/t5/S32G/gPTP-example-not-running-on-S32g399/m-p/2312839#M15952</link>
      <description>&lt;P&gt;hi,rizwan_at_disruptdotcom&lt;/P&gt;
&lt;P&gt;Could you try to use IVT Image or the .cmm file for your testing?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Thu, 05 Feb 2026 10:32:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/gPTP-example-not-running-on-S32g399/m-p/2312839#M15952</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2026-02-05T10:32:48Z</dc:date>
    </item>
    <item>
      <title>Re: gPTP example not running on S32g399</title>
      <link>https://community.nxp.com/t5/S32G/gPTP-example-not-running-on-S32g399/m-p/2312933#M15953</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/236188"&gt;@Joey_z&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We don't have a lauterbach debugger and only use the S32 debug probe, which works fine with our other applications on this board. I notice that the cmm is clearing sram sectors, if this is the issue then can you please let me know how to do the same with s32 debug probe?&lt;BR /&gt;&lt;BR /&gt;The example does not create an IVT, but and elf that we are directly trying to flash using DEBUG_RAM configuration.&lt;BR /&gt;&lt;BR /&gt;Rizwan&lt;/P&gt;</description>
      <pubDate>Thu, 05 Feb 2026 12:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/gPTP-example-not-running-on-S32g399/m-p/2312933#M15953</guid>
      <dc:creator>rizwan_at_disruptdotcom</dc:creator>
      <dc:date>2026-02-05T12:15:58Z</dc:date>
    </item>
    <item>
      <title>Re: gPTP example not running on S32g399</title>
      <link>https://community.nxp.com/t5/S32G/gPTP-example-not-running-on-S32g399/m-p/2313466#M15966</link>
      <description>&lt;P&gt;hi，&lt;SPAN&gt;rizwan_at_disru&lt;/SPAN&gt;&lt;WBR /&gt;&lt;SPAN&gt;ptdotcom&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thank you for your reply.&lt;/P&gt;
&lt;P&gt;How do you generate the code and build your project? Do you have any modify about the application configuration?&lt;/P&gt;
&lt;P&gt;Could you send your .elf file to me thought the link of &lt;A href="https://support.nxp.com?" target="_blank"&gt;https://support.nxp.com?&lt;/A&gt;&amp;nbsp;I will help you to check it.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Fri, 06 Feb 2026 07:45:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/gPTP-example-not-running-on-S32g399/m-p/2313466#M15966</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2026-02-06T07:45:23Z</dc:date>
    </item>
    <item>
      <title>Re: gPTP example not running on S32g399</title>
      <link>https://community.nxp.com/t5/S32G/gPTP-example-not-running-on-S32g399/m-p/2313583#M15968</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/236188"&gt;@Joey_z&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did not make any changes to the application, only updated the makefile to enable build on my machine.&lt;/P&gt;&lt;P&gt;I have uploaded the EBT folder zip to drive. Please access here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://drive.google.com/file/d/1_3vj19gXmwHmqs20aAPOWAjENRCYusfg/view?usp=sharing" target="_blank"&gt;https://drive.google.com/file/d/1_3vj19gXmwHmqs20aAPOWAjENRCYusfg/view?usp=sharing&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 06 Feb 2026 09:29:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/gPTP-example-not-running-on-S32g399/m-p/2313583#M15968</guid>
      <dc:creator>rizwan_at_disruptdotcom</dc:creator>
      <dc:date>2026-02-06T09:29:17Z</dc:date>
    </item>
    <item>
      <title>Re: gPTP example not running on S32g399</title>
      <link>https://community.nxp.com/t5/S32G/gPTP-example-not-running-on-S32g399/m-p/2313609#M15969</link>
      <description>I have also opened a support case: 00959194</description>
      <pubDate>Fri, 06 Feb 2026 09:41:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/gPTP-example-not-running-on-S32g399/m-p/2313609#M15969</guid>
      <dc:creator>rizwan_at_disruptdotcom</dc:creator>
      <dc:date>2026-02-06T09:41:36Z</dc:date>
    </item>
  </channel>
</rss>