<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32G-VNP-RDB2 LIGHT UP RGB LED in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-LIGHT-UP-RGB-LED/m-p/2304383#M15921</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/258283"&gt;@a_tosetto&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your reply.&lt;/P&gt;
&lt;P&gt;1. From NXP's perspective, both debugger could be used on RDB2, there is standalone IDE for Lauterbach, while the S32 debug probe is used with S32DS.&lt;/P&gt;
&lt;P&gt;2. From personal experience, for Industry/AUTOSAR development, which is especially working with EB/Vector, etc. The lauterbach is usually used and supported. While only working with S32DS for development, the S32 debug probe could also be used for debugging purpose&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
    <pubDate>Mon, 02 Feb 2026 04:04:47 GMT</pubDate>
    <dc:creator>chenyin_h</dc:creator>
    <dc:date>2026-02-02T04:04:47Z</dc:date>
    <item>
      <title>S32G-VNP-RDB2 LIGHT UP RGB LED</title>
      <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-LIGHT-UP-RGB-LED/m-p/2302885#M15914</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Hi to all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm new on this kind of applications, so I ve to ask help!&lt;/P&gt;&lt;P&gt;I'm following the user guide&amp;nbsp;S32G-VNP-RDB2 SOFTWARE ENABLEMENT GUIDE to create the RBG LED example. I 'm checked all the steps up to page 23. Checked also&amp;nbsp; (more the once) the switches on the board, but i insert the card, powerup&amp;nbsp; the board and the RBG led remains blue.&lt;/P&gt;&lt;P&gt;Previously I laoded the linux OS from the SD card provided by NXP and i can see the system boot up normally.&lt;/P&gt;&lt;P&gt;What I'm doing wrong? There is a way to debug the application? I do not have the debug probe, should I ve to buy it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Andrea&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jan 2026 10:11:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-LIGHT-UP-RGB-LED/m-p/2302885#M15914</guid>
      <dc:creator>a_tosetto</dc:creator>
      <dc:date>2026-01-29T10:11:15Z</dc:date>
    </item>
    <item>
      <title>Re: S32G-VNP-RDB2 LIGHT UP RGB LED</title>
      <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-LIGHT-UP-RGB-LED/m-p/2303343#M15915</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/258283"&gt;@a_tosetto&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;For M core related development and debugging on S32G2, we suggest using a debugger for the similar issue faced, currently, the Lauterbach is commonly used for S32G related development, besides, the S32 debug probe could also be used.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jan 2026 03:11:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-LIGHT-UP-RGB-LED/m-p/2303343#M15915</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2026-01-30T03:11:53Z</dc:date>
    </item>
    <item>
      <title>Re: S32G-VNP-RDB2 LIGHT UP RGB LED</title>
      <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-LIGHT-UP-RGB-LED/m-p/2303699#M15919</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;thank you for the feedback, from a not skilled user like me what is better, Lautebach or S32 Debug probe?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Andrea&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jan 2026 10:57:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-LIGHT-UP-RGB-LED/m-p/2303699#M15919</guid>
      <dc:creator>a_tosetto</dc:creator>
      <dc:date>2026-01-30T10:57:58Z</dc:date>
    </item>
    <item>
      <title>Re: S32G-VNP-RDB2 LIGHT UP RGB LED</title>
      <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-LIGHT-UP-RGB-LED/m-p/2304383#M15921</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/258283"&gt;@a_tosetto&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your reply.&lt;/P&gt;
&lt;P&gt;1. From NXP's perspective, both debugger could be used on RDB2, there is standalone IDE for Lauterbach, while the S32 debug probe is used with S32DS.&lt;/P&gt;
&lt;P&gt;2. From personal experience, for Industry/AUTOSAR development, which is especially working with EB/Vector, etc. The lauterbach is usually used and supported. While only working with S32DS for development, the S32 debug probe could also be used for debugging purpose&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Mon, 02 Feb 2026 04:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-LIGHT-UP-RGB-LED/m-p/2304383#M15921</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2026-02-02T04:04:47Z</dc:date>
    </item>
  </channel>
</rss>