<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to Modify the PFE Driver and Compile It into the BSP Image in S32G</title>
    <link>https://community.nxp.com/t5/S32G/How-to-Modify-the-PFE-Driver-and-Compile-It-into-the-BSP-Image/m-p/2301160#M15904</link>
    <description>&lt;P&gt;Hi,&lt;SPAN&gt;waitewang&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP support! &lt;BR /&gt;It is recommended to first attempt to force the compilation of PFE.&lt;/P&gt;
&lt;P&gt;bitbake -c compile -f pfe&lt;BR /&gt;bitbake -c install -f pfe&lt;BR /&gt;bitbake pfe&lt;/P&gt;
&lt;P&gt;Or&lt;BR /&gt;bitbake -c cleansstate pfe&lt;BR /&gt;bitbake pfe&lt;/P&gt;
&lt;P&gt;2. Independently compile the PFE driver and check if the added debugging information is being output normally. &lt;BR /&gt;3. Check the startup information of the development board's kernel, and verify whether the PFE version information and the compiled and downloaded PFE version information are consistent.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
    <pubDate>Tue, 27 Jan 2026 10:08:51 GMT</pubDate>
    <dc:creator>Joey_z</dc:creator>
    <dc:date>2026-01-27T10:08:51Z</dc:date>
    <item>
      <title>How to Modify the PFE Driver and Compile It into the BSP Image</title>
      <link>https://community.nxp.com/t5/S32G/How-to-Modify-the-PFE-Driver-and-Compile-It-into-the-BSP-Image/m-p/2299882#M15901</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Dear Experts&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; I am using the S32G-VNP-RDB2 development board with the S32G274A chip. The Yocto environment has been fully set up, and the BSP can be compiled normally. Now I want to try adding some debugging information to the PFE driver.&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; I tried to modify the code under this directory—such as altering existing print statements or adding new ones—but after recompiling with bitbake, there were no changes at all; the print output remained the same. Could it be that I’m looking in the wrong directory?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="waitewang_0-1769304200038.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/374154i8D92FEA56DDA228E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="waitewang_0-1769304200038.png" alt="waitewang_0-1769304200038.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;waitewang_0-1769304200038.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 25 Jan 2026 01:26:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-Modify-the-PFE-Driver-and-Compile-It-into-the-BSP-Image/m-p/2299882#M15901</guid>
      <dc:creator>waitewang</dc:creator>
      <dc:date>2026-01-25T01:26:06Z</dc:date>
    </item>
    <item>
      <title>Re: How to Modify the PFE Driver and Compile It into the BSP Image</title>
      <link>https://community.nxp.com/t5/S32G/How-to-Modify-the-PFE-Driver-and-Compile-It-into-the-BSP-Image/m-p/2301160#M15904</link>
      <description>&lt;P&gt;Hi,&lt;SPAN&gt;waitewang&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP support! &lt;BR /&gt;It is recommended to first attempt to force the compilation of PFE.&lt;/P&gt;
&lt;P&gt;bitbake -c compile -f pfe&lt;BR /&gt;bitbake -c install -f pfe&lt;BR /&gt;bitbake pfe&lt;/P&gt;
&lt;P&gt;Or&lt;BR /&gt;bitbake -c cleansstate pfe&lt;BR /&gt;bitbake pfe&lt;/P&gt;
&lt;P&gt;2. Independently compile the PFE driver and check if the added debugging information is being output normally. &lt;BR /&gt;3. Check the startup information of the development board's kernel, and verify whether the PFE version information and the compiled and downloaded PFE version information are consistent.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jan 2026 10:08:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-Modify-the-PFE-Driver-and-Compile-It-into-the-BSP-Image/m-p/2301160#M15904</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2026-01-27T10:08:51Z</dc:date>
    </item>
  </channel>
</rss>