<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32G3 – Debug with S32 Debug Probe when JTAG is password protected (memory dump) in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G3-Debug-with-S32-Debug-Probe-when-JTAG-is-password-protected/m-p/2299050#M15897</link>
    <description>&lt;P&gt;Hi,dtejada02&lt;/P&gt;
&lt;P&gt;Thank you for contacting us.&lt;/P&gt;
&lt;P&gt;Do you do the secure debug? you can refer to this link for your using.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Secure-Debugging-from-S32DS-IDE-with-S32-Debugger-and-S32/ta-p/1964462" target="_blank"&gt;HOWTO: Secure Debugging from S32DS IDE with S32 Debugger and S32 Debug Probe&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Technically, memory read/dump can be performed, but the secure memory/HSE protected area may still be unreadable.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
    <pubDate>Fri, 23 Jan 2026 10:12:47 GMT</pubDate>
    <dc:creator>Joey_z</dc:creator>
    <dc:date>2026-01-23T10:12:47Z</dc:date>
    <item>
      <title>S32G3 – Debug with S32 Debug Probe when JTAG is password protected (memory dump)</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-Debug-with-S32-Debug-Probe-when-JTAG-is-password-protected/m-p/2298805#M15890</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working with an &lt;STRONG&gt;S32G3&lt;/STRONG&gt; device using an &lt;STRONG&gt;S32 Debug Probe&lt;/STRONG&gt; and&lt;STRONG&gt; S32 Design Studio.&lt;/STRONG&gt;&lt;BR /&gt;The device has &lt;STRONG&gt;JTAG protected with a password&lt;/STRONG&gt; (debug authentication enabled).&lt;/P&gt;&lt;P&gt;I have authorization to access this device. My goal is to &lt;STRONG&gt;attach the debugger and dump internal memory (Flash/RAM)&lt;/STRONG&gt; for analysis.&lt;/P&gt;&lt;P&gt;At the moment, JTAG access is blocked due to the password, and I would like to know:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;What is the &lt;STRONG&gt;correct procedure to authenticate/unlock JTAG&lt;/STRONG&gt; on S32G3 using the debug password&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;How this is done in practice with &lt;STRONG&gt;S32 Design Studio&lt;/STRONG&gt; and the &lt;STRONG&gt;S32 Debug Probe&lt;/STRONG&gt;&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Once authenticated, whether &lt;STRONG&gt;full memory access / memory dump&lt;/STRONG&gt; is supported or if there are restrictions&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Fri, 23 Jan 2026 07:10:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-Debug-with-S32-Debug-Probe-when-JTAG-is-password-protected/m-p/2298805#M15890</guid>
      <dc:creator>dtejada02</dc:creator>
      <dc:date>2026-01-23T07:10:45Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 – Debug with S32 Debug Probe when JTAG is password protected (memory dump)</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-Debug-with-S32-Debug-Probe-when-JTAG-is-password-protected/m-p/2299050#M15897</link>
      <description>&lt;P&gt;Hi,dtejada02&lt;/P&gt;
&lt;P&gt;Thank you for contacting us.&lt;/P&gt;
&lt;P&gt;Do you do the secure debug? you can refer to this link for your using.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Secure-Debugging-from-S32DS-IDE-with-S32-Debugger-and-S32/ta-p/1964462" target="_blank"&gt;HOWTO: Secure Debugging from S32DS IDE with S32 Debugger and S32 Debug Probe&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Technically, memory read/dump can be performed, but the secure memory/HSE protected area may still be unreadable.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Fri, 23 Jan 2026 10:12:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-Debug-with-S32-Debug-Probe-when-JTAG-is-password-protected/m-p/2299050#M15897</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2026-01-23T10:12:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 – Debug with S32 Debug Probe when JTAG is password protected (memory dump)</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-Debug-with-S32-Debug-Probe-when-JTAG-is-password-protected/m-p/2299207#M15899</link>
      <description>Hi Joey_z,&lt;BR /&gt;&lt;BR /&gt;Thank you for your answer. I followed all the steps of the link you shared and after introducing the password i get the following error:&lt;BR /&gt;&lt;BR /&gt;"Failure during execution of python script. Reason: "[CCS: secure debug attempt failed]\r\n" error has occured during starting debug for launch: 'PROJECT_M7_0_Debug_RAM_S32Debug'. Error code is 1340. See GDB traces console for additional information.&lt;BR /&gt;&lt;BR /&gt;BR,&lt;BR /&gt;Diego Tejada</description>
      <pubDate>Fri, 23 Jan 2026 11:28:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-Debug-with-S32-Debug-Probe-when-JTAG-is-password-protected/m-p/2299207#M15899</guid>
      <dc:creator>dtejada02</dc:creator>
      <dc:date>2026-01-23T11:28:35Z</dc:date>
    </item>
  </channel>
</rss>