<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: S32G-VNP-RDB2(s32g274a) board PFE network ping failed</title>
    <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-s32g274a-board-PFE-network-ping-failed/m-p/2268786#M15745</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256633"&gt;@waitewang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;I understand that you are running with BSP44 on a RDB2, may I know:&lt;/P&gt;
&lt;P&gt;1. You are using a pre-built BSP image to boot the board or built it yourself?&lt;/P&gt;
&lt;P&gt;2. Would you mind sharing all log for booting the board? from bootloader to the kernel shell, so that I could help to analyze the issue with details&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
    <pubDate>Thu, 25 Dec 2025 03:00:21 GMT</pubDate>
    <dc:creator>chenyin_h</dc:creator>
    <dc:date>2025-12-25T03:00:21Z</dc:date>
    <item>
      <title>S32G-VNP-RDB2(s32g274a) board PFE network ping failed</title>
      <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-s32g274a-board-PFE-network-ping-failed/m-p/2268727#M15742</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the&amp;nbsp;S32G-VNP-RDB2 board and run the Linux BSP 44.0 from NXP.&lt;/P&gt;&lt;P&gt;The BSP print the version "Auto Linux BSP 44.0 s32g274ardb2 ttyLF0".&lt;/P&gt;&lt;P&gt;Set the pfe0 net interface the IP 192.168.0.12&lt;/P&gt;&lt;P&gt;&lt;EM&gt;root@s32g274ardb2:/# ifconfig pfe0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;pfe0: flags=4163&amp;lt;UP,BROADCAST,RUNNING,MULTICAST&amp;gt; mtu 1500&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;inet 192.168.0.12 netmask 255.255.255.0 broadcast 192.168.0.1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;inet6 fe80::204:9fff:febe:ef00 prefixlen 64 scopeid 0x20&amp;lt;link&amp;gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ether 00:04:9f:be:ef:00 txqueuelen 1000 (Ethernet)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;RX packets 0 bytes 0 (0.0 B)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;RX errors 0 dropped 0 overruns 0 frame 0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;TX packets 127 bytes 15832 (15.4 KiB)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;device memory 0x46000000-46ffffff&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;when I used the ping command, it print&lt;/P&gt;&lt;P&gt;&lt;EM&gt;root@s32g274ardb2:/# ping 192.168.0.11 &lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;PING 192.168.0.11 (192.168.0.11) 56(84) bytes of data.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;From 192.168.0.12 icmp_seq=1 Destination Host Unreachable&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;ping: sendmsg: No route to host&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;From 192.168.0.12 icmp_seq=2 Destination Host Unreachable&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;From 192.168.0.12 icmp_seq=3 Destination Host Unreachable&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the PFE is different of GMAC? Can you tell me how to use the PFE network?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Dec 2025 13:20:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-s32g274a-board-PFE-network-ping-failed/m-p/2268727#M15742</guid>
      <dc:creator>waitewang</dc:creator>
      <dc:date>2025-12-24T13:20:12Z</dc:date>
    </item>
    <item>
      <title>Re: S32G-VNP-RDB2(s32g274a) board PFE network ping failed</title>
      <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-s32g274a-board-PFE-network-ping-failed/m-p/2268786#M15745</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256633"&gt;@waitewang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;I understand that you are running with BSP44 on a RDB2, may I know:&lt;/P&gt;
&lt;P&gt;1. You are using a pre-built BSP image to boot the board or built it yourself?&lt;/P&gt;
&lt;P&gt;2. Would you mind sharing all log for booting the board? from bootloader to the kernel shell, so that I could help to analyze the issue with details&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Thu, 25 Dec 2025 03:00:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-s32g274a-board-PFE-network-ping-failed/m-p/2268786#M15745</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-12-25T03:00:21Z</dc:date>
    </item>
    <item>
      <title>Re: S32G-VNP-RDB2(s32g274a) board PFE network ping failed</title>
      <link>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-s32g274a-board-PFE-network-ping-failed/m-p/2294612#M15830</link>
      <description>&lt;P&gt;hello&amp;nbsp;&lt;/P&gt;&lt;P&gt;(1)&amp;nbsp;I am using the binary image file downloaded from the official NXP website.&lt;/P&gt;&lt;P&gt;(2) I try it according to the manaul as follow, it is successfully.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="waitewang_0-1768525603975.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/373068i3003BE384EE4E585/image-size/medium?v=v2&amp;amp;px=400" role="button" title="waitewang_0-1768525603975.png" alt="waitewang_0-1768525603975.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;thanks very much!&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jan 2026 01:07:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-VNP-RDB2-s32g274a-board-PFE-network-ping-failed/m-p/2294612#M15830</guid>
      <dc:creator>waitewang</dc:creator>
      <dc:date>2026-01-16T01:07:37Z</dc:date>
    </item>
  </channel>
</rss>