<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32G3: debugging Linux with s32 debug probe in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G3-debugging-Linux-with-s32-debug-probe/m-p/2264528#M15689</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/24163"&gt;@chenyin_h&lt;/a&gt;&amp;nbsp; I do not find any information regarding "attaching to a running target" in any of the available documentation for S32 debug probe, or any instructions on debugging a running linux image. Can you please check internally and provide a debug example for this use case.&lt;BR /&gt;Also on the S32 DS, the debug configuration has no option for setting "attach only". The debugger always gives a reset to the hardware and even if the target is stopped at u-boot for DDR initialization, the debugger would give it&amp;nbsp; reset and then timeout on the connection.&lt;/P&gt;</description>
    <pubDate>Wed, 17 Dec 2025 08:03:27 GMT</pubDate>
    <dc:creator>rizwan_at_disruptdotcom</dc:creator>
    <dc:date>2025-12-17T08:03:27Z</dc:date>
    <item>
      <title>S32G3: debugging Linux with s32 debug probe</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-debugging-Linux-with-s32-debug-probe/m-p/1827775#M6256</link>
      <description>&lt;P&gt;Dear NXP Support Team,&lt;/P&gt;&lt;P&gt;We have recently purchased the S32G-VNP-RDB3 Board and have successfully compiled the NXP Auto Yocto Linux BSP v38.0. We can run Linux and boot to the Linux prompt without issues. Additionally, we have purchased the S32 Debug Probe.&lt;/P&gt;&lt;P&gt;Our current objective is to debug the Linux kernel, ATF (Arm Trusted Firmware), and U-Boot using the debugger. We seek guidance on how to connect the debugger to these components, set breakpoints within the kernel, ATF, and U-Boot code, and navigate through the debugging process.&lt;/P&gt;&lt;P&gt;Could you kindly direct us to a comprehensive guide or provide instructions that cover the connection of the debugger, setting of breakpoints, and stepping through the debugger?&lt;/P&gt;&lt;P&gt;Thank you for your assistance.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
      <pubDate>Wed, 13 Mar 2024 23:27:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-debugging-Linux-with-s32-debug-probe/m-p/1827775#M6256</guid>
      <dc:creator>s153022</dc:creator>
      <dc:date>2024-03-13T23:27:11Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3: debugging Linux with s32 debug probe</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-debugging-Linux-with-s32-debug-probe/m-p/1828980#M6277</link>
      <description>&lt;P&gt;Hello, @&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/153022" target="_blank"&gt;contributor3&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Thanks for the question.&lt;/P&gt;
&lt;P&gt;For using the debugger, the corresponding official documents could be downloaded from the following link: (including the user guide, quick start guide and fact sheet), which could be the basics for using the debugger.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/automotive-software-and-tools/s32-debug-probe:S32-DP" target="_blank"&gt;https://www.nxp.com/design/design-center/software/automotive-software-and-tools/s32-debug-probe:S32-DP&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Besides, there are also some other useful posts from the community, which could help for the details.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-JTAG-Flash-Programming-with-S32-Debugger-and-S32-Debug/ta-p/1113953" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-JTAG-Flash-Programming-with-S32-Debugger-and-S32-Debug/ta-p/1113953&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Start-S32-Debugger-from-S32-Design-Studio-on-S32G274A-EVB/ta-p/1121865" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Start-S32-Debugger-from-S32-Design-Studio-on-S32G274A-EVB/ta-p/1121865&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Mar 2024 03:20:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-debugging-Linux-with-s32-debug-probe/m-p/1828980#M6277</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-03-15T03:20:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3: debugging Linux with s32 debug probe</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-debugging-Linux-with-s32-debug-probe/m-p/2264528#M15689</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/24163"&gt;@chenyin_h&lt;/a&gt;&amp;nbsp; I do not find any information regarding "attaching to a running target" in any of the available documentation for S32 debug probe, or any instructions on debugging a running linux image. Can you please check internally and provide a debug example for this use case.&lt;BR /&gt;Also on the S32 DS, the debug configuration has no option for setting "attach only". The debugger always gives a reset to the hardware and even if the target is stopped at u-boot for DDR initialization, the debugger would give it&amp;nbsp; reset and then timeout on the connection.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Dec 2025 08:03:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-debugging-Linux-with-s32-debug-probe/m-p/2264528#M15689</guid>
      <dc:creator>rizwan_at_disruptdotcom</dc:creator>
      <dc:date>2025-12-17T08:03:27Z</dc:date>
    </item>
  </channel>
</rss>