<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Where is dts for S32G? in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Where-is-dts-for-S32G/m-p/2264262#M15684</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;As the DTS for S32G in the u-boot source tree is empty, I am wondering where it is.&lt;/P&gt;&lt;P&gt;I do see the post&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32G/S32G399A-Is-Device-Tree-Configuration-for-U-Boot-required/td-p/1946745" target="_self"&gt;here&lt;/A&gt;&amp;nbsp;, but still wondering:&lt;/P&gt;&lt;P&gt;1) As the existing DTS for S32G is empty, what's the recommended way to initialize the devices like serial, MMC, ethernet, etc?&lt;/P&gt;&lt;P&gt;2) Would it recommended to just copy the dts file from ATF to u-boot?&lt;/P&gt;&lt;P&gt;3) In regard to the serial uart, when the DTS is empty and it is not placed in U_BOOT_DEVINFO and it is not initialized in the legacy method before DM is initialized, how is it initialized?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Crane&lt;/P&gt;</description>
    <pubDate>Tue, 16 Dec 2025 23:53:17 GMT</pubDate>
    <dc:creator>cranes</dc:creator>
    <dc:date>2025-12-16T23:53:17Z</dc:date>
    <item>
      <title>Where is dts for S32G?</title>
      <link>https://community.nxp.com/t5/S32G/Where-is-dts-for-S32G/m-p/2264262#M15684</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;As the DTS for S32G in the u-boot source tree is empty, I am wondering where it is.&lt;/P&gt;&lt;P&gt;I do see the post&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32G/S32G399A-Is-Device-Tree-Configuration-for-U-Boot-required/td-p/1946745" target="_self"&gt;here&lt;/A&gt;&amp;nbsp;, but still wondering:&lt;/P&gt;&lt;P&gt;1) As the existing DTS for S32G is empty, what's the recommended way to initialize the devices like serial, MMC, ethernet, etc?&lt;/P&gt;&lt;P&gt;2) Would it recommended to just copy the dts file from ATF to u-boot?&lt;/P&gt;&lt;P&gt;3) In regard to the serial uart, when the DTS is empty and it is not placed in U_BOOT_DEVINFO and it is not initialized in the legacy method before DM is initialized, how is it initialized?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Crane&lt;/P&gt;</description>
      <pubDate>Tue, 16 Dec 2025 23:53:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Where-is-dts-for-S32G/m-p/2264262#M15684</guid>
      <dc:creator>cranes</dc:creator>
      <dc:date>2025-12-16T23:53:17Z</dc:date>
    </item>
    <item>
      <title>Re: Where is dts for S32G?</title>
      <link>https://community.nxp.com/t5/S32G/Where-is-dts-for-S32G/m-p/2264533#M15690</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224785"&gt;@cranes&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;Actually in current u-boot(for example, BSP43/44), you may find that the MMC/UART/ethernet(GMAC,.PFE) drivers are already initialized and could be used directly.&lt;/P&gt;
&lt;P&gt;There is no related formal document provisioned by NXP, so I suggest referencing the code directly for this driver probe process in u-boot.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Wed, 17 Dec 2025 08:07:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Where-is-dts-for-S32G/m-p/2264533#M15690</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-12-17T08:07:51Z</dc:date>
    </item>
  </channel>
</rss>