<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Re: Issue while running usecase on GoldVIP (GUI) in Docker Container</title>
    <link>https://community.nxp.com/t5/S32G/Issue-while-running-usecase-on-GoldVIP-GUI-in-Docker-Container/m-p/1540018#M1565</link>
    <description>&lt;P&gt;Hi George.&lt;/P&gt;&lt;P&gt;The issue with the v2xdomu ip address has been resolved.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But now we are facing an issue with the GMAC0 port. Is it okay to connect the ethernet cable to the GMAC0 port before powering on the goldbox? Ping status was a failure when we connected the ethernet cable before powering on. But when we connected the ethernet cable after booting process was completed, the ping showed success.&lt;/P&gt;</description>
    <pubDate>Wed, 19 Oct 2022 10:21:01 GMT</pubDate>
    <dc:creator>MidhunSreenivas</dc:creator>
    <dc:date>2022-10-19T10:21:01Z</dc:date>
    <item>
      <title>Issue while running usecase on GoldVIP (GUI) in Docker Container</title>
      <link>https://community.nxp.com/t5/S32G/Issue-while-running-usecase-on-GoldVIP-GUI-in-Docker-Container/m-p/1539059#M1559</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;There seems to be an issue while running usecase on GoldVIP (GUI) in Docker Container. I tried to navigate to the GoldVIP dashboard by typing the following address,&lt;/P&gt;&lt;P&gt;&lt;A href="http://localhost/nxpdemo" target="_blank"&gt;http://localhost/nxpdemo&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;in the address bar. GoldVIP dashboard was successfully opened, but there seems to be an issue in providing Dom0 IP. I tried to provide IP which I got by using the command " ip a" in the docker cli.&lt;/P&gt;&lt;P&gt;I tried executing usecase by trying out different IPs, but it shows error. Could you please suggest any alternate method for finding out the Dom0 IP or if something else is the issue?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Attached the screenshot of the error for your reference.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 18 Oct 2022 07:30:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Issue-while-running-usecase-on-GoldVIP-GUI-in-Docker-Container/m-p/1539059#M1559</guid>
      <dc:creator>MidhunSreenivas</dc:creator>
      <dc:date>2022-10-18T07:30:43Z</dc:date>
    </item>
    <item>
      <title>Re: Issue while running usecase on GoldVIP (GUI) in Docker Container</title>
      <link>https://community.nxp.com/t5/S32G/Issue-while-running-usecase-on-GoldVIP-GUI-in-Docker-Container/m-p/1539939#M1564</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you be more specific on what steps you followed to get the IP of the dom0 VM? Did you connect to the board's serial console before running the `ip a s` command (this is not clear from the initial message)? Can you ping the board (using the IP assigned on the xenbr0 interface) from the docker container CLI / your host machine (e.g., `ping -c 4 &amp;lt;board_ip&amp;gt;`)?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;George&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 19 Oct 2022 08:56:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Issue-while-running-usecase-on-GoldVIP-GUI-in-Docker-Container/m-p/1539939#M1564</guid>
      <dc:creator>gmocanu</dc:creator>
      <dc:date>2022-10-19T08:56:09Z</dc:date>
    </item>
    <item>
      <title>Re: Issue while running usecase on GoldVIP (GUI) in Docker Container</title>
      <link>https://community.nxp.com/t5/S32G/Issue-while-running-usecase-on-GoldVIP-GUI-in-Docker-Container/m-p/1540018#M1565</link>
      <description>&lt;P&gt;Hi George.&lt;/P&gt;&lt;P&gt;The issue with the v2xdomu ip address has been resolved.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But now we are facing an issue with the GMAC0 port. Is it okay to connect the ethernet cable to the GMAC0 port before powering on the goldbox? Ping status was a failure when we connected the ethernet cable before powering on. But when we connected the ethernet cable after booting process was completed, the ping showed success.&lt;/P&gt;</description>
      <pubDate>Wed, 19 Oct 2022 10:21:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Issue-while-running-usecase-on-GoldVIP-GUI-in-Docker-Container/m-p/1540018#M1565</guid>
      <dc:creator>MidhunSreenivas</dc:creator>
      <dc:date>2022-10-19T10:21:01Z</dc:date>
    </item>
    <item>
      <title>Re: Issue while running usecase on GoldVIP (GUI) in Docker Container</title>
      <link>https://community.nxp.com/t5/S32G/Issue-while-running-usecase-on-GoldVIP-GUI-in-Docker-Container/m-p/1540774#M1568</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't think there should be any issue with doing that (having the GMAC port already connected before POR). Does the board still acquire the IP through the DHCP client, or do you use a static network configuration? What is the output of the `ip a s` command after the board was rebooted, and does the IP reported by that command is in the local network? Could you test whether this behavior reproduces in some other networks as well?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;</description>
      <pubDate>Thu, 20 Oct 2022 05:40:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Issue-while-running-usecase-on-GoldVIP-GUI-in-Docker-Container/m-p/1540774#M1568</guid>
      <dc:creator>gmocanu</dc:creator>
      <dc:date>2022-10-20T05:40:36Z</dc:date>
    </item>
  </channel>
</rss>