<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: Telemetry Server</title>
    <link>https://community.nxp.com/t5/S32G/Telemetry-Server/m-p/1537607#M1544</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;There seems to be some issue with ethernet connectivity in the goldbox. We tried to access internet via wired connection by connecting to ethernet port (P3B - GMAC0).&amp;nbsp;&lt;/P&gt;&lt;P&gt;We pinged google from &lt;A href="mailto:root@s32g274arb2" target="_blank"&gt;root@s32g274arb2&lt;/A&gt;&amp;nbsp;and &lt;A href="mailto:root@v2xdomu" target="_blank"&gt;root@v2xdomu&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But it is resulting in 100% packet loss. What could be the issue? The same wired network does not have any problem with internet access when connected to host PC. Could this be the problem behind running the telemetry server use case?&lt;/P&gt;</description>
    <pubDate>Fri, 14 Oct 2022 07:15:45 GMT</pubDate>
    <dc:creator>MidhunSreenivas</dc:creator>
    <dc:date>2022-10-14T07:15:45Z</dc:date>
    <item>
      <title>Telemetry Server</title>
      <link>https://community.nxp.com/t5/S32G/Telemetry-Server/m-p/1537016#M1537</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;For accessing Telemetry Server, I logged into the v2xdomu virtual machine using the command:&amp;nbsp;&lt;/P&gt;&lt;P&gt;$ xl console v2xdomu&lt;/P&gt;&lt;P&gt;I connected&amp;nbsp;v2xdomu VM&amp;nbsp;to the same local network as our workstation. I got the v2xdomu ip address, by using the lp a command. I tried to access the dashboard using the URL:&amp;nbsp;&amp;lt;v2xdomu ip address&amp;gt; :5000/system_telemetry. But it was unsuccessfull. Could you please help me to find a solution?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Oct 2022 09:28:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Telemetry-Server/m-p/1537016#M1537</guid>
      <dc:creator>MidhunSreenivas</dc:creator>
      <dc:date>2022-10-13T09:28:59Z</dc:date>
    </item>
    <item>
      <title>Re: Telemetry Server</title>
      <link>https://community.nxp.com/t5/S32G/Telemetry-Server/m-p/1537131#M1542</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please check whether the board is reachable from your workstation (using something like &lt;EM&gt;ping -c 4 &amp;lt;v2xdomu_ip&amp;gt;&lt;/EM&gt;) and ensure that no traffic is blocked by the firewall? Also, could you check whether the Telemetry Server service is running while why try to open the webpage (i.e., run &lt;EM&gt;ps -ef | grep telemetry-server&lt;/EM&gt; on the v2xdomu VM)?&lt;BR /&gt;&lt;BR /&gt;Also, could you describe what error you encounter while you try to open the webpage? Do you see any dashboard displayed? Also, how do you connect your device to the local network - via a wired connection or Wi-Fi?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;George Mocanu&lt;/P&gt;</description>
      <pubDate>Thu, 13 Oct 2022 13:07:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Telemetry-Server/m-p/1537131#M1542</guid>
      <dc:creator>gmocanu</dc:creator>
      <dc:date>2022-10-13T13:07:35Z</dc:date>
    </item>
    <item>
      <title>Re: Telemetry Server</title>
      <link>https://community.nxp.com/t5/S32G/Telemetry-Server/m-p/1537607#M1544</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;There seems to be some issue with ethernet connectivity in the goldbox. We tried to access internet via wired connection by connecting to ethernet port (P3B - GMAC0).&amp;nbsp;&lt;/P&gt;&lt;P&gt;We pinged google from &lt;A href="mailto:root@s32g274arb2" target="_blank"&gt;root@s32g274arb2&lt;/A&gt;&amp;nbsp;and &lt;A href="mailto:root@v2xdomu" target="_blank"&gt;root@v2xdomu&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But it is resulting in 100% packet loss. What could be the issue? The same wired network does not have any problem with internet access when connected to host PC. Could this be the problem behind running the telemetry server use case?&lt;/P&gt;</description>
      <pubDate>Fri, 14 Oct 2022 07:15:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Telemetry-Server/m-p/1537607#M1544</guid>
      <dc:creator>MidhunSreenivas</dc:creator>
      <dc:date>2022-10-14T07:15:45Z</dc:date>
    </item>
    <item>
      <title>Re: Telemetry Server</title>
      <link>https://community.nxp.com/t5/S32G/Telemetry-Server/m-p/1537797#M1547</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you test whether the board can be reached from the host machine (and vice-versa) using the local network connection? Does the board get any IP at all assigned on the xenbr0 interface? Or maybe you have to add the MAC addresses of the board in your DHCP server? Please check with your IT/Networking engineers if additional configuration is needed besides that.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;George&lt;/P&gt;</description>
      <pubDate>Fri, 14 Oct 2022 10:34:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Telemetry-Server/m-p/1537797#M1547</guid>
      <dc:creator>gmocanu</dc:creator>
      <dc:date>2022-10-14T10:34:48Z</dc:date>
    </item>
  </channel>
</rss>