<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IGMP Snooping with SJA1110 in S32G</title>
    <link>https://community.nxp.com/t5/S32G/IGMP-Snooping-with-SJA1110/m-p/2199185#M15429</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have an S32G with SJA1110 running bsp43 and am trying to enable IGMP snooping to dynamically route multicast streams.&amp;nbsp; I have identified a few unique issues related to IGMP which I am not sure how to resolve.&amp;nbsp; I have confirmed that disabling IGMP snooping causes multicast packets to flood the switch, so the IGMP snooping option is doing something...&amp;nbsp; Just not the expected behavior.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Multicast traffic is always forwarded to the lowest enumerated active port&lt;OL&gt;&lt;LI&gt;A stream egressing on port 4 with a node on port 3 requesting that traffic through IGMP will cause traffic to egress through port 1 (if that link is active) as if port 1 had requested the traffic.&amp;nbsp; If the port 1 link is not active, traffic will be forwarded to port 2 if that link is active.&lt;/LI&gt;&lt;LI&gt;I am able to manually route the traffic with mdb, but my expectation is that IGMP snooping should be managing this automatically&lt;/LI&gt;&lt;/OL&gt;&lt;/LI&gt;&lt;LI&gt;Enabling multicast-querier does not cause membership queries to egress the switch ports&lt;OL&gt;&lt;LI&gt;There are&amp;nbsp; IGMP queries on the DSA bridge interface, but no IGMP queries are visible on other links connected to the switch&lt;/LI&gt;&lt;LI&gt;I suspect I may need to set up a tc rule to trap IGMP queries from the bridge port and redirect them to the switch ports?&lt;/LI&gt;&lt;/OL&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;I'm not clear if this is some issue with Linux configuration or a limitation from switch hardware.&lt;/P&gt;&lt;P&gt;Thanks for any suggestions.&lt;/P&gt;</description>
    <pubDate>Wed, 05 Nov 2025 16:25:18 GMT</pubDate>
    <dc:creator>sg_cnh</dc:creator>
    <dc:date>2025-11-05T16:25:18Z</dc:date>
    <item>
      <title>IGMP Snooping with SJA1110</title>
      <link>https://community.nxp.com/t5/S32G/IGMP-Snooping-with-SJA1110/m-p/2199185#M15429</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have an S32G with SJA1110 running bsp43 and am trying to enable IGMP snooping to dynamically route multicast streams.&amp;nbsp; I have identified a few unique issues related to IGMP which I am not sure how to resolve.&amp;nbsp; I have confirmed that disabling IGMP snooping causes multicast packets to flood the switch, so the IGMP snooping option is doing something...&amp;nbsp; Just not the expected behavior.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Multicast traffic is always forwarded to the lowest enumerated active port&lt;OL&gt;&lt;LI&gt;A stream egressing on port 4 with a node on port 3 requesting that traffic through IGMP will cause traffic to egress through port 1 (if that link is active) as if port 1 had requested the traffic.&amp;nbsp; If the port 1 link is not active, traffic will be forwarded to port 2 if that link is active.&lt;/LI&gt;&lt;LI&gt;I am able to manually route the traffic with mdb, but my expectation is that IGMP snooping should be managing this automatically&lt;/LI&gt;&lt;/OL&gt;&lt;/LI&gt;&lt;LI&gt;Enabling multicast-querier does not cause membership queries to egress the switch ports&lt;OL&gt;&lt;LI&gt;There are&amp;nbsp; IGMP queries on the DSA bridge interface, but no IGMP queries are visible on other links connected to the switch&lt;/LI&gt;&lt;LI&gt;I suspect I may need to set up a tc rule to trap IGMP queries from the bridge port and redirect them to the switch ports?&lt;/LI&gt;&lt;/OL&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;I'm not clear if this is some issue with Linux configuration or a limitation from switch hardware.&lt;/P&gt;&lt;P&gt;Thanks for any suggestions.&lt;/P&gt;</description>
      <pubDate>Wed, 05 Nov 2025 16:25:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IGMP-Snooping-with-SJA1110/m-p/2199185#M15429</guid>
      <dc:creator>sg_cnh</dc:creator>
      <dc:date>2025-11-05T16:25:18Z</dc:date>
    </item>
    <item>
      <title>Re: IGMP Snooping with SJA1110</title>
      <link>https://community.nxp.com/t5/S32G/IGMP-Snooping-with-SJA1110/m-p/2199449#M15431</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256556"&gt;@sg_cnh&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thanks for reaching out to us. About your question, the&amp;nbsp;IGMP is not a feature we can support in the S32G community, as far as I can tell the IGMP is done over IP, it is not related to the S32G itself, I checked the GMAC, PFE modules and the SJA1110 chip and none of them include direct support or examples for that feature. You may get some guidance in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Other-NXP-Products/bd-p/other" target="_blank"&gt;Other-NXP-Products&lt;/A&gt;, where the support engineers for the SJA1110 can help you.&lt;/P&gt;
&lt;P&gt;I apologize for the inconveniences.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Nov 2025 22:16:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IGMP-Snooping-with-SJA1110/m-p/2199449#M15431</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2025-11-05T22:16:10Z</dc:date>
    </item>
    <item>
      <title>Re: IGMP Snooping with SJA1110</title>
      <link>https://community.nxp.com/t5/S32G/IGMP-Snooping-with-SJA1110/m-p/2199454#M15432</link>
      <description>&lt;P&gt;Thanks for the reply.&amp;nbsp; I have reposted to the other forum you suggested.&lt;/P&gt;</description>
      <pubDate>Wed, 05 Nov 2025 22:25:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IGMP-Snooping-with-SJA1110/m-p/2199454#M15432</guid>
      <dc:creator>sg_cnh</dc:creator>
      <dc:date>2025-11-05T22:25:26Z</dc:date>
    </item>
    <item>
      <title>Re: IGMP Snooping with SJA1110</title>
      <link>https://community.nxp.com/t5/S32G/IGMP-Snooping-with-SJA1110/m-p/2200280#M15440</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/256556"&gt;@sg_cnh&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thanks for understanding and reposting your question in the other forum.&lt;/P&gt;
&lt;P&gt;Let me know if there is something else you need support with.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 06 Nov 2025 19:33:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/IGMP-Snooping-with-SJA1110/m-p/2200280#M15440</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2025-11-06T19:33:22Z</dc:date>
    </item>
  </channel>
</rss>