<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 SRAM ECC solution</title>
    <link>https://community.nxp.com/t5/S32G/SRAM-ECC-solution/m-p/2179818#M15071</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;working on S32G3 board. enabled SRAM0 ECC error for monitoring SRAM0.&lt;/P&gt;&lt;P&gt;and then i see the SRAM UE (uncorrectable error) is being reported. through FCCU i have enabled the FAULT ID (2) - SRAM UE.&lt;/P&gt;&lt;P&gt;so, my question is there way to handle this kind of error. apart from just configuration reaction (alarm, NMI, reset)? also have eMCEM module of SAF integrated with it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;another question will Power on reset really clears the UE error from SRAM?&lt;/P&gt;</description>
    <pubDate>Fri, 03 Oct 2025 09:28:26 GMT</pubDate>
    <dc:creator>Harish_R</dc:creator>
    <dc:date>2025-10-03T09:28:26Z</dc:date>
    <item>
      <title>SRAM ECC solution</title>
      <link>https://community.nxp.com/t5/S32G/SRAM-ECC-solution/m-p/2179818#M15071</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;working on S32G3 board. enabled SRAM0 ECC error for monitoring SRAM0.&lt;/P&gt;&lt;P&gt;and then i see the SRAM UE (uncorrectable error) is being reported. through FCCU i have enabled the FAULT ID (2) - SRAM UE.&lt;/P&gt;&lt;P&gt;so, my question is there way to handle this kind of error. apart from just configuration reaction (alarm, NMI, reset)? also have eMCEM module of SAF integrated with it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;another question will Power on reset really clears the UE error from SRAM?&lt;/P&gt;</description>
      <pubDate>Fri, 03 Oct 2025 09:28:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/SRAM-ECC-solution/m-p/2179818#M15071</guid>
      <dc:creator>Harish_R</dc:creator>
      <dc:date>2025-10-03T09:28:26Z</dc:date>
    </item>
    <item>
      <title>Re: SRAM ECC solution</title>
      <link>https://community.nxp.com/t5/S32G/SRAM-ECC-solution/m-p/2181471#M15100</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242921"&gt;@Harish_R&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Sorry for the late reply.&amp;nbsp; The only reaction options are ones you mentioned, as detailed in section&amp;nbsp;&lt;EM&gt;2.4 Recovery Mechanisms &lt;/EM&gt;of eMcem User manual:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="alejandro_e_0-1759868383250.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/359808i99CE2E55A75814D0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="alejandro_e_0-1759868383250.png" alt="alejandro_e_0-1759868383250.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regarding your second question, checking the S32G3 fault map and Reference manual, the&amp;nbsp;&lt;EM&gt;M7_0 SRAM ECC uncorrectable error&amp;nbsp;&lt;/EM&gt;should be cleared by performing a &lt;EM&gt;Power On Reset&lt;/EM&gt;, however, if the error is a symptom of an silicon problem, for instance after a problem with the power supplies, the error will appear constantly.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Oct 2025 20:29:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/SRAM-ECC-solution/m-p/2181471#M15100</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2025-10-07T20:29:03Z</dc:date>
    </item>
  </channel>
</rss>