<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックS32G Goldvip CAN usecase hardware setup</title>
    <link>https://community.nxp.com/t5/S32G/S32G-Goldvip-CAN-usecase-hardware-setup/m-p/1533416#M1501</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to test the CAN usecase.&lt;/P&gt;&lt;P&gt;I connected the following pins using wires:&lt;/P&gt;&lt;P&gt;i) FlexCAN0(L) to LLCE-CAN0 (L)&lt;/P&gt;&lt;P&gt;ii) FlexCAN0(H) to LLCE-CAN0 (H)&lt;/P&gt;&lt;P&gt;iii) FlexCAN1(L) to LLCE-CAN1(L)&lt;/P&gt;&lt;P&gt;iv) FlexCAN1(H) to LLCE-CAN1(H)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I executed the following script:&lt;/P&gt;&lt;P&gt;./canperf.sh -t can0 -r can1 -i 0 -o 4 -s 64 -g 0 -l 10&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But the output was not as expected. Attaching the generated report below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1665062477469(1).jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/195941iB8FAA27C176FA718/image-size/large?v=v2&amp;amp;px=999" role="button" title="1665062477469(1).jpg" alt="1665062477469(1).jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;1665062477469(1).jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Could you please explain what could be the issue here? Is there any additional hardware requirement? The image used is golvip1.3.0&lt;/P&gt;</description>
    <pubDate>Thu, 06 Oct 2022 13:38:34 GMT</pubDate>
    <dc:creator>Vishnu13</dc:creator>
    <dc:date>2022-10-06T13:38:34Z</dc:date>
    <item>
      <title>S32G Goldvip CAN usecase hardware setup</title>
      <link>https://community.nxp.com/t5/S32G/S32G-Goldvip-CAN-usecase-hardware-setup/m-p/1533416#M1501</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to test the CAN usecase.&lt;/P&gt;&lt;P&gt;I connected the following pins using wires:&lt;/P&gt;&lt;P&gt;i) FlexCAN0(L) to LLCE-CAN0 (L)&lt;/P&gt;&lt;P&gt;ii) FlexCAN0(H) to LLCE-CAN0 (H)&lt;/P&gt;&lt;P&gt;iii) FlexCAN1(L) to LLCE-CAN1(L)&lt;/P&gt;&lt;P&gt;iv) FlexCAN1(H) to LLCE-CAN1(H)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I executed the following script:&lt;/P&gt;&lt;P&gt;./canperf.sh -t can0 -r can1 -i 0 -o 4 -s 64 -g 0 -l 10&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But the output was not as expected. Attaching the generated report below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1665062477469(1).jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/195941iB8FAA27C176FA718/image-size/large?v=v2&amp;amp;px=999" role="button" title="1665062477469(1).jpg" alt="1665062477469(1).jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;1665062477469(1).jpg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Could you please explain what could be the issue here? Is there any additional hardware requirement? The image used is golvip1.3.0&lt;/P&gt;</description>
      <pubDate>Thu, 06 Oct 2022 13:38:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-Goldvip-CAN-usecase-hardware-setup/m-p/1533416#M1501</guid>
      <dc:creator>Vishnu13</dc:creator>
      <dc:date>2022-10-06T13:38:34Z</dc:date>
    </item>
    <item>
      <title>Re: S32G Goldvip CAN usecase hardware setup</title>
      <link>https://community.nxp.com/t5/S32G/S32G-Goldvip-CAN-usecase-hardware-setup/m-p/1533492#M1502</link>
      <description>&lt;P&gt;Hello, Vishnu,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The fact that the reported M7 core loads are 0% tells me that the application doesn't run at all. Are you sure you booted from QSPI? The SW4.7 DIP switch should be set to OFF.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;George&lt;/P&gt;</description>
      <pubDate>Thu, 06 Oct 2022 16:03:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-Goldvip-CAN-usecase-hardware-setup/m-p/1533492#M1502</guid>
      <dc:creator>gmocanu</dc:creator>
      <dc:date>2022-10-06T16:03:30Z</dc:date>
    </item>
  </channel>
</rss>