<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: PFE1 ping is not working</title>
    <link>https://community.nxp.com/t5/S32G/PFE1-ping-is-not-working/m-p/2173228#M14966</link>
    <description>&lt;P&gt;hi,uiv12187&lt;/P&gt;
&lt;P&gt;Thank you for your reply and detail information.&lt;/P&gt;
&lt;P&gt;You configuration of Serdes is not successful, so you can use the PFE1.&lt;/P&gt;
&lt;P&gt;you need to set the&amp;nbsp;&lt;SPAN&gt;xpcs1_1 of Serdes1 when you use the PFE1.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Could you try to set the parameter an=0?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;setenv hwconfig "...;xpcs1_1:speed=100M,an=0"&lt;BR /&gt;save&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;And set the PFE1 function in Kernel mode to&amp;nbsp;fixed link.&lt;BR /&gt;&lt;BR /&gt;fixed-link {&lt;BR /&gt;speed = &amp;lt;100&amp;gt;;&lt;BR /&gt;full-duplex;&lt;BR /&gt;}&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Joey&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 22 Sep 2025 03:44:39 GMT</pubDate>
    <dc:creator>Joey_z</dc:creator>
    <dc:date>2025-09-22T03:44:39Z</dc:date>
    <item>
      <title>PFE1 ping is not working</title>
      <link>https://community.nxp.com/t5/S32G/PFE1-ping-is-not-working/m-p/2171624#M14926</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In out custom board we are using s32g3 and bsp44. here pfe1 we interfaced with external dp83tc812 100base T1 Phy. in kernel dts configuration i am using managed=in-band-status arm trusted firmware side i am not using manged= in-band-status. just in hwconfig an=1 i set but when i did this bellow error i am facing how to fix this issue please let me.&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Error:&lt;/STRONG&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;arch/arm/mach-s32/s32-cc/hwconfig_fixups.c:1124-set_xpcs_config_sgmii() Failed to configure XPCS1_1&lt;BR /&gt;arch/arm/mach-s32/s32-cc/hwconfig_fixups.c:1198-apply_hwconfig_fixups() Failed to update XPCS1 for SerDes1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Raghavendra&lt;/P&gt;</description>
      <pubDate>Thu, 18 Sep 2025 05:08:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/PFE1-ping-is-not-working/m-p/2171624#M14926</guid>
      <dc:creator>uiv12187</dc:creator>
      <dc:date>2025-09-18T05:08:31Z</dc:date>
    </item>
    <item>
      <title>Re: PFE1 ping is not working</title>
      <link>https://community.nxp.com/t5/S32G/PFE1-ping-is-not-working/m-p/2171978#M14944</link>
      <description>&lt;P&gt;hi,&lt;SPAN&gt;uiv12187&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thank you for contacting us.&lt;/P&gt;
&lt;P&gt;Could you provide more log in uboot and Kernel?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;How about the function of PFE1 in uboot?&amp;nbsp;Can do the PFE1 connect the PHY?&lt;/P&gt;
&lt;P&gt;Do you only use the A core?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Sep 2025 11:27:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/PFE1-ping-is-not-working/m-p/2171978#M14944</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2025-09-18T11:27:21Z</dc:date>
    </item>
    <item>
      <title>Re: PFE1 ping is not working</title>
      <link>https://community.nxp.com/t5/S32G/PFE1-ping-is-not-working/m-p/2171987#M14945</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;here i am using&amp;nbsp;&lt;SPAN&gt;&lt;STRONG&gt;external dp83tc812 100base T1 Phy&lt;/STRONG&gt; this phy supports &lt;STRONG&gt;100M&lt;/STRONG&gt; i configured dts properly it is connected &lt;STRONG&gt;s32g3 pfe1: serdes1 xpcs1 lane 1 to&amp;nbsp;dp83tc812 100base T1 Phy&lt;/STRONG&gt; if we use &lt;STRONG&gt;fixed link or manged=in-band-status it automatically set speed 1G Thats Why i removed fixed link and managed=in-band-status&lt;/STRONG&gt; i configured an=1 to pfe1 because i am using external phy if i use an=0 it inject fixed link and detach driver. now linux side driver is attahed but u-boot side i am facing this issue when i set an=1 but &lt;STRONG&gt;i want to set an=1 then only my driver will work how to fix this issue&lt;/STRONG&gt; bellow i added boot log for u-boot please refer and help me to resolve this issue as soon as possible&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;=&amp;gt; setenv hwconfig "serdes0:mode=pcie&amp;amp;xpcs0,clock=int,fmhz=100;pcie0:mode=rc;xpcs0_0:speed=1G,an=0;serdes1:mode=xpcs0&amp;amp;xpcs1,clock=int,fmhz=125;xpcs1_0:speed=1G,an=0;xpcs1_1:speed=100M"&lt;BR /&gt;=&amp;gt; save&lt;BR /&gt;Saving Environment to MMC... Writing to MMC(0)... OK&lt;BR /&gt;=&amp;gt; reset&lt;BR /&gt;resetting ...&lt;BR /&gt;NOTICE: Reset status: Destructive Reset (RUN)&lt;BR /&gt;NOTICE: BL2: v2.10.14(release):bsp44.0-2.10.14-dirty&lt;BR /&gt;NOTICE: BL2: Built : 08:13:32, May 13 2025&lt;BR /&gt;NOTICE: BL2: Booting BL31&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2022.04+g9a00323278+p0 (May 13 2025 - 06:57:56 +0000)&lt;/P&gt;&lt;P&gt;SoC: NXP S32G399A rev. 1.1&lt;BR /&gt;CPU: ARM Cortex-A53 r0p4 @ max 1300 MHz&lt;BR /&gt;Model: NXP S32G399A-RDB3&lt;BR /&gt;DRAM: 3.5 GiB&lt;BR /&gt;Core: 298 devices, 24 uclasses, devicetree: board&lt;BR /&gt;MMC: FSL_SDHC: 0&lt;BR /&gt;Loading Environment from MMC... OK&lt;BR /&gt;&lt;STRONG&gt;arch/arm/mach-s32/s32-cc/hwconfig_fixups.c:1124-set_xpcs_config_sgmii() Failed to configure XPCS1_1&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;arch/arm/mach-s32/s32-cc/hwconfig_fixups.c:1198-apply_hwconfig_fixups() Failed to update XPCS1 for SerDes1&lt;/STRONG&gt;&lt;BR /&gt;drivers/phy/nxp/s32cc-serdes.c:1013- init_serdes() s32cc_serdes_phy serdes@40480000: Using mode 1 for SerDes subsystem&lt;BR /&gt;Serdes@40480000 PCIE_PHY_GEN_CTRL = 0x10c00&lt;BR /&gt;Serdes@40480000 PCIE_PHY_GEN_CTRL = 0x10c00&lt;BR /&gt;drivers/pci/pci_s32cc.c:824-s32cc_pcie_init_controller() pci_s32cc pcie@40400000: Configuring as RootComplex&lt;BR /&gt;drivers/pci/pci_s32cc.c:845-s32cc_pcie_config_host() pci_s32cc pcie@40400000: Failed to get link up&lt;BR /&gt;In: serial@401c8000&lt;BR /&gt;Out: serial@401c8000&lt;BR /&gt;Err: serial@401c8000&lt;BR /&gt;Board revision: RDB3&lt;BR /&gt;PCIe: BusDevFun VendorId DeviceId Device Class Sub-Class&lt;BR /&gt;__________________________________________________________________________&lt;BR /&gt;pcie@40400000 RootComplex&lt;BR /&gt;| `-- 01:00.00 0x1957 0x4300 Bridge device 0x04&lt;BR /&gt;Net: drivers/phy/nxp/s32cc-serdes.c:495-xpcs_check_rx_stable() s32cc_serdes_phy serdes@40480000: Stable RX detected on XPCS0 after 0 Âµs&lt;BR /&gt;eth0: ethernet@4033c000drivers/net/nxp_pfeng/pfe_hw.c:814-pfe_hw_detect_version()&lt;BR /&gt;Found PFE version 0x0101 (S32G3)&lt;BR /&gt;drivers/net/nxp_pfeng/pfe_hw_pe.c:418-pfe_hw_pe_init_class() pfeng pfeng-base: Uploading CLASS firmware&lt;BR /&gt;drivers/net/nxp_pfeng/pfe_hw_emac.c:284- pfe_hw_emac_init() pfeng pfeng-base: EMAC0 block was initialized&lt;BR /&gt;drivers/net/nxp_pfeng/pfe_hw_emac.c:284- pfe_hw_emac_init() pfeng pfeng-base: EMAC1 block was initialized&lt;BR /&gt;drivers/net/nxp_pfeng/pfe_hw.c:684- pfe_hw_init() pfeng pfeng-base: EMAC2 not used, skipped&lt;BR /&gt;drivers/net/nxp_pfeng/pfe_hw.c:723- pfe_hw_init() pfeng pfeng-base: Enabling the CLASS block&lt;BR /&gt;drivers/net/nxp_pfeng/pfe_hw.c:739- pfe_hw_init() pfeng pfeng-base: PFE Platform started successfully (mask: 3)&lt;BR /&gt;drivers/phy/nxp/s32cc-serdes.c:1013- init_serdes() s32cc_serdes_phy serdes@44180000: Using mode 3 for SerDes subsystem&lt;BR /&gt;drivers/phy/nxp/s32cc-serdes.c:495-xpcs_check_rx_stable() s32cc_serdes_phy serdes@44180000: Stable RX detected on XPCS0 after 0 Âµs&lt;BR /&gt;, eth1: pfe0drivers/phy/nxp/s32cc-serdes.c:495-xpcs_check_rx_stable() s32cc_serdes_phy serdes@44180000: Stable RX detected on XPCS1 after 0 Âµs&lt;BR /&gt;, eth2: pfe1&lt;/P&gt;</description>
      <pubDate>Thu, 18 Sep 2025 11:43:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/PFE1-ping-is-not-working/m-p/2171987#M14945</guid>
      <dc:creator>uiv12187</dc:creator>
      <dc:date>2025-09-18T11:43:11Z</dc:date>
    </item>
    <item>
      <title>Re: PFE1 ping is not working</title>
      <link>https://community.nxp.com/t5/S32G/PFE1-ping-is-not-working/m-p/2173228#M14966</link>
      <description>&lt;P&gt;hi,uiv12187&lt;/P&gt;
&lt;P&gt;Thank you for your reply and detail information.&lt;/P&gt;
&lt;P&gt;You configuration of Serdes is not successful, so you can use the PFE1.&lt;/P&gt;
&lt;P&gt;you need to set the&amp;nbsp;&lt;SPAN&gt;xpcs1_1 of Serdes1 when you use the PFE1.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Could you try to set the parameter an=0?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;setenv hwconfig "...;xpcs1_1:speed=100M,an=0"&lt;BR /&gt;save&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;And set the PFE1 function in Kernel mode to&amp;nbsp;fixed link.&lt;BR /&gt;&lt;BR /&gt;fixed-link {&lt;BR /&gt;speed = &amp;lt;100&amp;gt;;&lt;BR /&gt;full-duplex;&lt;BR /&gt;}&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Joey&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Sep 2025 03:44:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/PFE1-ping-is-not-working/m-p/2173228#M14966</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2025-09-22T03:44:39Z</dc:date>
    </item>
    <item>
      <title>Re: PFE1 ping is not working</title>
      <link>https://community.nxp.com/t5/S32G/PFE1-ping-is-not-working/m-p/2261162#M15665</link>
      <description>&lt;P&gt;Hello Joey_z,&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; if using same driver and pfe1 changes bsp41 is working fine and i am able to ping but in bsp44 if i applied same changes it is showing driver attached inbandstatus, and link also but ping is failed&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 12 Dec 2025 11:34:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/PFE1-ping-is-not-working/m-p/2261162#M15665</guid>
      <dc:creator>uiv12187</dc:creator>
      <dc:date>2025-12-12T11:34:09Z</dc:date>
    </item>
  </channel>
</rss>