<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I2C communication happening only while using Debugger and breakpoints. in S32G</title>
    <link>https://community.nxp.com/t5/S32G/I2C-communication-happening-only-while-using-Debugger-and/m-p/1530539#M1477</link>
    <description>&lt;P&gt;I am trying to achieve an I2C communication with the EEPROM and Temperature sensor. As long as the communication is concerned, it is established and I am able to do all the read and write operations with the EEPROM and the temperature sensor. The issue is I am only able to do it in debugger view with the help of some breakpoints while sending the slave address and word address, if I try to do the communication without the breakpoints then I run into a popup which tells "Interrupt failed".&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 29 Sep 2022 14:42:56 GMT</pubDate>
    <dc:creator>prabhat_</dc:creator>
    <dc:date>2022-09-29T14:42:56Z</dc:date>
    <item>
      <title>I2C communication happening only while using Debugger and breakpoints.</title>
      <link>https://community.nxp.com/t5/S32G/I2C-communication-happening-only-while-using-Debugger-and/m-p/1530539#M1477</link>
      <description>&lt;P&gt;I am trying to achieve an I2C communication with the EEPROM and Temperature sensor. As long as the communication is concerned, it is established and I am able to do all the read and write operations with the EEPROM and the temperature sensor. The issue is I am only able to do it in debugger view with the help of some breakpoints while sending the slave address and word address, if I try to do the communication without the breakpoints then I run into a popup which tells "Interrupt failed".&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Sep 2022 14:42:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/I2C-communication-happening-only-while-using-Debugger-and/m-p/1530539#M1477</guid>
      <dc:creator>prabhat_</dc:creator>
      <dc:date>2022-09-29T14:42:56Z</dc:date>
    </item>
  </channel>
</rss>