<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: S32G3 LLCE on GoldVip image</title>
    <link>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2161995#M14718</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;I was able to build the BSP 44 image with the enabling of the LLCE FW.&lt;BR /&gt;Then I was trying to build my YOCTO image starting from the GoldVip base image and the attached local.conf file.&lt;BR /&gt;&lt;BR /&gt;I managed to build the image, but when it is loaded on the SD card and the board is on, no LLCE interfaces appear in ifconfig output. Although, I can see the LLCE interfaces as enabled in the DTS file after the build (attached as well).&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Can you explain how to face with this situation?&lt;BR /&gt;Thank you.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 02 Sep 2025 08:56:56 GMT</pubDate>
    <dc:creator>MrAlexIV</dc:creator>
    <dc:date>2025-09-02T08:56:56Z</dc:date>
    <item>
      <title>S32G3 LLCE on GoldVip image</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2156589#M14595</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I built and installed the GoldVip image on the SD card (using Yocto), as described in chapter 23 of the &lt;STRONG&gt;&lt;EM&gt;GoldVip-User-Manual.pdf&lt;/EM&gt;&lt;/STRONG&gt;, also including the components required for LLCE. When I boot the system, I can indeed see that the LLCE firmware is loaded. I also see that the &lt;STRONG&gt;llce_can&lt;/STRONG&gt; entries in the DTS (attached) are set to “okay,” and in the .&lt;STRONG&gt;config&amp;nbsp;&lt;/STRONG&gt;I have:&amp;nbsp;&lt;BR /&gt;CONFIG_CAN_LLCE=y&lt;BR /&gt;CONFIG_CAN_LLCE_CORE=y&lt;BR /&gt;CONFIG_CAN_LLCE_CONTROLLER=m&lt;BR /&gt;My problem, however, is that I don’t see the &lt;STRONG&gt;llce_can&lt;/STRONG&gt; interfaces with ifconfig or ip link show; I only see can0 and can and can1 (which belong to FlexCAN).&lt;BR /&gt;How is this possible?&lt;/P&gt;</description>
      <pubDate>Fri, 22 Aug 2025 07:33:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2156589#M14595</guid>
      <dc:creator>MrAlexIV</dc:creator>
      <dc:date>2025-08-22T07:33:27Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 LLCE on GoldVip image</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2156660#M14597</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252410"&gt;@MrAlexIV&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;1. May I know which version GoldVIP you are working with?&lt;/P&gt;
&lt;P&gt;2. Would you mind sharing me with the full booting log from console?&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Aug 2025 09:19:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2156660#M14597</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-08-22T09:19:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 LLCE on GoldVip image</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2156666#M14598</link>
      <description>&lt;P&gt;I am using &lt;STRONG&gt;GoldVip 1.14.0&lt;BR /&gt;&lt;/STRONG&gt;I attach the boot log in the following file&lt;/P&gt;</description>
      <pubDate>Fri, 22 Aug 2025 09:31:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2156666#M14598</guid>
      <dc:creator>MrAlexIV</dc:creator>
      <dc:date>2025-08-22T09:31:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 LLCE on GoldVip image</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2157339#M14605</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252410"&gt;@MrAlexIV&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Thanks for your reply.&lt;/P&gt;
&lt;P&gt;From the release notes, the BSP44 and LLCE1.0.10 are used in GoldVIP1.14, from the log, seems it was 1.0.9 used? would you mind checking it from your test？&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Mon, 25 Aug 2025 06:29:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2157339#M14605</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-08-25T06:29:38Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 LLCE on GoldVip image</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2157547#M14610</link>
      <description>&lt;P&gt;Thank you for the observation.&lt;BR /&gt;Yes, I was using 1.0.9, but I now re-builded with the 1.0.10.&lt;BR /&gt;Anyway, I always have the same problem (I do not see the interfaces). I also noticed that I can't start the board in booting in NOR Flash Boot Mode (log attached).&lt;/P&gt;</description>
      <pubDate>Mon, 25 Aug 2025 12:06:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2157547#M14610</guid>
      <dc:creator>MrAlexIV</dc:creator>
      <dc:date>2025-08-25T12:06:34Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 LLCE on GoldVip image</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2157945#M14621</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252410"&gt;@MrAlexIV&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your reply.&lt;/P&gt;
&lt;P&gt;I did a quick test with the BSP44 Yocto source directly, with the modification on the conf/local.conf&lt;/P&gt;
&lt;P&gt;DISTRO_FEATURES:append = " llce-fw-load llce-can"&lt;BR /&gt;NXP_FIRMWARE_LOCAL_DIR = "PATH_TO_LLCEFW"&lt;/P&gt;
&lt;P&gt;Once rebuilt, the llcecan0-15 could be seen from the linux shell.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Aug 2025 03:40:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2157945#M14621</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-08-26T03:40:25Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 LLCE on GoldVip image</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2158431#M14630</link>
      <description>&lt;P&gt;Thank you for your reply.&lt;BR /&gt;I tried with the BSP44.0, but I still can't see the interface. I used the lines you mentioned.&lt;BR /&gt;I attach the boot logs (with some operations I did).&lt;BR /&gt;Also, in the boot I can clearly see this message :&lt;BR /&gt;&lt;EM&gt;"[ 7.054478] llce_mb 43a00000.llce_mb: LLCE modules are under reset. Is the LLCE firmware loaded?&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;[ 7.062890] llce_mb: probe of 43a00000.llce_mb failed with error -13"&lt;BR /&gt;&lt;BR /&gt;&lt;/EM&gt;I uploaded the binaries before doing the build and changed the local.conf as you mentioned (the same procedure I did with the binaries of the LLCE 1.0.9, but at least there the firmware seemed uploaded).&lt;EM&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/EM&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Aug 2025 15:37:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2158431#M14630</guid>
      <dc:creator>MrAlexIV</dc:creator>
      <dc:date>2025-08-26T15:37:29Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 LLCE on GoldVip image</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2159119#M14640</link>
      <description>&lt;P&gt;I fixed the error for the BSP. It was a silly error name in the local.conf.&lt;BR /&gt;Thank you for your support&lt;/P&gt;</description>
      <pubDate>Wed, 27 Aug 2025 10:32:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2159119#M14640</guid>
      <dc:creator>MrAlexIV</dc:creator>
      <dc:date>2025-08-27T10:32:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 LLCE on GoldVip image</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2159128#M14641</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252410"&gt;@MrAlexIV&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Glad to hear that the issue has been fixed&lt;/P&gt;
&lt;P&gt;You are welcome.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Wed, 27 Aug 2025 10:38:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2159128#M14641</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-08-27T10:38:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 LLCE on GoldVip image</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2161995#M14718</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I was able to build the BSP 44 image with the enabling of the LLCE FW.&lt;BR /&gt;Then I was trying to build my YOCTO image starting from the GoldVip base image and the attached local.conf file.&lt;BR /&gt;&lt;BR /&gt;I managed to build the image, but when it is loaded on the SD card and the board is on, no LLCE interfaces appear in ifconfig output. Although, I can see the LLCE interfaces as enabled in the DTS file after the build (attached as well).&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Can you explain how to face with this situation?&lt;BR /&gt;Thank you.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Sep 2025 08:56:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2161995#M14718</guid>
      <dc:creator>MrAlexIV</dc:creator>
      <dc:date>2025-09-02T08:56:56Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 LLCE on GoldVip image</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2162549#M14732</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252410"&gt;@MrAlexIV&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the reply.&lt;/P&gt;
&lt;P&gt;The method provided could be used under pure BSP44, GoldVIP utilize the BSP44 for its A53 side implementation, however, it is a whole reference&lt;SPAN&gt;&amp;nbsp;software for automotive purposes, all CAN uses are managed by the real time cores, therefore adding LLCE-CAN to Linux may not be successful.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I suggest referencing the chapter 14 of GoldVIP User Manual, to get details of how the LLCE-CAN are handled in the GoldVIP.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Wed, 03 Sep 2025 04:20:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2162549#M14732</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-09-03T04:20:56Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 LLCE on GoldVip image</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2391511#M16560</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252410"&gt;@MrAlexIV&lt;/a&gt;. I have the exact same problem. Did you find a solution?&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jul 2026 09:18:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2391511#M16560</guid>
      <dc:creator>GioMusto</dc:creator>
      <dc:date>2026-07-07T09:18:43Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 LLCE on GoldVip image</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2393149#M16585</link>
      <description>&lt;P&gt;tnx 4 post&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jul 2026 15:48:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-LLCE-on-GoldVip-image/m-p/2393149#M16585</guid>
      <dc:creator>lucindaschatz</dc:creator>
      <dc:date>2026-07-09T15:48:25Z</dc:date>
    </item>
  </channel>
</rss>