<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32G3 - FlexCAN Example Build for A53 Core on Linux in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G3-FlexCAN-Example-Build-for-A53-Core-on-Linux/m-p/2159948#M14662</link>
    <description>&lt;P&gt;I update the topic saying that I solved the issued using Goldvip's image.&lt;/P&gt;</description>
    <pubDate>Thu, 28 Aug 2025 12:35:45 GMT</pubDate>
    <dc:creator>MrAlexIV</dc:creator>
    <dc:date>2025-08-28T12:35:45Z</dc:date>
    <item>
      <title>S32G3 - FlexCAN Example Build for A53 Core on Linux</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-FlexCAN-Example-Build-for-A53-Core-on-Linux/m-p/2138498#M14224</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;When I build the FlexCAN example project, I would like to obtain an .elf executable that runs on the &lt;STRONG&gt;A53 cores under Linux&lt;/STRONG&gt;.&lt;BR /&gt;However, the example seems to be designed for the &lt;STRONG&gt;M7 core&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Is there a way to build or adapt the FlexCAN example so that it produces an executable .elf suitable for the A53 cores?&lt;/P&gt;&lt;P&gt;I also tried creating a new Application Project targeting A53 from scratch, but I'm not sure how to &lt;STRONG&gt;reuse or transfer all the FlexCAN configurations&lt;/STRONG&gt; (peripherals, drivers, initialization code, etc.) into this new project.&lt;/P&gt;&lt;P&gt;Could you please guide me on how to achieve this?&lt;/P&gt;</description>
      <pubDate>Tue, 22 Jul 2025 14:38:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-FlexCAN-Example-Build-for-A53-Core-on-Linux/m-p/2138498#M14224</guid>
      <dc:creator>MrAlexIV</dc:creator>
      <dc:date>2025-07-22T14:38:31Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 - FlexCAN Example Build for A53 Core on Linux</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-FlexCAN-Example-Build-for-A53-Core-on-Linux/m-p/2138759#M14227</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252410"&gt;@MrAlexIV&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your question&lt;/P&gt;
&lt;P&gt;With the A53 core running linux the use of modules like gpios, can, etc. is a bit different, instead of passing the values directly with the register like in a baremetal implementation or with an RTD (like with the M7 core). For a linux implementation a driver is needed to pass those values between the OS and the hardware, some of those drivers are already implemented with the BSP distribution that NXP gives.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For the use of CAN with linux you could review the example that is given in the BSP User Manual&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="carlos_o_0-1753226320892.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/348916i047C03101D262F9D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="carlos_o_0-1753226320892.png" alt="carlos_o_0-1753226320892.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;[Linux BSP 44.0 User Manual for S32G2 platforms]&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;the example is writing those commands in the linux console, you could do a C program that use the &lt;EM&gt;system()&amp;nbsp;&lt;/EM&gt;function to send commands and only execute your C code.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Jul 2025 23:25:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-FlexCAN-Example-Build-for-A53-Core-on-Linux/m-p/2138759#M14227</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2025-07-22T23:25:52Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 - FlexCAN Example Build for A53 Core on Linux</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-FlexCAN-Example-Build-for-A53-Core-on-Linux/m-p/2139093#M14242</link>
      <description>&lt;P&gt;Thank you Carlos.&lt;BR /&gt;Ok I got your point. I followed your instructions, but in this way, I can only send and receive between can0 and can1. What I want, it's to receive or send to other device throug a CAN BUS (I have a CAN BUS where I connect all the devices ). With the FlexCan example, I could receive from the other devices, but if I just ldo candump can0, I can't receive the CAN messages from other devices.&lt;BR /&gt;The interface is not in loopback.&lt;BR /&gt;That's why I wanted to get the .elf for A53, because I have already tested the FlexCan example for M7 and it works.&lt;BR /&gt;I can use the simple candump can0 with the system() that you suggested, but it seems that I don't receive CAN messages from other devices.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MrAlexIV_0-1753255421094.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/349026iA4E4745FEDCD1D0E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="MrAlexIV_0-1753255421094.png" alt="MrAlexIV_0-1753255421094.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jul 2025 07:24:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-FlexCAN-Example-Build-for-A53-Core-on-Linux/m-p/2139093#M14242</guid>
      <dc:creator>MrAlexIV</dc:creator>
      <dc:date>2025-07-23T07:24:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 - FlexCAN Example Build for A53 Core on Linux</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-FlexCAN-Example-Build-for-A53-Core-on-Linux/m-p/2139106#M14244</link>
      <description>&lt;P&gt;Also, following the manual (I followed it for S32G3) it talks about J166, J169.....but on my board those Jumpers are not available.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MrAlexIV_0-1753256274840.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/349028i7D29077F56B56863/image-size/medium?v=v2&amp;amp;px=400" role="button" title="MrAlexIV_0-1753256274840.png" alt="MrAlexIV_0-1753256274840.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jul 2025 07:38:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-FlexCAN-Example-Build-for-A53-Core-on-Linux/m-p/2139106#M14244</guid>
      <dc:creator>MrAlexIV</dc:creator>
      <dc:date>2025-07-23T07:38:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 - FlexCAN Example Build for A53 Core on Linux</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-FlexCAN-Example-Build-for-A53-Core-on-Linux/m-p/2141116#M14298</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252410"&gt;@MrAlexIV&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you share which board are you using? the connectors are mentioned in the image I share is for the S32G-VNP-EVB3 with the extension&amp;nbsp;S32GRV-PLATEVB.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 25 Jul 2025 22:25:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-FlexCAN-Example-Build-for-A53-Core-on-Linux/m-p/2141116#M14298</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2025-07-25T22:25:05Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 - FlexCAN Example Build for A53 Core on Linux</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-FlexCAN-Example-Build-for-A53-Core-on-Linux/m-p/2141120#M14299</link>
      <description>&lt;P&gt;Hi, I am using this one&amp;nbsp;&lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/GOLDBOX-3" target="_blank"&gt;https://www.nxp.com/design/design-center/development-boards-and-designs/GOLDBOX-3&lt;/A&gt;&amp;nbsp; &amp;nbsp;(&lt;SPAN&gt;S32G3&amp;nbsp;&lt;/SPAN&gt;)&lt;/P&gt;</description>
      <pubDate>Fri, 25 Jul 2025 22:52:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-FlexCAN-Example-Build-for-A53-Core-on-Linux/m-p/2141120#M14299</guid>
      <dc:creator>MrAlexIV</dc:creator>
      <dc:date>2025-07-25T22:52:46Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 - FlexCAN Example Build for A53 Core on Linux</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-FlexCAN-Example-Build-for-A53-Core-on-Linux/m-p/2142086#M14328</link>
      <description>&lt;P&gt;Thanks for sharing the board you are using.&lt;/P&gt;
&lt;P&gt;For the GoldBox3, you need to enable the can0 and can1 nodes in the device tree. Within these nodes, you can configure which pins to use for CAN output. It’s important to ensure that the selected pins support can0 or can1 output in their SSS.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You could review which pins you could use with the schematic of the board and S32G3_IOMUX.xlsx file that is attached in the reference manual (you need to open the RM with acrobat reader to see the attached files)&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Jul 2025 23:35:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-FlexCAN-Example-Build-for-A53-Core-on-Linux/m-p/2142086#M14328</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2025-07-28T23:35:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 - FlexCAN Example Build for A53 Core on Linux</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-FlexCAN-Example-Build-for-A53-Core-on-Linux/m-p/2159948#M14662</link>
      <description>&lt;P&gt;I update the topic saying that I solved the issued using Goldvip's image.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Aug 2025 12:35:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-FlexCAN-Example-Build-for-A53-Core-on-Linux/m-p/2159948#M14662</guid>
      <dc:creator>MrAlexIV</dc:creator>
      <dc:date>2025-08-28T12:35:45Z</dc:date>
    </item>
  </channel>
</rss>