<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: LLCE LIN interrupt</title>
    <link>https://community.nxp.com/t5/S32G/LLCE-LIN-interrupt/m-p/2159626#M14651</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Yes, thanks for the reply.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The packages I use are:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;1. SW32G_RTD_4.4_5.0.0_QLP03&lt;/P&gt;&lt;P&gt;2. S32G_LLCE_1_0_10&lt;/P&gt;&lt;P&gt;The chip is s32g399a.&lt;/P&gt;</description>
    <pubDate>Thu, 28 Aug 2025 05:54:30 GMT</pubDate>
    <dc:creator>pmboat</dc:creator>
    <dc:date>2025-08-28T05:54:30Z</dc:date>
    <item>
      <title>LLCE LIN interrupt</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-LIN-interrupt/m-p/2158665#M14633</link>
      <description>&lt;P&gt;&lt;SPAN&gt;S32G3 has 4 LLCE lin channels, I configured Lin1 channel as slave and Lin0, 2, 3 as master. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I need to verify the slave's receive response function.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have configured and enabled Lin1's interrupt in EB, the callback function is Lin_CmdFromLlceIsr, when I send a Lin message to Lin1, Lin1 does not enter the interrupt response, only when I enable Lin2 interrupt instead, it can enter the interrupt, Lin1 will give a response at this time, why is this happening?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PixPin_2025-08-27_10-08-37.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/354203i68E8A91E887A669F/image-size/large?v=v2&amp;amp;px=999" role="button" title="PixPin_2025-08-27_10-08-37.png" alt="PixPin_2025-08-27_10-08-37.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PixPin_2025-08-27_10-10-07.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/354204iB7A094FF1F0AE80A/image-size/large?v=v2&amp;amp;px=999" role="button" title="PixPin_2025-08-27_10-10-07.png" alt="PixPin_2025-08-27_10-10-07.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Aug 2025 02:10:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-LIN-interrupt/m-p/2158665#M14633</guid>
      <dc:creator>pmboat</dc:creator>
      <dc:date>2025-08-27T02:10:38Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE LIN interrupt</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-LIN-interrupt/m-p/2159578#M14650</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254160"&gt;@pmboat&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;1. Seems you are working with LLCE LIN? is it right?&lt;/P&gt;
&lt;P&gt;2. Which version RTD/LLCE FW you are working with?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Thu, 28 Aug 2025 04:17:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-LIN-interrupt/m-p/2159578#M14650</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-08-28T04:17:18Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE LIN interrupt</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-LIN-interrupt/m-p/2159626#M14651</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Yes, thanks for the reply.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The packages I use are:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;1. SW32G_RTD_4.4_5.0.0_QLP03&lt;/P&gt;&lt;P&gt;2. S32G_LLCE_1_0_10&lt;/P&gt;&lt;P&gt;The chip is s32g399a.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Aug 2025 05:54:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-LIN-interrupt/m-p/2159626#M14651</guid>
      <dc:creator>pmboat</dc:creator>
      <dc:date>2025-08-28T05:54:30Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE LIN interrupt</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-LIN-interrupt/m-p/2159796#M14654</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/254160"&gt;@pmboat&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your reply.&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;By default, The Lin LLCE firmware is running on the internal CORE 2, so that the LLCE_INT2 is used for LLCE LIN cases.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Chenyin&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 28 Aug 2025 08:55:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-LIN-interrupt/m-p/2159796#M14654</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-08-28T08:55:40Z</dc:date>
    </item>
  </channel>
</rss>