<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 How to creat a S32G FreeRTOS project</title>
    <link>https://community.nxp.com/t5/S32G/How-to-creat-a-S32G-FreeRTOS-project/m-p/1529303#M1461</link>
    <description>&lt;P&gt;Hi, I am trying to compile and use the S32G FreeRTOS project example in S32DS. I am using S32DS version 3.4 , the FreeRTOS for S32G module version 3.0.2 and the RTD module version 3.02 installed. I follow the the installation instructions given in the freertos plugin release notes, install in the order : RTD 3_0_2&amp;nbsp;(SW32G_S32DS_3.4.3_D2112.zip) ,then RTD package (SW32G_RTD_4.4_3.0.2_DS_updatesite_D2203.zip),then FreeRTOS (SW32_FreeRTOS_10_4_6_UOS_3_0_2_DS_updatesite_D2204). I started my FreeRTOS project by customizing the existing demo. But the project did not include the FreeRTOS source code folder.&amp;nbsp;&lt;SPAN&gt;I right click on the project in the Project Explorer window, select S32 Configuration Tools-&amp;gt;Manage SDK Components, I can see the FreeRTOS option in the OS column. But when i chose FreeRTOS option and click OK, it did not work, no FreeRTOS folder appeared in the project directory.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I'm not sure if I missed installing a package, or anything else?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Wed, 28 Sep 2022 07:01:55 GMT</pubDate>
    <dc:creator>yqlau</dc:creator>
    <dc:date>2022-09-28T07:01:55Z</dc:date>
    <item>
      <title>How to creat a S32G FreeRTOS project</title>
      <link>https://community.nxp.com/t5/S32G/How-to-creat-a-S32G-FreeRTOS-project/m-p/1529303#M1461</link>
      <description>&lt;P&gt;Hi, I am trying to compile and use the S32G FreeRTOS project example in S32DS. I am using S32DS version 3.4 , the FreeRTOS for S32G module version 3.0.2 and the RTD module version 3.02 installed. I follow the the installation instructions given in the freertos plugin release notes, install in the order : RTD 3_0_2&amp;nbsp;(SW32G_S32DS_3.4.3_D2112.zip) ,then RTD package (SW32G_RTD_4.4_3.0.2_DS_updatesite_D2203.zip),then FreeRTOS (SW32_FreeRTOS_10_4_6_UOS_3_0_2_DS_updatesite_D2204). I started my FreeRTOS project by customizing the existing demo. But the project did not include the FreeRTOS source code folder.&amp;nbsp;&lt;SPAN&gt;I right click on the project in the Project Explorer window, select S32 Configuration Tools-&amp;gt;Manage SDK Components, I can see the FreeRTOS option in the OS column. But when i chose FreeRTOS option and click OK, it did not work, no FreeRTOS folder appeared in the project directory.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I'm not sure if I missed installing a package, or anything else?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Sep 2022 07:01:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-creat-a-S32G-FreeRTOS-project/m-p/1529303#M1461</guid>
      <dc:creator>yqlau</dc:creator>
      <dc:date>2022-09-28T07:01:55Z</dc:date>
    </item>
    <item>
      <title>Re: How to creat a S32G FreeRTOS project</title>
      <link>https://community.nxp.com/t5/S32G/How-to-creat-a-S32G-FreeRTOS-project/m-p/1529681#M1465</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Could be that you already did it but, Have you generated the code from the GUI configuration tool?&lt;/P&gt;
&lt;P&gt;In the examples provided by the FreeRTOS SDK, you need to first generate the code (pins, clocks, peripherals) in order to create and add everything needed for the project to run.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;This is not so clearly explained in the examples, but has to be done before running the examples.&lt;/P&gt;
&lt;P&gt;Let us know if this helps you or not.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Sep 2022 17:14:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-creat-a-S32G-FreeRTOS-project/m-p/1529681#M1465</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2022-09-28T17:14:20Z</dc:date>
    </item>
  </channel>
</rss>