<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックS32G IPCF LLCE examples</title>
    <link>https://community.nxp.com/t5/S32G/S32G-IPCF-LLCE-examples/m-p/2150759#M14511</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using S32G274A rdb2, S32DS 3.5, LLCE 1.0.9, IPCF&amp;nbsp;SW32G_IPCF_4.10.0_D2405&lt;/P&gt;&lt;P&gt;I checked both Can_Llce_DS_Loopback_S32G274A_M7 , IPCF_Example_S32G274A_M7_0&amp;nbsp; working well.&lt;/P&gt;&lt;P&gt;So I add ipcf module in&amp;nbsp;Can_Llce_DS_Loopback_S32G274A_M7, and configured same as the ipcf example. I also changed the main.c and&amp;nbsp;&lt;SPAN&gt;Linker file as ipcf. (LLCE will not work but my objective is to make ipcf work in CAN LLCE example) &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I also defined "MPU_DISABLE".&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But the same log below is printing&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;[ 22.685977] ipc-shm-sample: starting demo...&lt;BR /&gt;[ 22.686011] ipc-shm-sample: ch 0 &amp;gt;&amp;gt; 20 bytes: SENDING MESSAGES: 10&lt;BR /&gt;[ 22.686024] ipc-shm-sample: send_ctrl_msg(): tx failed on control channel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 12 Aug 2025 08:50:08 GMT</pubDate>
    <dc:creator>chansookang</dc:creator>
    <dc:date>2025-08-12T08:50:08Z</dc:date>
    <item>
      <title>S32G IPCF LLCE examples</title>
      <link>https://community.nxp.com/t5/S32G/S32G-IPCF-LLCE-examples/m-p/2150759#M14511</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using S32G274A rdb2, S32DS 3.5, LLCE 1.0.9, IPCF&amp;nbsp;SW32G_IPCF_4.10.0_D2405&lt;/P&gt;&lt;P&gt;I checked both Can_Llce_DS_Loopback_S32G274A_M7 , IPCF_Example_S32G274A_M7_0&amp;nbsp; working well.&lt;/P&gt;&lt;P&gt;So I add ipcf module in&amp;nbsp;Can_Llce_DS_Loopback_S32G274A_M7, and configured same as the ipcf example. I also changed the main.c and&amp;nbsp;&lt;SPAN&gt;Linker file as ipcf. (LLCE will not work but my objective is to make ipcf work in CAN LLCE example) &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I also defined "MPU_DISABLE".&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But the same log below is printing&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;[ 22.685977] ipc-shm-sample: starting demo...&lt;BR /&gt;[ 22.686011] ipc-shm-sample: ch 0 &amp;gt;&amp;gt; 20 bytes: SENDING MESSAGES: 10&lt;BR /&gt;[ 22.686024] ipc-shm-sample: send_ctrl_msg(): tx failed on control channel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Aug 2025 08:50:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-IPCF-LLCE-examples/m-p/2150759#M14511</guid>
      <dc:creator>chansookang</dc:creator>
      <dc:date>2025-08-12T08:50:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32G IPCF LLCE examples</title>
      <link>https://community.nxp.com/t5/S32G/S32G-IPCF-LLCE-examples/m-p/2150771#M14512</link>
      <description>&lt;P&gt;I checked ipcf working by defining "D_CACHE_ENABLE_NOT" but i am not sure what this will change the operation of LLCE example&lt;/P&gt;</description>
      <pubDate>Tue, 12 Aug 2025 09:04:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-IPCF-LLCE-examples/m-p/2150771#M14512</guid>
      <dc:creator>chansookang</dc:creator>
      <dc:date>2025-08-12T09:04:00Z</dc:date>
    </item>
    <item>
      <title>Re: S32G IPCF LLCE examples</title>
      <link>https://community.nxp.com/t5/S32G/S32G-IPCF-LLCE-examples/m-p/2150817#M14513</link>
      <description>&lt;P&gt;hi，&lt;SPAN&gt;chansookang&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thank you for cantacting us.&lt;/P&gt;
&lt;P&gt;Do you use the multi-core mode for RDB2? Which is the version of BSP are your using?&lt;/P&gt;
&lt;P&gt;And do you use the bootloader to boot both M core and A core?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Tue, 12 Aug 2025 09:50:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-IPCF-LLCE-examples/m-p/2150817#M14513</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2025-08-12T09:50:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32G IPCF LLCE examples</title>
      <link>https://community.nxp.com/t5/S32G/S32G-IPCF-LLCE-examples/m-p/2155556#M14582</link>
      <description>Sorry for late response. I solved it.&lt;BR /&gt;Thank you</description>
      <pubDate>Thu, 21 Aug 2025 00:09:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-IPCF-LLCE-examples/m-p/2155556#M14582</guid>
      <dc:creator>chansookang</dc:creator>
      <dc:date>2025-08-21T00:09:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32G IPCF LLCE examples</title>
      <link>https://community.nxp.com/t5/S32G/S32G-IPCF-LLCE-examples/m-p/2161465#M14696</link>
      <description>&lt;P&gt;I am also facing the same issue what is the solution?&lt;/P&gt;</description>
      <pubDate>Mon, 01 Sep 2025 12:23:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-IPCF-LLCE-examples/m-p/2161465#M14696</guid>
      <dc:creator>honeybee1881</dc:creator>
      <dc:date>2025-09-01T12:23:39Z</dc:date>
    </item>
    <item>
      <title>Re: S32G IPCF LLCE examples</title>
      <link>https://community.nxp.com/t5/S32G/S32G-IPCF-LLCE-examples/m-p/2161922#M14708</link>
      <description>define "D_CACHE_ENABLE_NOT" in preprocessor</description>
      <pubDate>Tue, 02 Sep 2025 07:55:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-IPCF-LLCE-examples/m-p/2161922#M14708</guid>
      <dc:creator>chansookang</dc:creator>
      <dc:date>2025-09-02T07:55:44Z</dc:date>
    </item>
  </channel>
</rss>