<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Question about Yocto build multi BSP version in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Question-about-Yocto-build-multi-BSP-version/m-p/2141493#M14317</link>
    <description>&lt;P&gt;Hi NXP team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For one code base folder with different BSP version&lt;/P&gt;&lt;P&gt;Does the Downloads, sstate-cache and build_s32g399ardb3 folders need to be separated?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My understand that Downloads can be the same, but I'm not sure it will have any risk if sstate-cache and build folder are the same.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;If separation is required, is there any parameter in nxp-setup-alb.sh that can separate them during initialization?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Mon, 28 Jul 2025 07:06:20 GMT</pubDate>
    <dc:creator>GG0712</dc:creator>
    <dc:date>2025-07-28T07:06:20Z</dc:date>
    <item>
      <title>Question about Yocto build multi BSP version</title>
      <link>https://community.nxp.com/t5/S32G/Question-about-Yocto-build-multi-BSP-version/m-p/2141493#M14317</link>
      <description>&lt;P&gt;Hi NXP team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For one code base folder with different BSP version&lt;/P&gt;&lt;P&gt;Does the Downloads, sstate-cache and build_s32g399ardb3 folders need to be separated?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My understand that Downloads can be the same, but I'm not sure it will have any risk if sstate-cache and build folder are the same.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;If separation is required, is there any parameter in nxp-setup-alb.sh that can separate them during initialization?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Mon, 28 Jul 2025 07:06:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Question-about-Yocto-build-multi-BSP-version/m-p/2141493#M14317</guid>
      <dc:creator>GG0712</dc:creator>
      <dc:date>2025-07-28T07:06:20Z</dc:date>
    </item>
    <item>
      <title>Re: Question about Yocto build multi BSP version</title>
      <link>https://community.nxp.com/t5/S32G/Question-about-Yocto-build-multi-BSP-version/m-p/2142169#M14332</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/236748"&gt;@GG0712&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;1. Officially, it is suggested putting different BSP distributions to the different directory for use, since the situation you mentioned is not formally tested.&lt;/P&gt;
&lt;P&gt;2. From my personal experience, in order for saving the size, you may use the same downloads directory, I did not test with the same&amp;nbsp;&lt;SPAN&gt;sstate-cache before, but it is said from the Yocto wiki that:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="chenyin_h_0-1753757230280.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/349841iA4CB48460BA9BD0D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="chenyin_h_0-1753757230280.png" alt="chenyin_h_0-1753757230280.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;chenyin_h_0-1753757230280.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;You may test it and check if it is correct without issues.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Tue, 29 Jul 2025 02:49:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Question-about-Yocto-build-multi-BSP-version/m-p/2142169#M14332</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-07-29T02:49:22Z</dc:date>
    </item>
  </channel>
</rss>