<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックLLCE-PFE example send can failed</title>
    <link>https://community.nxp.com/t5/S32G/LLCE-PFE-example-send-can-failed/m-p/2138915#M14234</link>
    <description>&lt;P&gt;I used the following driver versions to debug the llce_sample_app_pfe example:&lt;BR /&gt;*S32G_LLCE_GATEWAY_1.0.10_D2505&lt;BR /&gt;*SW32G_RTD_4.4_5.0.0_D2410&lt;BR /&gt;*PFE-DRV_S32G_M7_MCAL_1.6.0&lt;BR /&gt;When debugging with Lauterbach Trace32, no CAN messages were transmitted, and the debug interface displayed an ERR (error):&lt;/P&gt;&lt;P&gt;ERR_HM RUNTIME: [C:/NXP/SW32G_RTD_4.4_5.0.0/eclipse/plugins/Eth_43_PFE_TS_T40D11M16I0R0/src/pfe_pe.c:1900] Not enougth memory to copy FW section .messages. Increase option FwMessagesBufferSize to at least 4087.&lt;BR /&gt;ERR_HM RUNTIME: [C:/NXP/SW32G_RTD_4.4_5.0.0/eclipse/plugins/Eth_43_PFE_TS_T40D11M16I0R0/src/pfe_pe.c:1930] Not enougth memory to copy FW section .features. Increase option FwFeaturesBufferSize to at least 3108.&lt;BR /&gt;ERR_HM RUNTIME: [C:/NXP/SW32G_RTD_4.4_5.0.0/eclipse/plugins/Eth_43_PFE_TS_T40D11M16I0R0/src/pfe_class.c:463] Classifier firmware loading the PE failed: 22.&lt;BR /&gt;ERR_HM RUNTIME: [C:/NXP/SW32G_RTD_4.4_5.0.0/eclipse/plugins/Eth_43_PFE_TS_T40D11M16I0R0/src/pfe_platform_master.c:1310] Error during upload of CLASS firmware: 22.&lt;BR /&gt;ERR_HM RUNTIME: [C:/NXP/SW32G_RTD_4.4_5.0.0/eclipse/plugins/Eth_43_PFE_TS_T40D11M16I0R0/src/Eth_PFE_LLD.c:2027] Unable to initialize the platform&lt;BR /&gt;ERR_HM RUNTIME: [C:/NXP/SW32G_RTD_4.4_5.0.0/eclipse/plugins/Eth_43_PFE_TS_T40D11M16I0R0/src/pfe_minihif_drv.c:297] Minihif not initialized&lt;/P&gt;</description>
    <pubDate>Wed, 23 Jul 2025 03:43:43 GMT</pubDate>
    <dc:creator>liu823230301</dc:creator>
    <dc:date>2025-07-23T03:43:43Z</dc:date>
    <item>
      <title>LLCE-PFE example send can failed</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-PFE-example-send-can-failed/m-p/2138915#M14234</link>
      <description>&lt;P&gt;I used the following driver versions to debug the llce_sample_app_pfe example:&lt;BR /&gt;*S32G_LLCE_GATEWAY_1.0.10_D2505&lt;BR /&gt;*SW32G_RTD_4.4_5.0.0_D2410&lt;BR /&gt;*PFE-DRV_S32G_M7_MCAL_1.6.0&lt;BR /&gt;When debugging with Lauterbach Trace32, no CAN messages were transmitted, and the debug interface displayed an ERR (error):&lt;/P&gt;&lt;P&gt;ERR_HM RUNTIME: [C:/NXP/SW32G_RTD_4.4_5.0.0/eclipse/plugins/Eth_43_PFE_TS_T40D11M16I0R0/src/pfe_pe.c:1900] Not enougth memory to copy FW section .messages. Increase option FwMessagesBufferSize to at least 4087.&lt;BR /&gt;ERR_HM RUNTIME: [C:/NXP/SW32G_RTD_4.4_5.0.0/eclipse/plugins/Eth_43_PFE_TS_T40D11M16I0R0/src/pfe_pe.c:1930] Not enougth memory to copy FW section .features. Increase option FwFeaturesBufferSize to at least 3108.&lt;BR /&gt;ERR_HM RUNTIME: [C:/NXP/SW32G_RTD_4.4_5.0.0/eclipse/plugins/Eth_43_PFE_TS_T40D11M16I0R0/src/pfe_class.c:463] Classifier firmware loading the PE failed: 22.&lt;BR /&gt;ERR_HM RUNTIME: [C:/NXP/SW32G_RTD_4.4_5.0.0/eclipse/plugins/Eth_43_PFE_TS_T40D11M16I0R0/src/pfe_platform_master.c:1310] Error during upload of CLASS firmware: 22.&lt;BR /&gt;ERR_HM RUNTIME: [C:/NXP/SW32G_RTD_4.4_5.0.0/eclipse/plugins/Eth_43_PFE_TS_T40D11M16I0R0/src/Eth_PFE_LLD.c:2027] Unable to initialize the platform&lt;BR /&gt;ERR_HM RUNTIME: [C:/NXP/SW32G_RTD_4.4_5.0.0/eclipse/plugins/Eth_43_PFE_TS_T40D11M16I0R0/src/pfe_minihif_drv.c:297] Minihif not initialized&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jul 2025 03:43:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-PFE-example-send-can-failed/m-p/2138915#M14234</guid>
      <dc:creator>liu823230301</dc:creator>
      <dc:date>2025-07-23T03:43:43Z</dc:date>
    </item>
    <item>
      <title>Re: LLCE-PFE example send can failed</title>
      <link>https://community.nxp.com/t5/S32G/LLCE-PFE-example-send-can-failed/m-p/2139793#M14254</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217960"&gt;@liu823230301&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;According to the LLCE1.0.10 release notes, it is tested with RTD5.0.0QLP03(released at 2505), would you mind firstly checking with these version combination?&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="chenyin_h_0-1753328080020.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/349232i5F274F7BF25C12F8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="chenyin_h_0-1753328080020.png" alt="chenyin_h_0-1753328080020.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;chenyin_h_0-1753328080020.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Thu, 24 Jul 2025 03:38:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/LLCE-PFE-example-send-can-failed/m-p/2139793#M14254</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-07-24T03:38:38Z</dc:date>
    </item>
  </channel>
</rss>