<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックQuestion about S32G3 LLCE can2can and can2eth function kernel support version</title>
    <link>https://community.nxp.com/t5/S32G/Question-about-S32G3-LLCE-can2can-and-can2eth-function-kernel/m-p/2134927#M14147</link>
    <description>&lt;P&gt;Hi NXP team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;LLCE CAN controller start to support can2can, can2eth, ...&amp;nbsp; function from BSP38 kernel 5.15&lt;/P&gt;&lt;P&gt;I have lots of questions about this feature.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Does S32G3 Linux kernel 5.10 support these feature?&lt;/LI&gt;&lt;LI&gt;Does can2eth and eth2can support to custom ethernet switch or GMAC eth0 ?&lt;BR /&gt;I can not found how to use in LinuxBSP User Manual&lt;/LI&gt;&lt;LI&gt;Can I use this function without enabling m core?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 16 Jul 2025 10:29:30 GMT</pubDate>
    <dc:creator>GG0712</dc:creator>
    <dc:date>2025-07-16T10:29:30Z</dc:date>
    <item>
      <title>Question about S32G3 LLCE can2can and can2eth function kernel support version</title>
      <link>https://community.nxp.com/t5/S32G/Question-about-S32G3-LLCE-can2can-and-can2eth-function-kernel/m-p/2134927#M14147</link>
      <description>&lt;P&gt;Hi NXP team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;LLCE CAN controller start to support can2can, can2eth, ...&amp;nbsp; function from BSP38 kernel 5.15&lt;/P&gt;&lt;P&gt;I have lots of questions about this feature.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Does S32G3 Linux kernel 5.10 support these feature?&lt;/LI&gt;&lt;LI&gt;Does can2eth and eth2can support to custom ethernet switch or GMAC eth0 ?&lt;BR /&gt;I can not found how to use in LinuxBSP User Manual&lt;/LI&gt;&lt;LI&gt;Can I use this function without enabling m core?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 16 Jul 2025 10:29:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Question-about-S32G3-LLCE-can2can-and-can2eth-function-kernel/m-p/2134927#M14147</guid>
      <dc:creator>GG0712</dc:creator>
      <dc:date>2025-07-16T10:29:30Z</dc:date>
    </item>
    <item>
      <title>Re: Question about S32G3 LLCE can2can and can2eth function kernel support version</title>
      <link>https://community.nxp.com/t5/S32G/Question-about-S32G3-LLCE-can2can-and-can2eth-function-kernel/m-p/2135518#M14157</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/236748"&gt;@GG0712&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;1. No, I checked the code and it is not enabled in BSP38-5.10 kernel.&lt;/P&gt;
&lt;P&gt;2. No, only PFE is supported.&lt;/P&gt;
&lt;P&gt;3. Yes, it is supported, you may reference the LLCE chapter of BSP UM for details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jul 2025 06:50:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Question-about-S32G3-LLCE-can2can-and-can2eth-function-kernel/m-p/2135518#M14157</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-07-17T06:50:28Z</dc:date>
    </item>
  </channel>
</rss>