<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックHow to flash over SSH on S32G3 (GoldBox VIP3), without USB connection</title>
    <link>https://community.nxp.com/t5/S32G/How-to-flash-over-SSH-on-S32G3-GoldBox-VIP3-without-USB/m-p/2129419#M14029</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;I'm currently working with the S32G3 platform (GoldBox VIP 3) and would like to flash remotely via SSH, instead of using a direct USB connection (I am currenlty using S32 Flash Tool with the USB connection).&lt;BR /&gt;Is there any official procedure or tool support for performing the flashing process over SSH (e.g., copying the image and triggering the update remotely)?&lt;/P&gt;&lt;P&gt;I'm specifically interested in:&lt;/P&gt;&lt;P&gt;Flashing the application or boot image without physical access&lt;/P&gt;&lt;P&gt;Whether it's possible to do this via U-Boot, Linux shell, or remote tools&lt;/P&gt;&lt;P&gt;Any security or configuration considerations to be aware of&lt;/P&gt;&lt;P&gt;The system is running Linux and I have SSH access. Any documentation or reference would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
    <pubDate>Mon, 07 Jul 2025 15:18:54 GMT</pubDate>
    <dc:creator>MrAlexIV</dc:creator>
    <dc:date>2025-07-07T15:18:54Z</dc:date>
    <item>
      <title>How to flash over SSH on S32G3 (GoldBox VIP3), without USB connection</title>
      <link>https://community.nxp.com/t5/S32G/How-to-flash-over-SSH-on-S32G3-GoldBox-VIP3-without-USB/m-p/2129419#M14029</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I'm currently working with the S32G3 platform (GoldBox VIP 3) and would like to flash remotely via SSH, instead of using a direct USB connection (I am currenlty using S32 Flash Tool with the USB connection).&lt;BR /&gt;Is there any official procedure or tool support for performing the flashing process over SSH (e.g., copying the image and triggering the update remotely)?&lt;/P&gt;&lt;P&gt;I'm specifically interested in:&lt;/P&gt;&lt;P&gt;Flashing the application or boot image without physical access&lt;/P&gt;&lt;P&gt;Whether it's possible to do this via U-Boot, Linux shell, or remote tools&lt;/P&gt;&lt;P&gt;Any security or configuration considerations to be aware of&lt;/P&gt;&lt;P&gt;The system is running Linux and I have SSH access. Any documentation or reference would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jul 2025 15:18:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-flash-over-SSH-on-S32G3-GoldBox-VIP3-without-USB/m-p/2129419#M14029</guid>
      <dc:creator>MrAlexIV</dc:creator>
      <dc:date>2025-07-07T15:18:54Z</dc:date>
    </item>
    <item>
      <title>Re: How to flash over SSH on S32G3 (GoldBox VIP3), without USB connection</title>
      <link>https://community.nxp.com/t5/S32G/How-to-flash-over-SSH-on-S32G3-GoldBox-VIP3-without-USB/m-p/2130378#M14038</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252410"&gt;@MrAlexIV&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for you post&lt;/P&gt;
&lt;P&gt;ssh is not support by U-boot, what you could do is flash it via TFTP, please review the &lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN13727.pdf" target="_self"&gt;AN13727 Flashing Binaries to S32G-VNP-RDB3 Board&lt;/A&gt;&amp;nbsp;at chapter&amp;nbsp;2.3.2. Flashing image into eMMC via u-boot and&amp;nbsp;2.4. Flashing image with SD card-less&lt;/P&gt;</description>
      <pubDate>Tue, 08 Jul 2025 20:33:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/How-to-flash-over-SSH-on-S32G3-GoldBox-VIP3-without-USB/m-p/2130378#M14038</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2025-07-08T20:33:42Z</dc:date>
    </item>
  </channel>
</rss>