<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックS32G Bootable SD Card Setup – BSP Version Clarification Needed</title>
    <link>https://community.nxp.com/t5/S32G/S32G-Bootable-SD-Card-Setup-BSP-Version-Clarification-Needed/m-p/2122961#M13901</link>
    <description>&lt;P&gt;I'm trying to find the correct Linux BSP for the S32G platform.&lt;BR /&gt;I want to create a bootable SD card for the S32G-VNP-RDB2 board.&lt;BR /&gt;However, on the software download page, only Linux BSP 23.5 is available.&lt;BR /&gt;From what I understand, Linux BSP 23.5 seems to be intended for S32V series, not for S32G.&lt;BR /&gt;Where can I download the appropriate Linux BSP for the S32G platform?&lt;BR /&gt;Also, is it possible to use Linux BSP 23.5 to boot an S32G board?&lt;BR /&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 25 Jun 2025 08:27:45 GMT</pubDate>
    <dc:creator>yonghwa_seo</dc:creator>
    <dc:date>2025-06-25T08:27:45Z</dc:date>
    <item>
      <title>S32G Bootable SD Card Setup – BSP Version Clarification Needed</title>
      <link>https://community.nxp.com/t5/S32G/S32G-Bootable-SD-Card-Setup-BSP-Version-Clarification-Needed/m-p/2122961#M13901</link>
      <description>&lt;P&gt;I'm trying to find the correct Linux BSP for the S32G platform.&lt;BR /&gt;I want to create a bootable SD card for the S32G-VNP-RDB2 board.&lt;BR /&gt;However, on the software download page, only Linux BSP 23.5 is available.&lt;BR /&gt;From what I understand, Linux BSP 23.5 seems to be intended for S32V series, not for S32G.&lt;BR /&gt;Where can I download the appropriate Linux BSP for the S32G platform?&lt;BR /&gt;Also, is it possible to use Linux BSP 23.5 to boot an S32G board?&lt;BR /&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jun 2025 08:27:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-Bootable-SD-Card-Setup-BSP-Version-Clarification-Needed/m-p/2122961#M13901</guid>
      <dc:creator>yonghwa_seo</dc:creator>
      <dc:date>2025-06-25T08:27:45Z</dc:date>
    </item>
    <item>
      <title>Re: S32G Bootable SD Card Setup – BSP Version Clarification Needed</title>
      <link>https://community.nxp.com/t5/S32G/S32G-Bootable-SD-Card-Setup-BSP-Version-Clarification-Needed/m-p/2123263#M13906</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252031"&gt;@yonghwa_seo&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;No, it is not for the S32G product.&lt;/P&gt;
&lt;P&gt;For downloading the BSP images, it is suggested accessing the following URL:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/app-autopackagemgr/automotive-software-package-manager:AUTO-SW-PACKAGE-MANAGER" target="_blank"&gt;https://www.nxp.com/app-autopackagemgr/automotive-software-package-manager:AUTO-SW-PACKAGE-MANAGER&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="chenyin_h_0-1750862973255.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/344663i1039903B5F03CF1F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="chenyin_h_0-1750862973255.png" alt="chenyin_h_0-1750862973255.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Some other BSP version listed could also be downloaded via this page, I hope it will help.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jun 2025 14:50:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-Bootable-SD-Card-Setup-BSP-Version-Clarification-Needed/m-p/2123263#M13906</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-06-25T14:50:47Z</dc:date>
    </item>
  </channel>
</rss>