<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Error from DDR tool in project based on S32G3</title>
    <link>https://community.nxp.com/t5/S32G/Error-from-DDR-tool-in-project-based-on-S32G3/m-p/1515596#M1378</link>
    <description>&lt;P&gt;I'm trying to use DDR tool to bring up DDR4&amp;nbsp;MT53D512M32D2DS on our board with S32G3 MCU. I set chip in serial boot mode and try to run "Firmware Init test", but tool finishs the process with Fail. I attached log to the post.&lt;/P&gt;&lt;P&gt;What is the reason for such kind of error?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
    <pubDate>Thu, 01 Sep 2022 12:32:28 GMT</pubDate>
    <dc:creator>Gonchar</dc:creator>
    <dc:date>2022-09-01T12:32:28Z</dc:date>
    <item>
      <title>Error from DDR tool in project based on S32G3</title>
      <link>https://community.nxp.com/t5/S32G/Error-from-DDR-tool-in-project-based-on-S32G3/m-p/1515596#M1378</link>
      <description>&lt;P&gt;I'm trying to use DDR tool to bring up DDR4&amp;nbsp;MT53D512M32D2DS on our board with S32G3 MCU. I set chip in serial boot mode and try to run "Firmware Init test", but tool finishs the process with Fail. I attached log to the post.&lt;/P&gt;&lt;P&gt;What is the reason for such kind of error?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Thu, 01 Sep 2022 12:32:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Error-from-DDR-tool-in-project-based-on-S32G3/m-p/1515596#M1378</guid>
      <dc:creator>Gonchar</dc:creator>
      <dc:date>2022-09-01T12:32:28Z</dc:date>
    </item>
    <item>
      <title>Re: Error from DDR tool in project based on S32G3</title>
      <link>https://community.nxp.com/t5/S32G/Error-from-DDR-tool-in-project-based-on-S32G3/m-p/1530415#M1474</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/204136"&gt;@Gonchar&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Hope you are doing good.&lt;/P&gt;
&lt;P&gt;The issue seems in the serial module as the script accepts data serially and converts it into base 10.&lt;/P&gt;
&lt;P&gt;Can you please check that "0xmw340000" was sent properly over serial communication? Are any changes are done on the board side?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Mayank s Patel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Sep 2022 12:02:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Error-from-DDR-tool-in-project-based-on-S32G3/m-p/1530415#M1474</guid>
      <dc:creator>MayanksPatel</dc:creator>
      <dc:date>2022-09-29T12:02:32Z</dc:date>
    </item>
  </channel>
</rss>