<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Request for Full Yocto BSP Source Access</title>
    <link>https://community.nxp.com/t5/S32G/Request-for-Full-Yocto-BSP-Source-Access/m-p/2117858#M13767</link>
    <description>&lt;P&gt;After running repo init &amp;amp; repo sync on release/bsp39.0 or bsp44.0, I’m missing access to some required private sources during bitbake (kernel, ddr firmware, hse firmware…).&lt;BR /&gt;The previous repo (bsp38.0) worked fine, but newer releases seem to require NDA or additional access to NXP private repositories.&lt;BR /&gt;May I request full access to the complete BSP sources for Yocto S32G3 for version 39.0 or 44.0?&lt;BR /&gt;This is blocking bitbake fetch steps due to missing SRC_URI sources.&lt;/P&gt;</description>
    <pubDate>Tue, 17 Jun 2025 14:11:26 GMT</pubDate>
    <dc:creator>NancyW</dc:creator>
    <dc:date>2025-06-17T14:11:26Z</dc:date>
    <item>
      <title>Request for Full Yocto BSP Source Access</title>
      <link>https://community.nxp.com/t5/S32G/Request-for-Full-Yocto-BSP-Source-Access/m-p/2117858#M13767</link>
      <description>&lt;P&gt;After running repo init &amp;amp; repo sync on release/bsp39.0 or bsp44.0, I’m missing access to some required private sources during bitbake (kernel, ddr firmware, hse firmware…).&lt;BR /&gt;The previous repo (bsp38.0) worked fine, but newer releases seem to require NDA or additional access to NXP private repositories.&lt;BR /&gt;May I request full access to the complete BSP sources for Yocto S32G3 for version 39.0 or 44.0?&lt;BR /&gt;This is blocking bitbake fetch steps due to missing SRC_URI sources.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jun 2025 14:11:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Request-for-Full-Yocto-BSP-Source-Access/m-p/2117858#M13767</guid>
      <dc:creator>NancyW</dc:creator>
      <dc:date>2025-06-17T14:11:26Z</dc:date>
    </item>
    <item>
      <title>Re: Request for Full Yocto BSP Source Access</title>
      <link>https://community.nxp.com/t5/S32G/Request-for-Full-Yocto-BSP-Source-Access/m-p/2118100#M13769</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/249830"&gt;@NancyW&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could provide which version of Linux are you using? Also, Is it a native environment or an emulated?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jun 2025 22:58:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Request-for-Full-Yocto-BSP-Source-Access/m-p/2118100#M13769</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2025-06-17T22:58:05Z</dc:date>
    </item>
    <item>
      <title>Re: Request for Full Yocto BSP Source Access</title>
      <link>https://community.nxp.com/t5/S32G/Request-for-Full-Yocto-BSP-Source-Access/m-p/2118351#M13775</link>
      <description>&lt;P&gt;Hi how are you,&lt;/P&gt;&lt;P&gt;I'm using a Linux Ubuntu VM&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jun 2025 07:56:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Request-for-Full-Yocto-BSP-Source-Access/m-p/2118351#M13775</guid>
      <dc:creator>NancyW</dc:creator>
      <dc:date>2025-06-18T07:56:53Z</dc:date>
    </item>
    <item>
      <title>Re: Request for Full Yocto BSP Source Access</title>
      <link>https://community.nxp.com/t5/S32G/Request-for-Full-Yocto-BSP-Source-Access/m-p/2118882#M13786</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/249830"&gt;@NancyW&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The BSP Source Access is public, so you don't need to have any credentials to build your Yocto project.&lt;/P&gt;
&lt;P&gt;the bitbake command have some error in virtual environments if does not have enough RAM assigned, could you please verify the RAM assigned to your virtual machine?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also, could you share which version of Ubuntu are you using? (Ex: Ubuntu 22.04)&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jun 2025 21:42:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Request-for-Full-Yocto-BSP-Source-Access/m-p/2118882#M13786</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2025-06-18T21:42:00Z</dc:date>
    </item>
    <item>
      <title>Re: Request for Full Yocto BSP Source Access</title>
      <link>https://community.nxp.com/t5/S32G/Request-for-Full-Yocto-BSP-Source-Access/m-p/2119234#M13791</link>
      <description>Hi,&lt;BR /&gt;Thank you for your feedback.&lt;BR /&gt;I’ve currently allocated 6 GB of RAM (out of 8 GB total) to the virtual machine.&lt;BR /&gt;Also, I had previously worked on a Poky-based Yocto project — maybe that could be affecting the current setup. For reference, I’m using Ubuntu 22.04.5.</description>
      <pubDate>Thu, 19 Jun 2025 08:44:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Request-for-Full-Yocto-BSP-Source-Access/m-p/2119234#M13791</guid>
      <dc:creator>NancyW</dc:creator>
      <dc:date>2025-06-19T08:44:38Z</dc:date>
    </item>
    <item>
      <title>Re: Request for Full Yocto BSP Source Access</title>
      <link>https://community.nxp.com/t5/S32G/Request-for-Full-Yocto-BSP-Source-Access/m-p/2120313#M13815</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/249830"&gt;@NancyW&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;At the Yocto project documentation the requirements are at least 8GB of RAM in this case assigned to your virtual machine, so I cannot ensure it will work.&lt;/P&gt;
&lt;P&gt;I can suggest is to&amp;nbsp;set BB_NUMBER_THREADS and PARALLEL_MAKE this to make the build use lower resources of your machine (it will include cores).&lt;/P&gt;
&lt;P&gt;Just add this lines to your file [your_yocto_build_dir]/conf/local.conf&lt;/P&gt;
&lt;P&gt;BB_NUMBER_THREADS = "2"&lt;BR /&gt;PARALLEL_MAKE = "-j 2"&lt;/P&gt;
&lt;P&gt;And change the number 2 for the number that fits to your system. Remember, lower number slow down the Yocto building. Higher number increase Yocto build but can starve all other process in your machine.&lt;/P&gt;
&lt;P&gt;After the change local.conf, move to Yocto base dir and run command source setup-environment ./your_build_folder&lt;/P&gt;</description>
      <pubDate>Fri, 20 Jun 2025 17:27:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Request-for-Full-Yocto-BSP-Source-Access/m-p/2120313#M13815</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2025-06-20T17:27:26Z</dc:date>
    </item>
  </channel>
</rss>