<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Compatibility of S32G399A-RDB3 BSP Image with GoldBox 3 in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Compatibility-of-S32G399A-RDB3-BSP-Image-with-GoldBox-3/m-p/2115432#M13718</link>
    <description>&lt;P&gt;Hi all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have been working with the S32G399A-RDB3 board and have built a custom Yocto image based on your provided BSP, with some modifications.&lt;/P&gt;&lt;P&gt;I've purchased the S32G-VNP-GLDBOX3 &amp;nbsp;board and would like to confirm the following:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Can I use the same Yocto BSP and image that I built for the S32G399A-RDB3 directly on the GoldBox 3?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Are there any differences in device trees, hardware configurations (e.g., Ethernet PHYs, PMICs, USB transceivers), or bootloader settings that I should be aware of?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Do you provide a separate BSP or machine configuration specific to GoldBox 3?&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I would appreciate your guidance to ensure a smooth transition without compatibility issues.&lt;/P&gt;</description>
    <pubDate>Thu, 12 Jun 2025 13:14:07 GMT</pubDate>
    <dc:creator>MohamedAbdelslam</dc:creator>
    <dc:date>2025-06-12T13:14:07Z</dc:date>
    <item>
      <title>Compatibility of S32G399A-RDB3 BSP Image with GoldBox 3</title>
      <link>https://community.nxp.com/t5/S32G/Compatibility-of-S32G399A-RDB3-BSP-Image-with-GoldBox-3/m-p/2115432#M13718</link>
      <description>&lt;P&gt;Hi all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have been working with the S32G399A-RDB3 board and have built a custom Yocto image based on your provided BSP, with some modifications.&lt;/P&gt;&lt;P&gt;I've purchased the S32G-VNP-GLDBOX3 &amp;nbsp;board and would like to confirm the following:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Can I use the same Yocto BSP and image that I built for the S32G399A-RDB3 directly on the GoldBox 3?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Are there any differences in device trees, hardware configurations (e.g., Ethernet PHYs, PMICs, USB transceivers), or bootloader settings that I should be aware of?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Do you provide a separate BSP or machine configuration specific to GoldBox 3?&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I would appreciate your guidance to ensure a smooth transition without compatibility issues.&lt;/P&gt;</description>
      <pubDate>Thu, 12 Jun 2025 13:14:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Compatibility-of-S32G399A-RDB3-BSP-Image-with-GoldBox-3/m-p/2115432#M13718</guid>
      <dc:creator>MohamedAbdelslam</dc:creator>
      <dc:date>2025-06-12T13:14:07Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility of S32G399A-RDB3 BSP Image with GoldBox 3</title>
      <link>https://community.nxp.com/t5/S32G/Compatibility-of-S32G399A-RDB3-BSP-Image-with-GoldBox-3/m-p/2115783#M13728</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/240662"&gt;@MohamedAbdelslam&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the post.&lt;/P&gt;
&lt;P&gt;1. Yes, if your modified BSP images work fine on RDB3, then they could be used on GoldBOX3 correctly.&lt;/P&gt;
&lt;P&gt;2. No differences from my understanding.&lt;/P&gt;
&lt;P&gt;3. As what I have mentioned, the same BSP images could be used for RDB3 and GoldBOX3.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Jun 2025 02:41:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Compatibility-of-S32G399A-RDB3-BSP-Image-with-GoldBox-3/m-p/2115783#M13728</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-06-13T02:41:09Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility of S32G399A-RDB3 BSP Image with GoldBox 3</title>
      <link>https://community.nxp.com/t5/S32G/Compatibility-of-S32G399A-RDB3-BSP-Image-with-GoldBox-3/m-p/2116454#M13740</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Chenyin,&amp;nbsp;&lt;BR /&gt;thanks for your answer&lt;BR /&gt;I understand that flashing images is also the same way as flashing on s32g399ardb3 ( I mean the flashing methodology (switches configurations and s32 flash tool and so on)&amp;nbsp;&lt;BR /&gt;is that right?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 15 Jun 2025 14:41:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Compatibility-of-S32G399A-RDB3-BSP-Image-with-GoldBox-3/m-p/2116454#M13740</guid>
      <dc:creator>MohamedAbdelslam</dc:creator>
      <dc:date>2025-06-15T14:41:09Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility of S32G399A-RDB3 BSP Image with GoldBox 3</title>
      <link>https://community.nxp.com/t5/S32G/Compatibility-of-S32G399A-RDB3-BSP-Image-with-GoldBox-3/m-p/2116509#M13741</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/240662"&gt;@MohamedAbdelslam&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your reply.&lt;/P&gt;
&lt;P&gt;Yes, it is correct.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Mon, 16 Jun 2025 02:26:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Compatibility-of-S32G399A-RDB3-BSP-Image-with-GoldBox-3/m-p/2116509#M13741</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-06-16T02:26:10Z</dc:date>
    </item>
  </channel>
</rss>