<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックSAF eMCEM - Normal Operation Faults - S32G3</title>
    <link>https://community.nxp.com/t5/S32G/SAF-eMCEM-Normal-Operation-Faults-S32G3/m-p/2114114#M13686</link>
    <description>&lt;P&gt;Hello team!&lt;/P&gt;&lt;P&gt;I'm currently working on integrating SAF into BSW. While referring the eMCEM Safety Manual, there are 300+ S32G3 Faults listed.&lt;/P&gt;&lt;P&gt;1) Wanted to know if we are supposed to handle all of them?&lt;/P&gt;&lt;P&gt;2) If we can shortlist them, on what basis has it to be done?&lt;/P&gt;&lt;P&gt;3) On what basis do we forward them to either the Alarm Handler or the NMI Handler?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'd really appreciate if anyone could help me out.&lt;BR /&gt;Thank you!&lt;/P&gt;</description>
    <pubDate>Wed, 11 Jun 2025 04:30:27 GMT</pubDate>
    <dc:creator>SHIVRAJ</dc:creator>
    <dc:date>2025-06-11T04:30:27Z</dc:date>
    <item>
      <title>SAF eMCEM - Normal Operation Faults - S32G3</title>
      <link>https://community.nxp.com/t5/S32G/SAF-eMCEM-Normal-Operation-Faults-S32G3/m-p/2114114#M13686</link>
      <description>&lt;P&gt;Hello team!&lt;/P&gt;&lt;P&gt;I'm currently working on integrating SAF into BSW. While referring the eMCEM Safety Manual, there are 300+ S32G3 Faults listed.&lt;/P&gt;&lt;P&gt;1) Wanted to know if we are supposed to handle all of them?&lt;/P&gt;&lt;P&gt;2) If we can shortlist them, on what basis has it to be done?&lt;/P&gt;&lt;P&gt;3) On what basis do we forward them to either the Alarm Handler or the NMI Handler?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'd really appreciate if anyone could help me out.&lt;BR /&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Wed, 11 Jun 2025 04:30:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/SAF-eMCEM-Normal-Operation-Faults-S32G3/m-p/2114114#M13686</guid>
      <dc:creator>SHIVRAJ</dc:creator>
      <dc:date>2025-06-11T04:30:27Z</dc:date>
    </item>
    <item>
      <title>Re: SAF eMCEM - Normal Operation Faults - S32G3</title>
      <link>https://community.nxp.com/t5/S32G/SAF-eMCEM-Normal-Operation-Faults-S32G3/m-p/2114917#M13701</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/251448"&gt;@SHIVRAJ&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;1.&amp;nbsp;&lt;SPAN class="fontstyle0"&gt;The fault tables you mentioned present the FCCU fault symbolic names and their mapping to the NCFs of the S32G devices. It also contains the EIM channels. &lt;/SPAN&gt;&lt;SPAN class="fontstyle0"&gt;These EIM defines are valid for fault injection, which are not for fault reporting, so these&amp;nbsp;EMCEM_FCCU* faults need to be handled.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;2. FCCU can be configured to enter Alarm state when a fault is detected. In Alarm state, eMCEM module identifies which fault source or sources are active and calls a fault handler registered by the user for that source or sources.&amp;nbsp;&lt;/SPAN&gt;&lt;LI-WRAPPER&gt;&lt;SPAN class="fontstyle0"&gt;When the fault handler does not recover the fault before the alarm timeout interval expires, or when no fault handler is available, FCCU enters Fault State and generates a non-maskable interrupt. eMCEM module handles this interrupt and call Software Recovery (sReco) component in S32 SAF to records the fault information and issues a software functional reset.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/LI-WRAPPER&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Chenyin&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Jun 2025 03:00:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/SAF-eMCEM-Normal-Operation-Faults-S32G3/m-p/2114917#M13701</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-06-12T03:00:19Z</dc:date>
    </item>
  </channel>
</rss>