<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SAF Scheck Runtime Test - S32G3 in S32G</title>
    <link>https://community.nxp.com/t5/S32G/SAF-Scheck-Runtime-Test-S32G3/m-p/2109141#M13628</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242921"&gt;@Harish_R&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the reply.&lt;/P&gt;
&lt;P&gt;From my understanding, the&amp;nbsp;&lt;SPAN&gt;eMCEM module is used to&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;configure the reaction to the safety faults detected in the system; the sCheck could be used for testing&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;latent faults within the hardware safety mechanisms, when there would be errors, they would be automatically reported to the FCCU(Which is&amp;nbsp;&lt;SPAN class="fontstyle0"&gt;HW transition&lt;/SPAN&gt;).&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Chenyin&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 03 Jun 2025 05:51:16 GMT</pubDate>
    <dc:creator>chenyin_h</dc:creator>
    <dc:date>2025-06-03T05:51:16Z</dc:date>
    <item>
      <title>SAF Scheck Runtime Test - S32G3</title>
      <link>https://community.nxp.com/t5/S32G/SAF-Scheck-Runtime-Test-S32G3/m-p/2107034#M13597</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;im trying to integrate SAF into basic software referring to SAF user and integration manual. was checking to perform scheck tests during runtime. is it really necessary to perform scheck test during runtime.?&amp;nbsp;&lt;/P&gt;&lt;P&gt;is there any suggestion or recommendation to perform Scheck in runtime&lt;/P&gt;&lt;P&gt;Br,&lt;/P&gt;&lt;P&gt;Harish R&lt;/P&gt;</description>
      <pubDate>Thu, 29 May 2025 09:14:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/SAF-Scheck-Runtime-Test-S32G3/m-p/2107034#M13597</guid>
      <dc:creator>Harish_R</dc:creator>
      <dc:date>2025-05-29T09:14:46Z</dc:date>
    </item>
    <item>
      <title>Re: SAF Scheck Runtime Test - S32G3</title>
      <link>https://community.nxp.com/t5/S32G/SAF-Scheck-Runtime-Test-S32G3/m-p/2107585#M13604</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242921"&gt;@Harish_R&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the post.&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;From my understanding, it is necessary. During runtime, the configuration of the safety context should be checked to detect latent faults. These are typically found in the configuration of safety mechanisms.&amp;nbsp;&lt;/SPAN&gt;&lt;LI-WRAPPER&gt;&lt;SPAN class="fontstyle0"&gt;The S32 SAF SquareCheck module provides a number of tests that can be scheduled to run during runtime. Execution of the SquareCheck tests during runtime is the responsibility of the application software.&amp;nbsp;&lt;/SPAN&gt;&lt;/LI-WRAPPER&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;For testing it runtime, I think the chapter3.5 of sCheck UM could be a useful reference.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Chenyin&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 30 May 2025 03:04:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/SAF-Scheck-Runtime-Test-S32G3/m-p/2107585#M13604</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-05-30T03:04:58Z</dc:date>
    </item>
    <item>
      <title>Re: SAF Scheck Runtime Test - S32G3</title>
      <link>https://community.nxp.com/t5/S32G/SAF-Scheck-Runtime-Test-S32G3/m-p/2108423#M13616</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/24163"&gt;@chenyin_h&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Thanks for the info. i was going the UM and few points were not clear to me.&lt;/P&gt;&lt;P&gt;1. is Scheck reporting faults to FCCU?? but configuration side im not configuring any scheck fault reaction.&lt;/P&gt;&lt;P&gt;2. in eMCEM module all the faults are configured for necessary reactions. which module is actually reporting faults??&amp;nbsp;&lt;/P&gt;&lt;P&gt;if i could more info on this it would be helpful for understanding.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Harish R&lt;/P&gt;</description>
      <pubDate>Mon, 02 Jun 2025 05:50:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/SAF-Scheck-Runtime-Test-S32G3/m-p/2108423#M13616</guid>
      <dc:creator>Harish_R</dc:creator>
      <dc:date>2025-06-02T05:50:16Z</dc:date>
    </item>
    <item>
      <title>Re: SAF Scheck Runtime Test - S32G3</title>
      <link>https://community.nxp.com/t5/S32G/SAF-Scheck-Runtime-Test-S32G3/m-p/2109141#M13628</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242921"&gt;@Harish_R&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the reply.&lt;/P&gt;
&lt;P&gt;From my understanding, the&amp;nbsp;&lt;SPAN&gt;eMCEM module is used to&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;configure the reaction to the safety faults detected in the system; the sCheck could be used for testing&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;latent faults within the hardware safety mechanisms, when there would be errors, they would be automatically reported to the FCCU(Which is&amp;nbsp;&lt;SPAN class="fontstyle0"&gt;HW transition&lt;/SPAN&gt;).&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;BR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Chenyin&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 03 Jun 2025 05:51:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/SAF-Scheck-Runtime-Test-S32G3/m-p/2109141#M13628</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-06-03T05:51:16Z</dc:date>
    </item>
    <item>
      <title>Re: SAF Scheck Runtime Test - S32G3</title>
      <link>https://community.nxp.com/t5/S32G/SAF-Scheck-Runtime-Test-S32G3/m-p/2110040#M13636</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/24163"&gt;@chenyin_h&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the info.&amp;nbsp;&lt;/P&gt;&lt;P&gt;so, if in case if im not performing scheck in runtime. what would be the impact?&lt;/P&gt;&lt;P&gt;would still the errors be reported by HW?? to take necessary reactions?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Harish R&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jun 2025 05:22:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/SAF-Scheck-Runtime-Test-S32G3/m-p/2110040#M13636</guid>
      <dc:creator>Harish_R</dc:creator>
      <dc:date>2025-06-04T05:22:08Z</dc:date>
    </item>
    <item>
      <title>Re: SAF Scheck Runtime Test - S32G3</title>
      <link>https://community.nxp.com/t5/S32G/SAF-Scheck-Runtime-Test-S32G3/m-p/2110321#M13640</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242921"&gt;@Harish_R&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your reply.&lt;/P&gt;
&lt;P&gt;Yes, from my understanding, the sCheck tests may inject some errors, and then they could be captured by FCCU, if no sCheck running, instead, when there would be errors caused by other software/hardware issues, if the corresponding reactions had been set before(for example, via eMCEM), then the necessary reaction would also be taken.&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jun 2025 09:47:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/SAF-Scheck-Runtime-Test-S32G3/m-p/2110321#M13640</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-06-04T09:47:24Z</dc:date>
    </item>
  </channel>
</rss>