<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックS32G3-NAD or Modem</title>
    <link>https://community.nxp.com/t5/S32G/S32G3-NAD-or-Modem/m-p/2101444#M13523</link>
    <description>&lt;P&gt;&lt;SPAN class=""&gt;Hi,&lt;BR /&gt;Does The NXP S32G399A-RDB3 development board include a built-in cellular modem or Network Access Device (NAD)?&lt;BR /&gt;If not, does it provide expansion options to add one?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 21 May 2025 09:03:32 GMT</pubDate>
    <dc:creator>MohamedAbdelslam</dc:creator>
    <dc:date>2025-05-21T09:03:32Z</dc:date>
    <item>
      <title>S32G3-NAD or Modem</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-NAD-or-Modem/m-p/2101444#M13523</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;Hi,&lt;BR /&gt;Does The NXP S32G399A-RDB3 development board include a built-in cellular modem or Network Access Device (NAD)?&lt;BR /&gt;If not, does it provide expansion options to add one?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 21 May 2025 09:03:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-NAD-or-Modem/m-p/2101444#M13523</guid>
      <dc:creator>MohamedAbdelslam</dc:creator>
      <dc:date>2025-05-21T09:03:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3-NAD or Modem</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-NAD-or-Modem/m-p/2101536#M13527</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/240662"&gt;@MohamedAbdelslam&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Thanks for the post.&lt;/P&gt;
&lt;P&gt;The RDB3 provides the following network connectors, but not including built-in modems.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="chenyin_h_0-1747823221373.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/338968iCC60E7AD89867FDB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="chenyin_h_0-1747823221373.png" alt="chenyin_h_0-1747823221373.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;There are M.2, PCIe, USB, etc. exist on the RDB3, from my experience, devices like WIFI module, LTE/5G module could be connected to the board.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 21 May 2025 10:32:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-NAD-or-Modem/m-p/2101536#M13527</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-05-21T10:32:08Z</dc:date>
    </item>
  </channel>
</rss>