<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックPTP using RTD GMAC Driver</title>
    <link>https://community.nxp.com/t5/S32G/PTP-using-RTD-GMAC-Driver/m-p/2085944#M13300</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;I'm trying to setup the S32G GMAC0 as a ptp master on the M7 cores.&lt;BR /&gt;I'm using RTD driver for GMAC. I could find the function to enable timestamping and correcting the clock but I couldn't find any function related to enabling PTP offloading.&lt;BR /&gt;&lt;BR /&gt;Is there an RTD driver that allows that, or do I have to manually setup the various registers.&lt;BR /&gt;If so can you give me the list of register to set to make it act as a ptp master ?&lt;BR /&gt;&lt;BR /&gt;Best regards&lt;/P&gt;</description>
    <pubDate>Wed, 23 Apr 2025 21:23:27 GMT</pubDate>
    <dc:creator>yanis-waabi</dc:creator>
    <dc:date>2025-04-23T21:23:27Z</dc:date>
    <item>
      <title>PTP using RTD GMAC Driver</title>
      <link>https://community.nxp.com/t5/S32G/PTP-using-RTD-GMAC-Driver/m-p/2085944#M13300</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I'm trying to setup the S32G GMAC0 as a ptp master on the M7 cores.&lt;BR /&gt;I'm using RTD driver for GMAC. I could find the function to enable timestamping and correcting the clock but I couldn't find any function related to enabling PTP offloading.&lt;BR /&gt;&lt;BR /&gt;Is there an RTD driver that allows that, or do I have to manually setup the various registers.&lt;BR /&gt;If so can you give me the list of register to set to make it act as a ptp master ?&lt;BR /&gt;&lt;BR /&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Wed, 23 Apr 2025 21:23:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/PTP-using-RTD-GMAC-Driver/m-p/2085944#M13300</guid>
      <dc:creator>yanis-waabi</dc:creator>
      <dc:date>2025-04-23T21:23:27Z</dc:date>
    </item>
    <item>
      <title>Re: PTP using RTD GMAC Driver</title>
      <link>https://community.nxp.com/t5/S32G/PTP-using-RTD-GMAC-Driver/m-p/2086039#M13301</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245960"&gt;@yanis-waabi&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thanks for your question.&lt;/P&gt;
&lt;P&gt;You could find a Reference Software of the&amp;nbsp;&lt;STRONG&gt;Automotive SW - S32G - gPTP Stack&amp;nbsp;&lt;/STRONG&gt;at Flexera, the package you have an example that has a function to initialize the PTP Stack&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="carlos_o_0-1745449144476.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/334562i3E3F1FA5A9E96C7A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="carlos_o_0-1745449144476.png" alt="carlos_o_0-1745449144476.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;carlos_o_0-1745449144476.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Also refers to the&amp;nbsp;&lt;STRONG&gt;gPTP S32G User Manual&amp;nbsp;&lt;/STRONG&gt;that is included when you download the package, there you could see the prerequisites to run the example.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if you have more questions about this topic.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Apr 2025 23:04:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/PTP-using-RTD-GMAC-Driver/m-p/2086039#M13301</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2025-04-23T23:04:44Z</dc:date>
    </item>
    <item>
      <title>Re: PTP using RTD GMAC Driver</title>
      <link>https://community.nxp.com/t5/S32G/PTP-using-RTD-GMAC-Driver/m-p/2086045#M13302</link>
      <description>&lt;P&gt;Thank you for your quick response.&lt;BR /&gt;It seems the doc you shared is for using the PFE with PTP. But I want to use instead the GMAC which provide functions to offload the PTP messaging, controlled by&amp;nbsp;GMAC_MAC_PTO_CONTROL register for instance.&lt;BR /&gt;Is there somewhere a high level API that I could use for that ?&lt;/P&gt;</description>
      <pubDate>Wed, 23 Apr 2025 23:31:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/PTP-using-RTD-GMAC-Driver/m-p/2086045#M13302</guid>
      <dc:creator>yanis-waabi</dc:creator>
      <dc:date>2025-04-23T23:31:46Z</dc:date>
    </item>
    <item>
      <title>Re: PTP using RTD GMAC Driver</title>
      <link>https://community.nxp.com/t5/S32G/PTP-using-RTD-GMAC-Driver/m-p/2086880#M13304</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245960"&gt;@yanis-waabi&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You could use the PTP functionality with the linux BSP distributions to run it with GMAC&lt;/P&gt;
&lt;P&gt;please refer to the&lt;STRONG&gt;&amp;nbsp;Linux BSP 42.0 User Manual for S32G3 platforms (or the BSP Version you use)&amp;nbsp;&lt;/STRONG&gt;at chapter 8&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="carlos_o_0-1745527441967.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/334809i02D908CCA5E62230/image-size/medium?v=v2&amp;amp;px=400" role="button" title="carlos_o_0-1745527441967.png" alt="carlos_o_0-1745527441967.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;carlos_o_0-1745527441967.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Otherwise, you need to do your own implementation if you want to do it with the RTDs.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Apr 2025 20:58:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/PTP-using-RTD-GMAC-Driver/m-p/2086880#M13304</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2025-04-24T20:58:45Z</dc:date>
    </item>
    <item>
      <title>Re: PTP using RTD GMAC Driver</title>
      <link>https://community.nxp.com/t5/S32G/PTP-using-RTD-GMAC-Driver/m-p/2306032#M15941</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245960"&gt;@yanis-waabi&lt;/a&gt;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241501"&gt;@carlos_o&lt;/a&gt;&amp;nbsp;Is there an update on this thread? Do we have a GMAC port for S32G3 gPTP stack? If not then can you please provide details on what changes will be required to reliably port gPTP stack to GMAC for S32G3?&lt;/P&gt;</description>
      <pubDate>Wed, 04 Feb 2026 10:17:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/PTP-using-RTD-GMAC-Driver/m-p/2306032#M15941</guid>
      <dc:creator>rizwan_at_disruptdotcom</dc:creator>
      <dc:date>2026-02-04T10:17:03Z</dc:date>
    </item>
  </channel>
</rss>