<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Re: EB tree 29.0.0</title>
    <link>https://community.nxp.com/t5/S32G/EB-tree-29-0-0/m-p/2083226#M13281</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/248899"&gt;@liujian_abup&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the post.&lt;/P&gt;
&lt;P&gt;For building the project configured by EB, we suggest referencing the 5.3 part of AN13750(&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN13750" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=AN13750&lt;/A&gt;), Cygwin is used and the compiler for the building is set with the GCC installation path from S32DS.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
    <pubDate>Fri, 18 Apr 2025 09:23:38 GMT</pubDate>
    <dc:creator>chenyin_h</dc:creator>
    <dc:date>2025-04-18T09:23:38Z</dc:date>
    <item>
      <title>EB tree 29.0.0</title>
      <link>https://community.nxp.com/t5/S32G/EB-tree-29-0-0/m-p/2082500#M13278</link>
      <description>&lt;P&gt;hi，NXP：&lt;BR /&gt;&amp;nbsp;&amp;nbsp; I was able to build it using a full project, but when I executed the launch.bat file, I couldn't find the corresponding make compiler. Moreover, the compiler in S32 doesn't have a make.exe compiler either. So, I need to use the 32-bit mingw compiler for Windows&lt;/P&gt;</description>
      <pubDate>Thu, 17 Apr 2025 10:06:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/EB-tree-29-0-0/m-p/2082500#M13278</guid>
      <dc:creator>liujian_abup</dc:creator>
      <dc:date>2025-04-17T10:06:40Z</dc:date>
    </item>
    <item>
      <title>Re: EB tree 29.0.0</title>
      <link>https://community.nxp.com/t5/S32G/EB-tree-29-0-0/m-p/2083226#M13281</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/248899"&gt;@liujian_abup&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for the post.&lt;/P&gt;
&lt;P&gt;For building the project configured by EB, we suggest referencing the 5.3 part of AN13750(&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN13750" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=AN13750&lt;/A&gt;), Cygwin is used and the compiler for the building is set with the GCC installation path from S32DS.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Fri, 18 Apr 2025 09:23:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/EB-tree-29-0-0/m-p/2083226#M13281</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-04-18T09:23:38Z</dc:date>
    </item>
  </channel>
</rss>