<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32G399A - System timer module frequency in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G399A-System-timer-module-frequency/m-p/2064495#M13009</link>
    <description>&lt;P&gt;Perfect, thank you for your help.&lt;/P&gt;</description>
    <pubDate>Wed, 19 Mar 2025 08:28:59 GMT</pubDate>
    <dc:creator>Matteo_Zini</dc:creator>
    <dc:date>2025-03-19T08:28:59Z</dc:date>
    <item>
      <title>S32G399A - System timer module frequency</title>
      <link>https://community.nxp.com/t5/S32G/S32G399A-System-timer-module-frequency/m-p/2062946#M12958</link>
      <description>&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;I have an S32G399-RDB3 board with a setup derived from the GoldVIP package. The M7 binary and the Linux kernel images were changed, but the bootloader configuration is practically the same of the original configuration.&lt;/P&gt;&lt;P&gt;I'm using one of the system timer instances to collect measurements, and I wanted to ask whether there is a practical way to read the STM frequency without following the entire chain of clock signals.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Mon, 17 Mar 2025 09:46:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G399A-System-timer-module-frequency/m-p/2062946#M12958</guid>
      <dc:creator>Matteo_Zini</dc:creator>
      <dc:date>2025-03-17T09:46:43Z</dc:date>
    </item>
    <item>
      <title>Re: S32G399A - System timer module frequency</title>
      <link>https://community.nxp.com/t5/S32G/S32G399A-System-timer-module-frequency/m-p/2063023#M12964</link>
      <description>&lt;P&gt;hi，&lt;SPAN&gt;Matteo_Zini&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thank you for contacting us.&lt;BR /&gt;May I ask why you want to read the STM frequency without following the entire chain of clock signals?&lt;BR /&gt;In addition, You can refer to the attachment to check the clock of M core STM.&lt;/P&gt;</description>
      <pubDate>Mon, 17 Mar 2025 11:11:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G399A-System-timer-module-frequency/m-p/2063023#M12964</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2025-03-17T11:11:04Z</dc:date>
    </item>
    <item>
      <title>Re: S32G399A - System timer module frequency</title>
      <link>https://community.nxp.com/t5/S32G/S32G399A-System-timer-module-frequency/m-p/2063042#M12967</link>
      <description>Hi, thank you for the reply.&lt;BR /&gt;Because for example if you need to do it at runtime, there are multiple possible sources of the XBAR_DIV3_CLK clock and reconstructing the full chain is not trivial.&lt;BR /&gt;</description>
      <pubDate>Mon, 17 Mar 2025 11:41:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G399A-System-timer-module-frequency/m-p/2063042#M12967</guid>
      <dc:creator>Matteo_Zini</dc:creator>
      <dc:date>2025-03-17T11:41:17Z</dc:date>
    </item>
    <item>
      <title>Re: S32G399A - System timer module frequency</title>
      <link>https://community.nxp.com/t5/S32G/S32G399A-System-timer-module-frequency/m-p/2063317#M12969</link>
      <description>&lt;P&gt;hi,&lt;SPAN&gt;Matteo_Zini&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thank you for your reply.&lt;/P&gt;
&lt;P&gt;There are multiple possible sources of the XBAR_DIV3_CLK clock, so you need to configure the same value of&amp;nbsp;&lt;SPAN&gt;XBAR_DIV3_CLK for the M core and A core, to avoid conflicts.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Tue, 18 Mar 2025 01:57:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G399A-System-timer-module-frequency/m-p/2063317#M12969</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2025-03-18T01:57:58Z</dc:date>
    </item>
    <item>
      <title>Re: S32G399A - System timer module frequency</title>
      <link>https://community.nxp.com/t5/S32G/S32G399A-System-timer-module-frequency/m-p/2063880#M12997</link>
      <description>&lt;P&gt;I'm using Linux on the Cortex-A cores, so I'm not sure how to configure it.&lt;/P&gt;&lt;P&gt;Anyway, I would just need to understand the frequency to transform the ticks into seconds, not to set it to any specific value.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Tue, 18 Mar 2025 14:32:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G399A-System-timer-module-frequency/m-p/2063880#M12997</guid>
      <dc:creator>Matteo_Zini</dc:creator>
      <dc:date>2025-03-18T14:32:23Z</dc:date>
    </item>
    <item>
      <title>Re: S32G399A - System timer module frequency</title>
      <link>https://community.nxp.com/t5/S32G/S32G399A-System-timer-module-frequency/m-p/2064316#M13004</link>
      <description>&lt;P&gt;hi，&lt;SPAN&gt;Matteo_Zini&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thank you for your reply.&lt;/P&gt;
&lt;P&gt;If you want to know the exact STM timer time, you must know that the XBAR_DIV3_CLK default is 133.33Mhz, the frequency division factor CPS and CMP values.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Wed, 19 Mar 2025 04:01:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G399A-System-timer-module-frequency/m-p/2064316#M13004</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2025-03-19T04:01:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32G399A - System timer module frequency</title>
      <link>https://community.nxp.com/t5/S32G/S32G399A-System-timer-module-frequency/m-p/2064495#M13009</link>
      <description>&lt;P&gt;Perfect, thank you for your help.&lt;/P&gt;</description>
      <pubDate>Wed, 19 Mar 2025 08:28:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G399A-System-timer-module-frequency/m-p/2064495#M13009</guid>
      <dc:creator>Matteo_Zini</dc:creator>
      <dc:date>2025-03-19T08:28:59Z</dc:date>
    </item>
  </channel>
</rss>