<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32 doesn't boot in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32-doesn-t-boot/m-p/1336150#M128</link>
    <description>&lt;P&gt;I am booting S32G from SD Card. Yesterday everything was working fine.&lt;/P&gt;&lt;P&gt;Today when I started the Eval-board I got the following error:&lt;/P&gt;&lt;P&gt;U-Boot 2018.07&lt;/P&gt;&lt;P&gt;CPU: NXP S32G274A rev. 1.0.1&lt;BR /&gt;Reset cause: Power-On Reset&lt;BR /&gt;Model: NXP S32G27x&lt;BR /&gt;Board: NXP S32G274A-EVB&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: ddrss: 1D firmware execution failed!&lt;BR /&gt;### ERROR ### Please RESET the board ###&lt;/P&gt;&lt;P&gt;I tried to unscrew and screw again the Soc, but keep receiving the same error message.&lt;/P&gt;&lt;P&gt;I tried also to replace the Soc with a CAT2 Soc (The first one was a CAT1), but then I received no output&lt;/P&gt;&lt;P&gt;Can anybody help on this issue, is there any way to debug the Problem ?&lt;/P&gt;</description>
    <pubDate>Tue, 07 Sep 2021 13:13:53 GMT</pubDate>
    <dc:creator>bou6</dc:creator>
    <dc:date>2021-09-07T13:13:53Z</dc:date>
    <item>
      <title>S32 doesn't boot</title>
      <link>https://community.nxp.com/t5/S32G/S32-doesn-t-boot/m-p/1336150#M128</link>
      <description>&lt;P&gt;I am booting S32G from SD Card. Yesterday everything was working fine.&lt;/P&gt;&lt;P&gt;Today when I started the Eval-board I got the following error:&lt;/P&gt;&lt;P&gt;U-Boot 2018.07&lt;/P&gt;&lt;P&gt;CPU: NXP S32G274A rev. 1.0.1&lt;BR /&gt;Reset cause: Power-On Reset&lt;BR /&gt;Model: NXP S32G27x&lt;BR /&gt;Board: NXP S32G274A-EVB&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: ddrss: 1D firmware execution failed!&lt;BR /&gt;### ERROR ### Please RESET the board ###&lt;/P&gt;&lt;P&gt;I tried to unscrew and screw again the Soc, but keep receiving the same error message.&lt;/P&gt;&lt;P&gt;I tried also to replace the Soc with a CAT2 Soc (The first one was a CAT1), but then I received no output&lt;/P&gt;&lt;P&gt;Can anybody help on this issue, is there any way to debug the Problem ?&lt;/P&gt;</description>
      <pubDate>Tue, 07 Sep 2021 13:13:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32-doesn-t-boot/m-p/1336150#M128</guid>
      <dc:creator>bou6</dc:creator>
      <dc:date>2021-09-07T13:13:53Z</dc:date>
    </item>
    <item>
      <title>Re: S32 doesn't boot</title>
      <link>https://community.nxp.com/t5/S32G/S32-doesn-t-boot/m-p/1345848#M146</link>
      <description>&lt;P&gt;This message is output by DDR controller driver and indicates that DDR interface training failed. This process is done by the embedded calibration processor and is fully automatic. What you can do is:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Check that all jumpers are at their default positions. Refer to the board User Guide.&lt;/LI&gt;
&lt;LI&gt;Re-program the boot SD card, in case the boot binaries are corrupt.&lt;/LI&gt;
&lt;LI&gt;Run diagnostic tests which are available under &lt;A href="https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32G2-REFSW-D" target="_self"&gt;S32G2 Reference Software&lt;/A&gt; category.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;If the problem persists or the diagnostic tests find any errors, the board may be permanently damaged.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 24 Sep 2021 12:21:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32-doesn-t-boot/m-p/1345848#M146</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2021-09-24T12:21:40Z</dc:date>
    </item>
    <item>
      <title>Re: S32 doesn't boot</title>
      <link>https://community.nxp.com/t5/S32G/S32-doesn-t-boot/m-p/1910466#M8768</link>
      <description>&lt;P&gt;hi bpe,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am also facing similar kind of issue, can i get the diagnostic SD card image for "S32G-VNP-EVB3",&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jul 2024 09:06:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32-doesn-t-boot/m-p/1910466#M8768</guid>
      <dc:creator>SARATHI_22</dc:creator>
      <dc:date>2024-07-17T09:06:15Z</dc:date>
    </item>
  </channel>
</rss>