<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Generation of UDP Ethernet Packet when configuring IEEE802.1 CB (FRER) in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Generation-of-UDP-Ethernet-Packet-when-configuring-IEEE802-1-CB/m-p/2053180#M12770</link>
    <description>&lt;P&gt;&lt;SPAN&gt;I have configured, CB Sequence Generation and Individual recovery Table, L2 Lookup Table and I configured General Parameters --&amp;gt; RTAG_TYPE = 0xF1C1/ 0x0800 i tried two option, enabled SEQNUM_GENERATOR -- ENABLE &amp;amp; CB_EN -- ENABLE&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;BR /&gt;But when Generating an Ethernet Frame there was some misalignment is happening in generation of Ethernet Frames&lt;BR /&gt;It should generate frame&amp;nbsp;&lt;BR /&gt;[Dst MAC] [Src MAC] [EtherType (0x0800)] [IPv4 Header] [UDP Header] [Payload]&lt;BR /&gt;But the Frame is getting Generated is&amp;nbsp;&lt;BR /&gt;[Dst MAC] [Src MAC] [RTAG_TYPE (0xF1C1)] [Some extra bytes] [EtherType (0x0800)] [IPv4 Header] ...&lt;BR /&gt;below is my sample data&lt;BR /&gt;11 22 33 44 55 66 4C 4C 43 45 41 46 F1 C1 00 00 00 04 08 00&lt;BR /&gt;45 00 00 2C 00 04 40 00 10 11 6C BB 7F 00 00 01 7F 00 00 01&lt;BR /&gt;05 DC 05 DC 00 18 CA 20 0C 03 20 C8 00 00 00 08 FF 0F FF FF&lt;BR /&gt;FF FF FF FF 00 00&lt;BR /&gt;&lt;BR /&gt;I have configured based on the Documentation -- "AH SJA1110 TCAM and TSN"&lt;BR /&gt;&lt;BR /&gt;due to this issue its unable to generate a UDP Frame as Expected which is causing the issue&amp;nbsp;&lt;BR /&gt;so how can i overcome this issue&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;Abrar&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 27 Feb 2025 18:03:36 GMT</pubDate>
    <dc:creator>Abrar_23</dc:creator>
    <dc:date>2025-02-27T18:03:36Z</dc:date>
    <item>
      <title>Generation of UDP Ethernet Packet when configuring IEEE802.1 CB (FRER)</title>
      <link>https://community.nxp.com/t5/S32G/Generation-of-UDP-Ethernet-Packet-when-configuring-IEEE802-1-CB/m-p/2053180#M12770</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I have configured, CB Sequence Generation and Individual recovery Table, L2 Lookup Table and I configured General Parameters --&amp;gt; RTAG_TYPE = 0xF1C1/ 0x0800 i tried two option, enabled SEQNUM_GENERATOR -- ENABLE &amp;amp; CB_EN -- ENABLE&amp;nbsp;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;BR /&gt;But when Generating an Ethernet Frame there was some misalignment is happening in generation of Ethernet Frames&lt;BR /&gt;It should generate frame&amp;nbsp;&lt;BR /&gt;[Dst MAC] [Src MAC] [EtherType (0x0800)] [IPv4 Header] [UDP Header] [Payload]&lt;BR /&gt;But the Frame is getting Generated is&amp;nbsp;&lt;BR /&gt;[Dst MAC] [Src MAC] [RTAG_TYPE (0xF1C1)] [Some extra bytes] [EtherType (0x0800)] [IPv4 Header] ...&lt;BR /&gt;below is my sample data&lt;BR /&gt;11 22 33 44 55 66 4C 4C 43 45 41 46 F1 C1 00 00 00 04 08 00&lt;BR /&gt;45 00 00 2C 00 04 40 00 10 11 6C BB 7F 00 00 01 7F 00 00 01&lt;BR /&gt;05 DC 05 DC 00 18 CA 20 0C 03 20 C8 00 00 00 08 FF 0F FF FF&lt;BR /&gt;FF FF FF FF 00 00&lt;BR /&gt;&lt;BR /&gt;I have configured based on the Documentation -- "AH SJA1110 TCAM and TSN"&lt;BR /&gt;&lt;BR /&gt;due to this issue its unable to generate a UDP Frame as Expected which is causing the issue&amp;nbsp;&lt;BR /&gt;so how can i overcome this issue&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;Abrar&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Feb 2025 18:03:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Generation-of-UDP-Ethernet-Packet-when-configuring-IEEE802-1-CB/m-p/2053180#M12770</guid>
      <dc:creator>Abrar_23</dc:creator>
      <dc:date>2025-02-27T18:03:36Z</dc:date>
    </item>
    <item>
      <title>Re: Generation of UDP Ethernet Packet when configuring IEEE802.1 CB (FRER)</title>
      <link>https://community.nxp.com/t5/S32G/Generation-of-UDP-Ethernet-Packet-when-configuring-IEEE802-1-CB/m-p/2056600#M12849</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/247351"&gt;@Abrar_23&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Sorry for the late response. about your problem, I see you created a similar post here:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32G/Generated-Ethernet-Frame-is-not-UDP-0x800-in-IEEE802-1CB-FRER/td-p/2053054" target="_blank"&gt;2053054&lt;/A&gt;, are the two post about the exact same problem? if so, is it ok for you if we keep the discussion only in this one?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 06 Mar 2025 00:30:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Generation-of-UDP-Ethernet-Packet-when-configuring-IEEE802-1-CB/m-p/2056600#M12849</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2025-03-06T00:30:00Z</dc:date>
    </item>
  </channel>
</rss>