<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic uboot setenv ethaddr in S32G</title>
    <link>https://community.nxp.com/t5/S32G/uboot-setenv-ethaddr/m-p/2052460#M12752</link>
    <description>&lt;P&gt;Hello I want to fix the mac address of the S32G gmac, I execute the following command under uboot&lt;/P&gt;&lt;P&gt;setenv ethaddr d6:20:eb:40:75:d8&lt;/P&gt;&lt;P&gt;saveenv&lt;/P&gt;&lt;P&gt;The mac address obtained when running ifconfig eth0 to the kernel is different from ethaddr. Does the current s32g support mac address passing from uboot to the kernel.&lt;/P&gt;</description>
    <pubDate>Thu, 27 Feb 2025 02:29:59 GMT</pubDate>
    <dc:creator>shiyiheng</dc:creator>
    <dc:date>2025-02-27T02:29:59Z</dc:date>
    <item>
      <title>uboot setenv ethaddr</title>
      <link>https://community.nxp.com/t5/S32G/uboot-setenv-ethaddr/m-p/2052460#M12752</link>
      <description>&lt;P&gt;Hello I want to fix the mac address of the S32G gmac, I execute the following command under uboot&lt;/P&gt;&lt;P&gt;setenv ethaddr d6:20:eb:40:75:d8&lt;/P&gt;&lt;P&gt;saveenv&lt;/P&gt;&lt;P&gt;The mac address obtained when running ifconfig eth0 to the kernel is different from ethaddr. Does the current s32g support mac address passing from uboot to the kernel.&lt;/P&gt;</description>
      <pubDate>Thu, 27 Feb 2025 02:29:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/uboot-setenv-ethaddr/m-p/2052460#M12752</guid>
      <dc:creator>shiyiheng</dc:creator>
      <dc:date>2025-02-27T02:29:59Z</dc:date>
    </item>
    <item>
      <title>Re: uboot setenv ethaddr</title>
      <link>https://community.nxp.com/t5/S32G/uboot-setenv-ethaddr/m-p/2052586#M12754</link>
      <description>&lt;P&gt;hi,&lt;SPAN&gt;shiyiheng&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Are you using S32G2 or S32G3? Which version of BSP are you using?&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Thu, 27 Feb 2025 05:51:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/uboot-setenv-ethaddr/m-p/2052586#M12754</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2025-02-27T05:51:28Z</dc:date>
    </item>
    <item>
      <title>Re: uboot setenv ethaddr</title>
      <link>https://community.nxp.com/t5/S32G/uboot-setenv-ethaddr/m-p/2052588#M12755</link>
      <description>&lt;P&gt;I am using S32G3,RDB3 development version I, BSP34 version, I have tried other versions, it seems that it is not possible.&lt;/P&gt;</description>
      <pubDate>Thu, 27 Feb 2025 05:57:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/uboot-setenv-ethaddr/m-p/2052588#M12755</guid>
      <dc:creator>shiyiheng</dc:creator>
      <dc:date>2025-02-27T05:57:10Z</dc:date>
    </item>
    <item>
      <title>Re: uboot setenv ethaddr</title>
      <link>https://community.nxp.com/t5/S32G/uboot-setenv-ethaddr/m-p/2054353#M12800</link>
      <description>&lt;P&gt;hi,&lt;SPAN&gt;shiyiheng&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Sorry for the reply late.&lt;/P&gt;
&lt;P&gt;You can try modifying the u-boot env&amp;nbsp;&lt;SPAN&gt;variable as shown in the picture.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Hope it can help you.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Mon, 03 Mar 2025 04:27:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/uboot-setenv-ethaddr/m-p/2054353#M12800</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2025-03-03T04:27:22Z</dc:date>
    </item>
  </channel>
</rss>