<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Secure boot of kernel image in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Secure-boot-of-kernel-image/m-p/2039190#M12532</link>
    <description>&lt;P&gt;Hello I am currently working on securing the boot process of the kernel image using U-Boot on the S32G3 board (BSP 40). I would appreciate some clarification on the following:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;In the event of a kernel image boot failure, what is the recommended recovery mechanism? On the M core side, there are two slots available for an image, allowing for a fallback to a backup or alternate image if the primary image fails. This process is managed based on the SMR (Secure Memory Region) configurations. Is there a similar recovery mechanism for the kernel image? If so, could you please provide further details?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 06 Feb 2025 09:10:08 GMT</pubDate>
    <dc:creator>Jayashree</dc:creator>
    <dc:date>2025-02-06T09:10:08Z</dc:date>
    <item>
      <title>Secure boot of kernel image</title>
      <link>https://community.nxp.com/t5/S32G/Secure-boot-of-kernel-image/m-p/2039190#M12532</link>
      <description>&lt;P&gt;Hello I am currently working on securing the boot process of the kernel image using U-Boot on the S32G3 board (BSP 40). I would appreciate some clarification on the following:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;In the event of a kernel image boot failure, what is the recommended recovery mechanism? On the M core side, there are two slots available for an image, allowing for a fallback to a backup or alternate image if the primary image fails. This process is managed based on the SMR (Secure Memory Region) configurations. Is there a similar recovery mechanism for the kernel image? If so, could you please provide further details?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 06 Feb 2025 09:10:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Secure-boot-of-kernel-image/m-p/2039190#M12532</guid>
      <dc:creator>Jayashree</dc:creator>
      <dc:date>2025-02-06T09:10:08Z</dc:date>
    </item>
    <item>
      <title>Re: Secure boot of kernel image</title>
      <link>https://community.nxp.com/t5/S32G/Secure-boot-of-kernel-image/m-p/2039676#M12558</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235643"&gt;@Jayashree&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;From my understanding, there seems not such features provided within BSP for kernel booting recovery, and it may be designed and implemented by the user according to the specific requirements.&lt;/P&gt;
&lt;P&gt;I apologize for your inconvenience.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Feb 2025 03:34:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Secure-boot-of-kernel-image/m-p/2039676#M12558</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2025-02-07T03:34:02Z</dc:date>
    </item>
    <item>
      <title>Re: Secure boot of kernel image</title>
      <link>https://community.nxp.com/t5/S32G/Secure-boot-of-kernel-image/m-p/2075420#M13171</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;In a scenario where a previously working system is updated with a new kernel image, and the updated system fails to boot due to a bad hash indicating a verification or integrity issue with the newly flashed kernel.&lt;BR /&gt;In such a situation, what would be the recommended recovery procedure?&lt;BR /&gt;&lt;BR /&gt;Is it possible to revert to the previous kernel image safely? If so will the newly updated fip.s32 and ATF&amp;nbsp; support the previous kernel image&lt;BR /&gt;&lt;BR /&gt;Or would reflashing with a known good kernel be the best course of action?&lt;BR /&gt;&lt;BR /&gt;I would appreciate any guidance on best practices for handling such recovery scenarios.&lt;BR /&gt;Thank you&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Mon, 07 Apr 2025 19:07:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Secure-boot-of-kernel-image/m-p/2075420#M13171</guid>
      <dc:creator>Jayashree</dc:creator>
      <dc:date>2025-04-07T19:07:41Z</dc:date>
    </item>
  </channel>
</rss>