<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32G RDB2 boot hang in bsp42 + RTD4.0.2 in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G-RDB2-boot-hang-in-bsp42-RTD4-0-2/m-p/2031406#M12395</link>
    <description>&lt;P&gt;Hi,&lt;SPAN&gt;Allen_Cheng&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thank you for contacting us.&lt;/P&gt;
&lt;P&gt;Is&amp;nbsp;Application 1 Image&amp;nbsp;an IPCF image? Which version of IPCF are you using?&lt;/P&gt;
&lt;P&gt;In addition, which version of the bootloader project are you using?&lt;/P&gt;
&lt;P&gt;BR&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
    <pubDate>Tue, 21 Jan 2025 10:55:13 GMT</pubDate>
    <dc:creator>Joey_z</dc:creator>
    <dc:date>2025-01-21T10:55:13Z</dc:date>
    <item>
      <title>S32G RDB2 boot hang in bsp42 + RTD4.0.2</title>
      <link>https://community.nxp.com/t5/S32G/S32G-RDB2-boot-hang-in-bsp42-RTD4-0-2/m-p/2031157#M12392</link>
      <description>&lt;P&gt;Hi NXP team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to create a multicore boot environment following AN13750.&lt;/P&gt;&lt;P&gt;Before the issue occurred, BSP42+RTD4.0.0 will bootup into Linux kernel successfully.&lt;/P&gt;&lt;P&gt;Below is my sw version:&lt;/P&gt;&lt;P&gt;Linux BSP42&lt;/P&gt;&lt;P&gt;RTD4.0.2 HF03&lt;/P&gt;&lt;P&gt;bootloader project(GoldVIP-S32G2-1.12.0)&lt;/P&gt;&lt;P&gt;HSE S32G2XX_0_2_22_0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;boot hang log:(first time)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;bootloader 0x2 ComDal_Init() done.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;bootloader 0x2 CryptoDal HSE status HSE_STATUS_RNG_INIT_OK&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;bootloader 0x2 CryptoDal HSE status HSE_STATUS_INIT_OK&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;bootloader 0x2 CryptoDal HSE status HSE_STATUS_INSTALL_OK&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;bootloader 0x2 CryptoDal HSE status HSE_STATUS_BOOT_OK&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;bootloader 0x2 CryptoDal HSE status HSE_STATUS_CUST_SUPER_USER&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;bootloader 0x2 CryptoDal HSE status HSE_STATUS_PRIMARY_SYS_IMAGE&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;bootloader 0x2 HSE FW Version: 0.1.0_2.22.0&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;bootloader 0x2 CryptoDal skipped the key catalogs format&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;bootloader 0x2 Bootloader secure boot is enabled.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;bootloader 0x2 Bootloader initialization complete.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;bootloader 0x2 Application 0 image fragment 0 of size 262144 was loaded from QSPI, address 0x100000.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;bootloader 0x2 Application 0 image fragment 0 was loaded in 10.847 milliseconds.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;bootloader 0x2 Application A53_0 was loaded.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;bootloader 0x2 Application 1 image fragment 0 of size 1048576 was loaded from QSPI, address 0x200000.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;bootloader 0x2 Application 1 image fragment 0 was loaded in 15.135 milliseconds.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;bootloader 0x2 Application M7_0 was loaded.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;NOTICE: Reset status: Power-On Reset&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;NOTICE: BL2: v2.10.0 (release):bsp42.0-2.10-dirty&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;NOTICE: BL2: Built : 13:53:34, Jan 16 2025&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;NOTICE: BL2: Booting BL31&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;After RDB2 power cycle log:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;bootloader 0x2 ComDal_Init() done.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please supply some suggestions?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Allen&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jan 2025 06:55:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-RDB2-boot-hang-in-bsp42-RTD4-0-2/m-p/2031157#M12392</guid>
      <dc:creator>Allen_Cheng</dc:creator>
      <dc:date>2025-01-21T06:55:55Z</dc:date>
    </item>
    <item>
      <title>Re: S32G RDB2 boot hang in bsp42 + RTD4.0.2</title>
      <link>https://community.nxp.com/t5/S32G/S32G-RDB2-boot-hang-in-bsp42-RTD4-0-2/m-p/2031406#M12395</link>
      <description>&lt;P&gt;Hi,&lt;SPAN&gt;Allen_Cheng&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thank you for contacting us.&lt;/P&gt;
&lt;P&gt;Is&amp;nbsp;Application 1 Image&amp;nbsp;an IPCF image? Which version of IPCF are you using?&lt;/P&gt;
&lt;P&gt;In addition, which version of the bootloader project are you using?&lt;/P&gt;
&lt;P&gt;BR&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jan 2025 10:55:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-RDB2-boot-hang-in-bsp42-RTD4-0-2/m-p/2031406#M12395</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2025-01-21T10:55:13Z</dc:date>
    </item>
    <item>
      <title>Re: S32G RDB2 boot hang in bsp42 + RTD4.0.2</title>
      <link>https://community.nxp.com/t5/S32G/S32G-RDB2-boot-hang-in-bsp42-RTD4-0-2/m-p/2036995#M12501</link>
      <description>&lt;P&gt;Hi Joey,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry to late reply.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;U&gt;Is&amp;nbsp;Application 1 Image&amp;nbsp;an IPCF image? Which version of IPCF are you using?&lt;/U&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Ans: based on 4.6(AN13750 example version) patch to 4.8&lt;/P&gt;&lt;P&gt;&lt;U&gt;&lt;EM&gt;In addition, which version of the bootloader project are you using?&lt;/EM&gt;&lt;/U&gt;&lt;/P&gt;&lt;P&gt;Ans: the bootloader project from GoldVIP-S32G-1.12.0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Allen&lt;/P&gt;</description>
      <pubDate>Mon, 03 Feb 2025 03:05:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-RDB2-boot-hang-in-bsp42-RTD4-0-2/m-p/2036995#M12501</guid>
      <dc:creator>Allen_Cheng</dc:creator>
      <dc:date>2025-02-03T03:05:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32G RDB2 boot hang in bsp42 + RTD4.0.2</title>
      <link>https://community.nxp.com/t5/S32G/S32G-RDB2-boot-hang-in-bsp42-RTD4-0-2/m-p/2038286#M12518</link>
      <description>&lt;P&gt;Hi，Allen_Cheng&lt;/P&gt;
&lt;P&gt;Thank you for your reply.&lt;/P&gt;
&lt;P&gt;According to the ReleaseNotes, If you are using the version&amp;nbsp;4.8 of IPCF , then the RTD version 4.0.0 is required. If you are using the version&amp;nbsp;4.9 of IPCF , then the RTD version 4.0.2 is required.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Wed, 05 Feb 2025 06:28:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-RDB2-boot-hang-in-bsp42-RTD4-0-2/m-p/2038286#M12518</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2025-02-05T06:28:40Z</dc:date>
    </item>
  </channel>
</rss>