<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Kernel image authentication using FIT image (secure boot)</title>
    <link>https://community.nxp.com/t5/S32G/Kernel-image-authentication-using-FIT-image-secure-boot/m-p/2029057#M12359</link>
    <description>&lt;P&gt;I am currently working on the S32G3 Goldbox using BSP 40. I have followed the manual's instructions to create a FIT image. However, when I execute the bootm along with the load address im getting the following error&lt;/P&gt;&lt;P&gt;Wrong Image Format for bootm command&lt;BR /&gt;ERROR: can't get kernel image!&lt;/P&gt;&lt;P&gt;iminfo gives the following statement&lt;BR /&gt;iminfo&lt;BR /&gt;## Checking Image at 80000000 ...&lt;BR /&gt;Unknown image format!&lt;/P&gt;&lt;P&gt;But when i do the md command, it shows like this&lt;BR /&gt;md 0x80000000 100&lt;BR /&gt;80000000: edfe0dd0 821f1101 38000000 441d1101 ...........8...D&lt;BR /&gt;80000010: 28000000 11000000 10000000 00000000 ...(............&lt;BR /&gt;80000020: c9000000 0c1d1101 00000000 00000000 ................&lt;BR /&gt;80000030: 00000000 00000000 01000000 00000000 ................&lt;BR /&gt;80000040: 03000000 04000000 82000000 edb88867 ............g...&lt;BR /&gt;80000050: 03000000 27000000 00000000 20544946 .......'....FIT&lt;BR /&gt;80000060: 67616d69 69772065 63206874 72706d6f image with compr&lt;BR /&gt;80000070: 69737365 61206e6f 7320646e 696e6769 ession and signi&lt;BR /&gt;80000080: 0000676e 03000000 04000000 0c000000 ng..............&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Could you please provide guidance or assistance in resolving this issue&lt;/P&gt;</description>
    <pubDate>Thu, 16 Jan 2025 13:22:23 GMT</pubDate>
    <dc:creator>Jayashree</dc:creator>
    <dc:date>2025-01-16T13:22:23Z</dc:date>
    <item>
      <title>Kernel image authentication using FIT image (secure boot)</title>
      <link>https://community.nxp.com/t5/S32G/Kernel-image-authentication-using-FIT-image-secure-boot/m-p/2029057#M12359</link>
      <description>&lt;P&gt;I am currently working on the S32G3 Goldbox using BSP 40. I have followed the manual's instructions to create a FIT image. However, when I execute the bootm along with the load address im getting the following error&lt;/P&gt;&lt;P&gt;Wrong Image Format for bootm command&lt;BR /&gt;ERROR: can't get kernel image!&lt;/P&gt;&lt;P&gt;iminfo gives the following statement&lt;BR /&gt;iminfo&lt;BR /&gt;## Checking Image at 80000000 ...&lt;BR /&gt;Unknown image format!&lt;/P&gt;&lt;P&gt;But when i do the md command, it shows like this&lt;BR /&gt;md 0x80000000 100&lt;BR /&gt;80000000: edfe0dd0 821f1101 38000000 441d1101 ...........8...D&lt;BR /&gt;80000010: 28000000 11000000 10000000 00000000 ...(............&lt;BR /&gt;80000020: c9000000 0c1d1101 00000000 00000000 ................&lt;BR /&gt;80000030: 00000000 00000000 01000000 00000000 ................&lt;BR /&gt;80000040: 03000000 04000000 82000000 edb88867 ............g...&lt;BR /&gt;80000050: 03000000 27000000 00000000 20544946 .......'....FIT&lt;BR /&gt;80000060: 67616d69 69772065 63206874 72706d6f image with compr&lt;BR /&gt;80000070: 69737365 61206e6f 7320646e 696e6769 ession and signi&lt;BR /&gt;80000080: 0000676e 03000000 04000000 0c000000 ng..............&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Could you please provide guidance or assistance in resolving this issue&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jan 2025 13:22:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Kernel-image-authentication-using-FIT-image-secure-boot/m-p/2029057#M12359</guid>
      <dc:creator>Jayashree</dc:creator>
      <dc:date>2025-01-16T13:22:23Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel image authentication using FIT image (secure boot)</title>
      <link>https://community.nxp.com/t5/S32G/Kernel-image-authentication-using-FIT-image-secure-boot/m-p/2029200#M12362</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235643"&gt;@Jayashree&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Are you booting from SD or QSPI?&lt;/P&gt;
&lt;P&gt;Can you please describe the process you follow to flash the image?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jan 2025 18:25:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Kernel-image-authentication-using-FIT-image-secure-boot/m-p/2029200#M12362</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2025-01-16T18:25:10Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel image authentication using FIT image (secure boot)</title>
      <link>https://community.nxp.com/t5/S32G/Kernel-image-authentication-using-FIT-image-secure-boot/m-p/2029484#M12369</link>
      <description>&lt;P&gt;As mentioned in the manual, "&lt;STRONG&gt;The resulting FIT image must be copied to the boot partition of the SD Card&lt;/STRONG&gt;." i am copying the image to the boot partition of the sd card and booting&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jan 2025 05:17:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Kernel-image-authentication-using-FIT-image-secure-boot/m-p/2029484#M12369</guid>
      <dc:creator>Jayashree</dc:creator>
      <dc:date>2025-01-17T05:17:28Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel image authentication using FIT image (secure boot)</title>
      <link>https://community.nxp.com/t5/S32G/Kernel-image-authentication-using-FIT-image-secure-boot/m-p/2029920#M12375</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235643"&gt;@Jayashree&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Which version of HSE are you using?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Double check that your .its file is configured correctly, essentially the paths to the kernel and dtb.&lt;/P&gt;
&lt;P&gt;If you want to share the configuration to review it, you can do it in a private channel opening a ticket with the same issue and my user to track it.&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jan 2025 18:18:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Kernel-image-authentication-using-FIT-image-secure-boot/m-p/2029920#M12375</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2025-01-17T18:18:17Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel image authentication using FIT image (secure boot)</title>
      <link>https://community.nxp.com/t5/S32G/Kernel-image-authentication-using-FIT-image-secure-boot/m-p/2030378#M12382</link>
      <description>&lt;P&gt;i am using this HSE version HSE_FW_S32G3_0_2_22_0&lt;BR /&gt;But how does HSE matter in the kernel image verification using FIT image?&lt;BR /&gt;My bootm command seems to fail but im not sure why&lt;/P&gt;</description>
      <pubDate>Mon, 20 Jan 2025 07:10:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Kernel-image-authentication-using-FIT-image-secure-boot/m-p/2030378#M12382</guid>
      <dc:creator>Jayashree</dc:creator>
      <dc:date>2025-01-20T07:10:36Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel image authentication using FIT image (secure boot)</title>
      <link>https://community.nxp.com/t5/S32G/Kernel-image-authentication-using-FIT-image-secure-boot/m-p/2031664#M12401</link>
      <description>&lt;P&gt;The HSE is the component that execute the secure boot in this case that's why is important to know that you a using the compatible version of it with the BSP.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jan 2025 19:19:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Kernel-image-authentication-using-FIT-image-secure-boot/m-p/2031664#M12401</guid>
      <dc:creator>carlos_o</dc:creator>
      <dc:date>2025-01-21T19:19:39Z</dc:date>
    </item>
  </channel>
</rss>