<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックBSP43.0 S32G3 FIP Update</title>
    <link>https://community.nxp.com/t5/S32G/BSP43-0-S32G3-FIP-Update/m-p/2017475#M12078</link>
    <description>&lt;P&gt;BSP43 splits the fip.s32-sdcard file into two files, bl2_2_dtb.s32-sdcard and fip.bin-sdcard.&lt;/P&gt;&lt;P&gt;My hardware has a emmc and qspi, with no sdcard.&lt;/P&gt;&lt;P&gt;Previously, we would use the flash tool to load the bootloader to address 0 of the qspi, the m-core app at 0x50000, and the fip.s32-sdcard file to 0x600000.&amp;nbsp; We would also flash the fip.s32-sdcard file to address 0x0 of the emmc.&amp;nbsp; This would boot to u-boot, and from there we would tftp the full linux image onto the emmc.&lt;/P&gt;&lt;P&gt;With the new change, I can't get it to work.&amp;nbsp; I loaded the bl2_2_dtb.s32-sdcard file to 0x600000 of the qspi and the fip.bin-sdcard to address 0x0 of the emmc.&amp;nbsp; The bl2 runs, but does not find the fip file.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It appears in the linux reference manual that the fip needs to be in the 'first partition' of the emmc?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Before loading the linux image, the emmc is not partitioned, and the fip is in unpartitioned space.&lt;/P&gt;&lt;P&gt;Is there a way to load the fip file into a partition using the flash tool, or is there another way to do this?&lt;/P&gt;</description>
    <pubDate>Thu, 19 Dec 2024 22:20:53 GMT</pubDate>
    <dc:creator>eburley</dc:creator>
    <dc:date>2024-12-19T22:20:53Z</dc:date>
    <item>
      <title>BSP43.0 S32G3 FIP Update</title>
      <link>https://community.nxp.com/t5/S32G/BSP43-0-S32G3-FIP-Update/m-p/2017475#M12078</link>
      <description>&lt;P&gt;BSP43 splits the fip.s32-sdcard file into two files, bl2_2_dtb.s32-sdcard and fip.bin-sdcard.&lt;/P&gt;&lt;P&gt;My hardware has a emmc and qspi, with no sdcard.&lt;/P&gt;&lt;P&gt;Previously, we would use the flash tool to load the bootloader to address 0 of the qspi, the m-core app at 0x50000, and the fip.s32-sdcard file to 0x600000.&amp;nbsp; We would also flash the fip.s32-sdcard file to address 0x0 of the emmc.&amp;nbsp; This would boot to u-boot, and from there we would tftp the full linux image onto the emmc.&lt;/P&gt;&lt;P&gt;With the new change, I can't get it to work.&amp;nbsp; I loaded the bl2_2_dtb.s32-sdcard file to 0x600000 of the qspi and the fip.bin-sdcard to address 0x0 of the emmc.&amp;nbsp; The bl2 runs, but does not find the fip file.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It appears in the linux reference manual that the fip needs to be in the 'first partition' of the emmc?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Before loading the linux image, the emmc is not partitioned, and the fip is in unpartitioned space.&lt;/P&gt;&lt;P&gt;Is there a way to load the fip file into a partition using the flash tool, or is there another way to do this?&lt;/P&gt;</description>
      <pubDate>Thu, 19 Dec 2024 22:20:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/BSP43-0-S32G3-FIP-Update/m-p/2017475#M12078</guid>
      <dc:creator>eburley</dc:creator>
      <dc:date>2024-12-19T22:20:53Z</dc:date>
    </item>
    <item>
      <title>Re: BSP43.0 S32G3 FIP Update</title>
      <link>https://community.nxp.com/t5/S32G/BSP43-0-S32G3-FIP-Update/m-p/2017849#M12083</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/190401"&gt;@eburley&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;Yes, in latest BSP43, the original fip.s32 is divided into two binaries, and the new fip.bin is stored under the first partition of SD/MMC.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I could understand your issue, and will test it from our end to check further, I will update the status once any findings made.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 20 Dec 2024 11:07:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/BSP43-0-S32G3-FIP-Update/m-p/2017849#M12083</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-12-20T11:07:20Z</dc:date>
    </item>
  </channel>
</rss>