<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: Error while integrating the HSE with yocto</title>
    <link>https://community.nxp.com/t5/S32G/Error-while-integrating-the-HSE-with-yocto/m-p/2013324#M12021</link>
    <description>&lt;P&gt;The content of the local.conf is :&lt;/P&gt;&lt;P&gt;DISTRO_FEATURES:append = " hse "&lt;/P&gt;&lt;P&gt;NXP_FIRMWARE_LOCAL_DIR = "/yocto-s32g3/folder"&lt;/P&gt;&lt;P&gt;HSE_VERSION="0_2_22_0"&lt;/P&gt;&lt;P&gt;HSE_SOC_REV="rev1.1"&lt;/P&gt;&lt;P&gt;HSE_LIC_MD5 = "a1bda359fc5cdcfca04f84834841a5ca"&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;and the command i used for building is :&lt;BR /&gt;bitbake ros-image-core&lt;/P&gt;</description>
    <pubDate>Fri, 13 Dec 2024 05:48:29 GMT</pubDate>
    <dc:creator>ashwini2024</dc:creator>
    <dc:date>2024-12-13T05:48:29Z</dc:date>
    <item>
      <title>Error while integrating the HSE with yocto</title>
      <link>https://community.nxp.com/t5/S32G/Error-while-integrating-the-HSE-with-yocto/m-p/2012006#M11998</link>
      <description>&lt;P&gt;I am using bsp 40 and the firmware version is HSE_FW_S32G3XX_0_2_22_0. I am getting the following error when adding the lines in local.conf:&lt;/P&gt;&lt;P&gt;ERROR: ros-image-core-1.0-r0 do_rootfs: The postinstall intercept hook 'update_mime_database' failed, details in /yocto-s32g3/build_s32g399ardb3/tmp/work/s32g399ardb3-fsl-linux/ros-image-core/1.0-r0/temp/log.do_rootfs&lt;BR /&gt;ERROR: Logfile of failure stored in: /yocto-s32g3/build_s32g399ardb3/tmp/work/s32g399ardb3-fsl-linux/ros-image-core/1.0-r0/temp/log.do_rootfs.52670&lt;BR /&gt;ERROR: Task (/yocto-s32g3/sources/meta-ros/meta-ros-common/recipes-core/images/ros-image-core.bb:do_rootfs) failed with exit code '1'&lt;BR /&gt;NOTE: Tasks Summary: Attempted 9099 tasks of which 9098 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Summary: 1 task failed:&lt;BR /&gt;&amp;nbsp; /yocto-s32g3/sources/meta-ros/meta-ros-common/recipes-core/images/ros-image-core.bb:do_rootfs&lt;BR /&gt;Summary: There was 1 ERROR message, returning a non-zero exit code.&lt;/P&gt;</description>
      <pubDate>Wed, 11 Dec 2024 12:03:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Error-while-integrating-the-HSE-with-yocto/m-p/2012006#M11998</guid>
      <dc:creator>ashwini2024</dc:creator>
      <dc:date>2024-12-11T12:03:08Z</dc:date>
    </item>
    <item>
      <title>Re: Error while integrating the HSE with yocto</title>
      <link>https://community.nxp.com/t5/S32G/Error-while-integrating-the-HSE-with-yocto/m-p/2012065#M12000</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234952"&gt;@ashwini2024&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;Would you mind sharing your local.conf used, and also the command you used to build the Yocto BSP?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Wed, 11 Dec 2024 13:56:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Error-while-integrating-the-HSE-with-yocto/m-p/2012065#M12000</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-12-11T13:56:50Z</dc:date>
    </item>
    <item>
      <title>Re: Error while integrating the HSE with yocto</title>
      <link>https://community.nxp.com/t5/S32G/Error-while-integrating-the-HSE-with-yocto/m-p/2013324#M12021</link>
      <description>&lt;P&gt;The content of the local.conf is :&lt;/P&gt;&lt;P&gt;DISTRO_FEATURES:append = " hse "&lt;/P&gt;&lt;P&gt;NXP_FIRMWARE_LOCAL_DIR = "/yocto-s32g3/folder"&lt;/P&gt;&lt;P&gt;HSE_VERSION="0_2_22_0"&lt;/P&gt;&lt;P&gt;HSE_SOC_REV="rev1.1"&lt;/P&gt;&lt;P&gt;HSE_LIC_MD5 = "a1bda359fc5cdcfca04f84834841a5ca"&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;and the command i used for building is :&lt;BR /&gt;bitbake ros-image-core&lt;/P&gt;</description>
      <pubDate>Fri, 13 Dec 2024 05:48:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Error-while-integrating-the-HSE-with-yocto/m-p/2013324#M12021</guid>
      <dc:creator>ashwini2024</dc:creator>
      <dc:date>2024-12-13T05:48:29Z</dc:date>
    </item>
    <item>
      <title>Re: Error while integrating the HSE with yocto</title>
      <link>https://community.nxp.com/t5/S32G/Error-while-integrating-the-HSE-with-yocto/m-p/2013639#M12024</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/234952"&gt;@ashwini2024&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your reply&lt;/P&gt;
&lt;P&gt;From the BSP40.0 UM, the ubuntu release only support the following images:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="chenyin_h_0-1734097064268.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/315816i13A7BDD0E203AF36/image-size/medium?v=v2&amp;amp;px=400" role="button" title="chenyin_h_0-1734097064268.png" alt="chenyin_h_0-1734097064268.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;chenyin_h_0-1734097064268.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I suggest using "bitbake fsl-image-ubuntu-base" to have another try.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Fri, 13 Dec 2024 13:38:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Error-while-integrating-the-HSE-with-yocto/m-p/2013639#M12024</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-12-13T13:38:52Z</dc:date>
    </item>
  </channel>
</rss>