<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 回复： s32g sja1110 startup in S32G</title>
    <link>https://community.nxp.com/t5/S32G/s32g-sja1110-startup/m-p/2001555#M11852</link>
    <description>&lt;P&gt;hi，&lt;SPAN&gt;jiajun_cheng&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thank you for contacting us.&lt;BR /&gt;1. I will further test the problems encountered in put sja1110_uc.bin and sja1110_switch.bin in /lib/firmwarene.Thank you&amp;nbsp; for your information.&lt;BR /&gt;2. In addition, Refer to UGS32G-VNP-RDB3-ethernet-enablem-guide.pdf (3.sJA1110 Port Configuration) Section 3 (download link S32G-VNP-RDB3 Ethernet:&lt;A href="https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true" target="_blank"&gt;S32G-VNP-RDB3 Ethernet Enablement User Guide&lt;/A&gt;). The&amp;nbsp; User Guide describes how to configure port functionality for SJA1110 using the S32DS.&lt;BR /&gt;3. I think data is written to SJA1110 through SPI, and it should be ok to control SJA1110 with A core or M core. I will conduct internal consultation on the specific reasons and reply to you as soon as possible after getting the result.&lt;/P&gt;
&lt;P&gt;Hope it can help you.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
    <pubDate>Tue, 26 Nov 2024 03:42:03 GMT</pubDate>
    <dc:creator>Joey_z</dc:creator>
    <dc:date>2024-11-26T03:42:03Z</dc:date>
    <item>
      <title>s32g sja1110 startup</title>
      <link>https://community.nxp.com/t5/S32G/s32g-sja1110-startup/m-p/2000792#M11841</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am developing the functions of SJA1110 recently, and I know very little about it. Currently, the SJA1110 S32 SDK is being applied for by the supplier. I can only learn about the functions of SJA1110 through "S32G2_LinuxBSP_39.0_User_Manual.pdf" and posts on the forum. So I have the following questions:&lt;BR /&gt;1. What are the functions of SJA1110 S32 SDK? Can I use this SDK to configure the port functions of SJA1110 on S32DS? Because the network interface of our customized version is slightly different from that of S32G2-VNP-RDB2&lt;BR /&gt;2. At present, because the SJA1110 S32 SDK is being applied for, I downloaded Godvip1.1.0 from the official website. From the user manual, I saw that the supported linux bsp version is 39, and extracted the sja1110 firmware from it. So I also downloaded yocto's bsp39 in my linux environment, and modified the build/conf/local.conf file, added the paths of sja1110_uc.bin and sja1110_switch.bin, and finally compiled and generated the .sdcard file, burned the image to my SD card, and finally loaded it in S32G2-VNP-RDB2. I set SW12 to 1-0 and started from norflash. Finally, I found from the serial port log that the SJA1110 function was not enabled. I put the log in the attachment. Please help me analyze the reason and give suggestions. Thank you&lt;BR /&gt;3. Finally, I would like to ask, for the development of SJA1110, my understanding is that data is written to SJA1110 through SPI, so it should be feasible for A core or M core control;&lt;BR /&gt;3.1 But why do I see in the forum that everyone is basically developing based on A core?&lt;BR /&gt;3.2 If you want to modify the port function of SJA1110, how should you modify it?&lt;BR /&gt;Please give me some suggestions, thank you~&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="SJA1110" id="SJA1110"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;LI-PRODUCT title="S32G2" id="S32G2"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;LI-PRODUCT title="S32G-VNP-RDB2" id="S32G-VNP-RDB2"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Nov 2024 07:18:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g-sja1110-startup/m-p/2000792#M11841</guid>
      <dc:creator>jiajun_cheng</dc:creator>
      <dc:date>2024-11-25T07:18:47Z</dc:date>
    </item>
    <item>
      <title>回复： s32g sja1110 startup</title>
      <link>https://community.nxp.com/t5/S32G/s32g-sja1110-startup/m-p/2001496#M11851</link>
      <description>&lt;P&gt;After reading &lt;A href="https://community.nxp.com/t5/S32G/S32GARDB2-can-not-drive-SJA1110/m-p/1550978" target="_self"&gt;this article&lt;/A&gt;, I chose to put sja1110_uc.bin and sja1110_switch.bin in /lib/firmware, and the log is as follows&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;root@s32g274ardb2:~# dmesg | grep sja&lt;BR /&gt;[ 0.544308] gpio-345 (sja1110-rst-phy-t1): hogged as output/low&lt;BR /&gt;[ 0.549823] gpio-402 (sja1110-rst-core): hogged as output/low&lt;BR /&gt;[ 0.615697] sja1110-sw@1 enforce active low on chipselect handle&lt;BR /&gt;[ 7.283003] sja1110: loading out-of-tree module taints kernel.&lt;BR /&gt;[ 7.290192] SPI driver sja1110 has no spi_device_id for nxp,sja1110-switch&lt;BR /&gt;[ 7.290198] SPI driver sja1110 has no spi_device_id for nxp,sja1110-uc&lt;BR /&gt;[ 7.290309] sja1110 spi5.0: probing uc&lt;BR /&gt;[ 7.290468] sja1110 spi5.1: probing switch&lt;BR /&gt;[ 7.290781] sja1110 spi5.1: Could not get GPIO from device tree&lt;BR /&gt;[ 7.290809] sja1110 spi5.1: [sja1110_post_probe_upload_worker] Trying to initializ e switch&lt;BR /&gt;[ 7.294511] sja1110 spi5.1: [sja1110_init_hw] loaded fw 'sja1110_switch.bin'&lt;BR /&gt;[ 7.294621] sja1110 spi5.1: [sja1110_pre_switch_upload] Found switch config of siz e 2236&lt;BR /&gt;[ 7.294768] sja1110 spi5.1: Uploading config...&lt;BR /&gt;[ 7.373625] sja1110 spi5.1: Successfully configured!&lt;BR /&gt;[ 7.373655] sja1110 spi5.0: [sja1110_post_probe_upload_worker] Trying to initializ e uC&lt;BR /&gt;[ 7.394231] sja1110 spi5.0: [sja1110_init_hw] loaded fw 'sja1110_uc.bin'&lt;BR /&gt;[ 7.394252] sja1110 spi5.0: [sja1110_pre_uc_upload] Found firmware of size 320280&lt;BR /&gt;[ 7.394370] sja1110 spi5.0: [sja1110_pre_uc_upload] firmware appears to be valid&lt;BR /&gt;[ 7.394422] sja1110 spi5.0: [sja1110_pre_uc_upload] µC not ready for download (Sta tus=0x31)&lt;BR /&gt;[ 7.394649] sja1110 spi5.0: Uploading firmware...&lt;BR /&gt;[ 8.200328] sja1110 spi5.0: Upload successfully verified!&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Nov 2024 02:22:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g-sja1110-startup/m-p/2001496#M11851</guid>
      <dc:creator>jiajun_cheng</dc:creator>
      <dc:date>2024-11-26T02:22:17Z</dc:date>
    </item>
    <item>
      <title>回复： s32g sja1110 startup</title>
      <link>https://community.nxp.com/t5/S32G/s32g-sja1110-startup/m-p/2001555#M11852</link>
      <description>&lt;P&gt;hi，&lt;SPAN&gt;jiajun_cheng&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thank you for contacting us.&lt;BR /&gt;1. I will further test the problems encountered in put sja1110_uc.bin and sja1110_switch.bin in /lib/firmwarene.Thank you&amp;nbsp; for your information.&lt;BR /&gt;2. In addition, Refer to UGS32G-VNP-RDB3-ethernet-enablem-guide.pdf (3.sJA1110 Port Configuration) Section 3 (download link S32G-VNP-RDB3 Ethernet:&lt;A href="https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true" target="_blank"&gt;S32G-VNP-RDB3 Ethernet Enablement User Guide&lt;/A&gt;). The&amp;nbsp; User Guide describes how to configure port functionality for SJA1110 using the S32DS.&lt;BR /&gt;3. I think data is written to SJA1110 through SPI, and it should be ok to control SJA1110 with A core or M core. I will conduct internal consultation on the specific reasons and reply to you as soon as possible after getting the result.&lt;/P&gt;
&lt;P&gt;Hope it can help you.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;</description>
      <pubDate>Tue, 26 Nov 2024 03:42:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g-sja1110-startup/m-p/2001555#M11852</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2024-11-26T03:42:03Z</dc:date>
    </item>
    <item>
      <title>回复： s32g sja1110 startup</title>
      <link>https://community.nxp.com/t5/S32G/s32g-sja1110-startup/m-p/2001987#M11858</link>
      <description>&lt;P&gt;Hi，&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/236188"&gt;@Joey_z&lt;/a&gt;&amp;nbsp;:&lt;/P&gt;&lt;P&gt;In the afternoon, my SJA1110 SDK application was approved, and I followed" &lt;SPAN class=""&gt;S32G-VNP-RDB3 Ethernet Enablement Guide&lt;/SPAN&gt;"Loaded switch_uc.bin.For the configuration of sja1110, is there any article for RDB2 development board.Is there any article that explains it in more detail?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;s32g274ardb2 login: root
root@s32g274ardb2:~# dmesg | grep sja1110
[    0.548540] gpio-24 (sja1110-rst-phy-t1): hogged as output/low
[    0.553963] gpio-81 (sja1110-rst-core): hogged as output/low
[    0.619550] sja1110-sw@1 enforce active low on chipselect handle
[    8.417247] sja1110: loading out-of-tree module taints kernel.
[    8.417843] SPI driver sja1110 has no spi_device_id for nxp,sja1110-switch
[    8.417852] SPI driver sja1110 has no spi_device_id for nxp,sja1110-uc
[    8.417961] sja1110 spi5.0: probing uc
[    8.418121] sja1110 spi5.1: probing switch
[    8.418445] sja1110 spi5.1: Could not get GPIO from device tree
[    8.418473] sja1110 spi5.1: [sja1110_post_probe_upload_worker] Trying to initialize switch
[    8.418628] sja1110 spi5.1: Direct firmware load for sja1110_switch.bin failed with error -2
[    8.418641] sja1110 spi5.1: request_firmware failed with -2
[    8.418648] sja1110 spi5.0: [sja1110_post_probe_upload_worker] Trying to initialize uC
[    8.425720] sja1110 spi5.0: [sja1110_init_hw] loaded fw 'sja1110_uc.bin'
[    8.425740] sja1110 spi5.0: [sja1110_pre_uc_upload] Found firmware of size 126400
[    8.425844] sja1110 spi5.0: [sja1110_pre_uc_upload] firmware appears to be valid
[    8.425896] sja1110 spi5.0: [sja1110_pre_uc_upload] \xc2\xb5C not ready for download (Status=0x31)
[    8.426017] sja1110 spi5.0: Uploading firmware...
[    8.733955] sja1110 spi5.0: Upload successfully verified!&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Nov 2024 12:16:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g-sja1110-startup/m-p/2001987#M11858</guid>
      <dc:creator>jiajun_cheng</dc:creator>
      <dc:date>2024-11-26T12:16:58Z</dc:date>
    </item>
    <item>
      <title>回复： s32g sja1110 startup</title>
      <link>https://community.nxp.com/t5/S32G/s32g-sja1110-startup/m-p/2002387#M11863</link>
      <description>&lt;P&gt;hi，&lt;SPAN&gt;jiajun_cheng&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thank you for your reply.&lt;/P&gt;
&lt;P&gt;For details, see 4. SJA1110 Port4 PHY Speed Configuration in the S32G-VNP-RDB2 Reference Design Ethernet Enablement Guide (download link&lt;SPAN&gt;：&lt;/SPAN&gt;&lt;A href="https://www.nxp.com.cn/webapp/sps/download/preDownload.jsp?render=true" target="_blank"&gt;&lt;SPAN&gt;S32G-VNP-RDB2 Reference Design Ethernet Enablement Guide&lt;/SPAN&gt;&lt;/A&gt;)&lt;/P&gt;
&lt;P&gt;In addition, “Upload successfully verified” means SJA1110 image loaded successfully, and SJA1110 Port will work on your configuration&lt;/P&gt;
&lt;P&gt;Hope it can help you.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Joey&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Nov 2024 02:33:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32g-sja1110-startup/m-p/2002387#M11863</guid>
      <dc:creator>Joey_z</dc:creator>
      <dc:date>2024-11-27T02:33:54Z</dc:date>
    </item>
  </channel>
</rss>