<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32G3 - HSE FW Install directly without IVT in S32G</title>
    <link>https://community.nxp.com/t5/S32G/S32G3-HSE-FW-Install-directly-without-IVT/m-p/1996486#M11757</link>
    <description>&lt;P&gt;Hello, My goal is to be able to flash the HSE and then test the crypto services.&lt;/P&gt;&lt;P&gt;I need to flash the HSE directly using the Lauterbach debugger without the need to flash/create an IVT.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When i tried to directly flash the bin/hex file of the HSE, i find that the dedicated area for the HSE is not accessible (??s in T32 window) -&amp;gt; Address 0x22000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a way to enable the HSE memory area (maybe with a cmm script) so that i can flash it accordingly?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;</description>
    <pubDate>Mon, 18 Nov 2024 14:51:26 GMT</pubDate>
    <dc:creator>SahaarA</dc:creator>
    <dc:date>2024-11-18T14:51:26Z</dc:date>
    <item>
      <title>S32G3 - HSE FW Install directly without IVT</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-HSE-FW-Install-directly-without-IVT/m-p/1996486#M11757</link>
      <description>&lt;P&gt;Hello, My goal is to be able to flash the HSE and then test the crypto services.&lt;/P&gt;&lt;P&gt;I need to flash the HSE directly using the Lauterbach debugger without the need to flash/create an IVT.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When i tried to directly flash the bin/hex file of the HSE, i find that the dedicated area for the HSE is not accessible (??s in T32 window) -&amp;gt; Address 0x22000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a way to enable the HSE memory area (maybe with a cmm script) so that i can flash it accordingly?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;</description>
      <pubDate>Mon, 18 Nov 2024 14:51:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-HSE-FW-Install-directly-without-IVT/m-p/1996486#M11757</guid>
      <dc:creator>SahaarA</dc:creator>
      <dc:date>2024-11-18T14:51:26Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 - HSE FW Install directly without IVT</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-HSE-FW-Install-directly-without-IVT/m-p/1997423#M11774</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243477"&gt;@SahaarA&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;If I understood your problem correctly, you should be able to load and debug an application using the crypto services following the instructions in&amp;nbsp;&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/application-note/AN14070.pdf" target="_blank"&gt;AN14070 -&amp;nbsp;How to Run HSE Demo Application&lt;/A&gt;, please check section&amp;nbsp;&lt;STRONG&gt;How to load the HSE demo .elf to the SRAM&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="alejandro_e_0-1732040629780.png" style="width: 562px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/311310i3D1AAB0B56FBF504/image-dimensions/562x146?v=v2" width="562" height="146" role="button" title="alejandro_e_0-1732040629780.png" alt="alejandro_e_0-1732040629780.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if this information solves your problem.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Alejandro&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Nov 2024 18:25:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-HSE-FW-Install-directly-without-IVT/m-p/1997423#M11774</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2024-11-19T18:25:50Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 - HSE FW Install directly without IVT</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-HSE-FW-Install-directly-without-IVT/m-p/1998012#M11786</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/238460"&gt;@alejandro_e&lt;/a&gt;&amp;nbsp;,&amp;nbsp;&lt;/P&gt;&lt;P&gt;From what i understand, we can boot the board either from RAM or from QSPI.&lt;/P&gt;&lt;P&gt;Booting from QSPI needs a blob image, such that the HSE and Application would then be loaded to the RAM.&lt;/P&gt;&lt;P&gt;The other way is flashing directly to the RAM using a debugger, which I'm currently doing.&amp;nbsp;&lt;/P&gt;&lt;P&gt;For the Application, i can directly flash it with the debugger in the desired memory address.&lt;/P&gt;&lt;P&gt;But for the HSE, the memory region is not accessible by the debugger. so i guess the HSE partition starting address 0x22000000 needs to be enabled somehow, like with a cmm script enabling the clock or something.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I saw some other ways where the HSE can be flashed without the IVT but on other targets like the DCF options in S32K, so i'm wondering if there is a similar way but for S32G3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank You,&lt;/P&gt;&lt;P&gt;Sahar.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Nov 2024 12:22:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-HSE-FW-Install-directly-without-IVT/m-p/1998012#M11786</guid>
      <dc:creator>SahaarA</dc:creator>
      <dc:date>2024-11-20T12:22:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 - HSE FW Install directly without IVT</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-HSE-FW-Install-directly-without-IVT/m-p/1998118#M11787</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243477"&gt;@SahaarA&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;It is not possible to access HSE memory, as you can see in the memory map attached to the &lt;A href="https://www.nxp.com/webapp/Download?colCode=RMS32G3" target="_blank"&gt;S32G3 Reference manual&lt;/A&gt;:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="alejandro_e_0-1732118540616.png" style="width: 592px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/311480i63084C93E6A9E8C4/image-dimensions/592x37?v=v2" width="592" height="37" role="button" title="alejandro_e_0-1732118540616.png" alt="alejandro_e_0-1732118540616.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;The steps I mentioned before will help you debugging your HSE application, but you cannot write the HSE FW directly like it is done in the S32K microcontrollers.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if this information answers your questions.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Nov 2024 16:13:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-HSE-FW-Install-directly-without-IVT/m-p/1998118#M11787</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2024-11-20T16:13:43Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 - HSE FW Install directly without IVT</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-HSE-FW-Install-directly-without-IVT/m-p/1998735#M11799</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/238460"&gt;@alejandro_e&lt;/a&gt;&amp;nbsp;,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes actually that answers my question.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was just wondering if there was a way to access the HSE directly, but now i just have to flash it with a blob image as mentioned in the documentation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank You,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sahar&lt;/P&gt;</description>
      <pubDate>Thu, 21 Nov 2024 09:17:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-HSE-FW-Install-directly-without-IVT/m-p/1998735#M11799</guid>
      <dc:creator>SahaarA</dc:creator>
      <dc:date>2024-11-21T09:17:05Z</dc:date>
    </item>
    <item>
      <title>Re: S32G3 - HSE FW Install directly without IVT</title>
      <link>https://community.nxp.com/t5/S32G/S32G3-HSE-FW-Install-directly-without-IVT/m-p/1999155#M11809</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/243477"&gt;@SahaarA&lt;/a&gt;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I'm glad to know that the information answers your question. Thanks for letting me know and thanks for accepting my reply as a solution.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Alejandro&lt;/P&gt;</description>
      <pubDate>Thu, 21 Nov 2024 17:18:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G3-HSE-FW-Install-directly-without-IVT/m-p/1999155#M11809</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2024-11-21T17:18:49Z</dc:date>
    </item>
  </channel>
</rss>