<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Accessing DDR memory controller from M7 cores in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Accessing-DDR-memory-controller-from-M7-cores/m-p/1992198#M11672</link>
    <description>&lt;P&gt;is the length of the DDR registers dependent on the memory size? for example, if the DDR memory size is above 2GB, then all DDR registers or some of them must be 64-bit? in that case are these registers accessible from the M7 cores? does these registers require atomic access?&amp;nbsp; if so, is there a way to mitigate this?&lt;/P&gt;</description>
    <pubDate>Mon, 11 Nov 2024 19:58:23 GMT</pubDate>
    <dc:creator>maboeln11</dc:creator>
    <dc:date>2024-11-11T19:58:23Z</dc:date>
    <item>
      <title>Accessing DDR memory controller from M7 cores</title>
      <link>https://community.nxp.com/t5/S32G/Accessing-DDR-memory-controller-from-M7-cores/m-p/1992198#M11672</link>
      <description>&lt;P&gt;is the length of the DDR registers dependent on the memory size? for example, if the DDR memory size is above 2GB, then all DDR registers or some of them must be 64-bit? in that case are these registers accessible from the M7 cores? does these registers require atomic access?&amp;nbsp; if so, is there a way to mitigate this?&lt;/P&gt;</description>
      <pubDate>Mon, 11 Nov 2024 19:58:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Accessing-DDR-memory-controller-from-M7-cores/m-p/1992198#M11672</guid>
      <dc:creator>maboeln11</dc:creator>
      <dc:date>2024-11-11T19:58:23Z</dc:date>
    </item>
  </channel>
</rss>