<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Access to eIQ auto ML toolkit in S32G</title>
    <link>https://community.nxp.com/t5/S32G/Access-to-eIQ-auto-ML-toolkit/m-p/1988513#M11599</link>
    <description>&lt;P&gt;Hello， &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220976"&gt;@Geonha_&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;As far as I know, when sharing with the AI related packages to the customer, they have all signed the NDAs.&lt;/P&gt;
&lt;P&gt;I could help to double confirm it, if there is any changes(if the standard version could be used without NDA), I will update the status here.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
    <pubDate>Wed, 06 Nov 2024 06:23:45 GMT</pubDate>
    <dc:creator>chenyin_h</dc:creator>
    <dc:date>2024-11-06T06:23:45Z</dc:date>
    <item>
      <title>Access to eIQ auto ML toolkit</title>
      <link>https://community.nxp.com/t5/S32G/Access-to-eIQ-auto-ML-toolkit/m-p/1987610#M11584</link>
      <description>&lt;P&gt;Hello!&lt;BR /&gt;&lt;BR /&gt;I'm planning to use the GOLDBOX3 platform from NXP to research model optimization methods for machine learning applications in a vehicle-embedded environment.&lt;/P&gt;&lt;P&gt;To achieve this, I aim to explore performance baselines and investigate optimization methods using the NXP-AUTO-ML toolkit.&lt;/P&gt;&lt;P&gt;My question is, without signing an NDA, is it completely inaccessible?&lt;/P&gt;&lt;P&gt;In the presentation here(&lt;A href="https://www.nxp.com/design/design-center/training/TIP-ACCELERATING-VEHICLE-INTELLIGENCE-MACHINE-LEAR" target="_blank"&gt;https://www.nxp.com/design/design-center/training/TIP-ACCELERATING-VEHICLE-INTELLIGENCE-MACHINE-LEAR&lt;/A&gt;), it mentions that a standard version is also available, but I haven’t been able to locate it anywhere.&lt;/P&gt;&lt;P&gt;If anyone has had similar concerns, I’d appreciate any advice.&lt;/P&gt;&lt;P&gt;Thank you!!&lt;/P&gt;</description>
      <pubDate>Tue, 05 Nov 2024 03:47:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Access-to-eIQ-auto-ML-toolkit/m-p/1987610#M11584</guid>
      <dc:creator>Geonha_</dc:creator>
      <dc:date>2024-11-05T03:47:56Z</dc:date>
    </item>
    <item>
      <title>Re: Access to eIQ auto ML toolkit</title>
      <link>https://community.nxp.com/t5/S32G/Access-to-eIQ-auto-ML-toolkit/m-p/1988513#M11599</link>
      <description>&lt;P&gt;Hello， &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220976"&gt;@Geonha_&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;As far as I know, when sharing with the AI related packages to the customer, they have all signed the NDAs.&lt;/P&gt;
&lt;P&gt;I could help to double confirm it, if there is any changes(if the standard version could be used without NDA), I will update the status here.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 06:23:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Access-to-eIQ-auto-ML-toolkit/m-p/1988513#M11599</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-11-06T06:23:45Z</dc:date>
    </item>
  </channel>
</rss>