<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックCertificate slots</title>
    <link>https://community.nxp.com/t5/S32G/Certificate-slots/m-p/1977790#M11345</link>
    <description>&lt;P&gt;Hi team,&lt;/P&gt;&lt;P&gt;Following are the Hardware details that I'm currently using,&lt;/P&gt;&lt;P&gt;Board: S32G399RDB3 with Autosar application in M7 core and BSP.V.40 used in the A core.&lt;/P&gt;&lt;P&gt;I am using the HSE Standard version, below are some of the questions I have,&lt;/P&gt;&lt;P&gt;1. I noticed that there are no certificate slots defined as "&lt;SPAN&gt;HSE_KEY_TYPE_ECC_PUB_EXT"&amp;nbsp;&lt;/SPAN&gt;in HSE. Is it required for me to use the HSE Premium version? If yes, then how do we get it?&lt;/P&gt;&lt;P&gt;2. Can we modify the HSE application code for the premium version SW package according to our requirements?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Jayateerth&lt;/P&gt;</description>
    <pubDate>Mon, 21 Oct 2024 06:35:05 GMT</pubDate>
    <dc:creator>Jayateerth</dc:creator>
    <dc:date>2024-10-21T06:35:05Z</dc:date>
    <item>
      <title>Certificate slots</title>
      <link>https://community.nxp.com/t5/S32G/Certificate-slots/m-p/1977790#M11345</link>
      <description>&lt;P&gt;Hi team,&lt;/P&gt;&lt;P&gt;Following are the Hardware details that I'm currently using,&lt;/P&gt;&lt;P&gt;Board: S32G399RDB3 with Autosar application in M7 core and BSP.V.40 used in the A core.&lt;/P&gt;&lt;P&gt;I am using the HSE Standard version, below are some of the questions I have,&lt;/P&gt;&lt;P&gt;1. I noticed that there are no certificate slots defined as "&lt;SPAN&gt;HSE_KEY_TYPE_ECC_PUB_EXT"&amp;nbsp;&lt;/SPAN&gt;in HSE. Is it required for me to use the HSE Premium version? If yes, then how do we get it?&lt;/P&gt;&lt;P&gt;2. Can we modify the HSE application code for the premium version SW package according to our requirements?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Jayateerth&lt;/P&gt;</description>
      <pubDate>Mon, 21 Oct 2024 06:35:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Certificate-slots/m-p/1977790#M11345</guid>
      <dc:creator>Jayateerth</dc:creator>
      <dc:date>2024-10-21T06:35:05Z</dc:date>
    </item>
    <item>
      <title>Re: Certificate slots</title>
      <link>https://community.nxp.com/t5/S32G/Certificate-slots/m-p/1979162#M11377</link>
      <description>&lt;P&gt;Hello, &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241687"&gt;@Jayateerth&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your post.&lt;/P&gt;
&lt;P&gt;May I know which version HSE FW you are working with? I have checked the FW0.2.22, and found that HSE_KEY_TYPE_ECC_PUB_EXT is defined under hse_keymgmt_common_types.h, would you please double check on it.&lt;/P&gt;
&lt;P&gt;For premium package related questions, I suggest submiting a ticket via the support channel, or contacting&lt;/P&gt;
&lt;P&gt;your DFAE/FAE for further support on this topic.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Chenyin&lt;/P&gt;</description>
      <pubDate>Tue, 22 Oct 2024 10:40:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/Certificate-slots/m-p/1979162#M11377</guid>
      <dc:creator>chenyin_h</dc:creator>
      <dc:date>2024-10-22T10:40:29Z</dc:date>
    </item>
  </channel>
</rss>