<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32GのトピックRe: S32G IPCF communication problem</title>
    <link>https://community.nxp.com/t5/S32G/S32G-IPCF-communication-problem/m-p/1974505#M11252</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224758"&gt;@Alex_mjl&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thanks for the information. I will share this topic with the internal team&amp;nbsp; and let you know if we have specific data on the IPCF latency. For now I can tell you that IPCF transfers are faster than the protocols you mentioned, so it will not be a bottleneck in your application.&lt;/P&gt;
&lt;P&gt;I will get back to you as soon as I have new information.&lt;/P&gt;</description>
    <pubDate>Tue, 15 Oct 2024 17:57:00 GMT</pubDate>
    <dc:creator>alejandro_e</dc:creator>
    <dc:date>2024-10-15T17:57:00Z</dc:date>
    <item>
      <title>S32G IPCF communication problem</title>
      <link>https://community.nxp.com/t5/S32G/S32G-IPCF-communication-problem/m-p/1973459#M11215</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;I am using the S32G274A chip.&amp;nbsp;I want to know what is the bandwidth and latency of core A and core M when they use IPCF for inter-core communication.&amp;nbsp;These parameters do not appear to be mentioned in the user manual.&lt;/P&gt;</description>
      <pubDate>Mon, 14 Oct 2024 16:12:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-IPCF-communication-problem/m-p/1973459#M11215</guid>
      <dc:creator>Alex_mjl</dc:creator>
      <dc:date>2024-10-14T16:12:30Z</dc:date>
    </item>
    <item>
      <title>Re: S32G IPCF communication problem</title>
      <link>https://community.nxp.com/t5/S32G/S32G-IPCF-communication-problem/m-p/1973629#M11219</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224758"&gt;@Alex_mjl&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thanks for contacting NXP support. About your question, we don't have public latency data related to transfers between the cores A and M. Could you tell me more information about your setup so I may share the information with the internal team, and ask if there is performance data related to the IPCF in the S32G2? please help me providing the following:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Are you using the RDB2 or a custom board?&lt;/LI&gt;
&lt;LI&gt;Which BSP are you using?&lt;/LI&gt;
&lt;LI&gt;Which configuration are you using for the M7 core, Bare-Metal, FreeRTOS, AUTOSAR?&lt;/LI&gt;
&lt;LI&gt;could you describe a little about the scenario in which you are going to use IPCF?&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks in advance for the information.&lt;/P&gt;</description>
      <pubDate>Mon, 14 Oct 2024 21:45:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-IPCF-communication-problem/m-p/1973629#M11219</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2024-10-14T21:45:13Z</dc:date>
    </item>
    <item>
      <title>Re: S32G IPCF communication problem</title>
      <link>https://community.nxp.com/t5/S32G/S32G-IPCF-communication-problem/m-p/1973698#M11223</link>
      <description>&lt;P&gt;Hi alejandro_e,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;Thank you for your reply. Pls allow me to describe the use case first:&amp;nbsp;I want to use M-core to collect low speed bus data, such as CAN, LIN, FlexRay, etc.&amp;nbsp;Then the collected data is sent to A-core through IPCF for calculation. That's why I want to know the bandwidth and latency of IPCF communication.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;Now let me answer your question:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN&gt;custom board&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;BSP38&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;bare metal&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Tue, 15 Oct 2024 01:21:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-IPCF-communication-problem/m-p/1973698#M11223</guid>
      <dc:creator>Alex_mjl</dc:creator>
      <dc:date>2024-10-15T01:21:58Z</dc:date>
    </item>
    <item>
      <title>Re: S32G IPCF communication problem</title>
      <link>https://community.nxp.com/t5/S32G/S32G-IPCF-communication-problem/m-p/1974505#M11252</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224758"&gt;@Alex_mjl&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Thanks for the information. I will share this topic with the internal team&amp;nbsp; and let you know if we have specific data on the IPCF latency. For now I can tell you that IPCF transfers are faster than the protocols you mentioned, so it will not be a bottleneck in your application.&lt;/P&gt;
&lt;P&gt;I will get back to you as soon as I have new information.&lt;/P&gt;</description>
      <pubDate>Tue, 15 Oct 2024 17:57:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-IPCF-communication-problem/m-p/1974505#M11252</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2024-10-15T17:57:00Z</dc:date>
    </item>
    <item>
      <title>Re: S32G IPCF communication problem</title>
      <link>https://community.nxp.com/t5/S32G/S32G-IPCF-communication-problem/m-p/1980345#M11404</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224758"&gt;@Alex_mjl&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Sorry for the late reply, the internal team was overloaded this past week. They provided the following information:&lt;/P&gt;
&lt;P&gt;"&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#808080"&gt;Since the IPCF is&amp;nbsp;&lt;SPAN&gt;share memory based, it won't be the&amp;nbsp;bottleneck for those low data volume applications.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#808080"&gt;&lt;SPAN&gt;Regarding the latency, a processing latency exists and depends on the interrupt handler on the A53 OS side.&amp;nbsp;&lt;/SPAN&gt;We don't have the latency result of the interrupt handler. Customer integrates the IPCF into their OS, it varies and depends on the OS they choose.&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;"&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please let me know if this information answers your question.&lt;/P&gt;</description>
      <pubDate>Wed, 23 Oct 2024 15:26:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/S32G-IPCF-communication-problem/m-p/1980345#M11404</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2024-10-23T15:26:53Z</dc:date>
    </item>
  </channel>
</rss>