<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: s32G274RDB2 using BSP ATF in S32G</title>
    <link>https://community.nxp.com/t5/S32G/s32G274RDB2-using-BSP-ATF/m-p/1973744#M11225</link>
    <description>I was able to start both core A and core M, but once executing the bitbake arm-trusted- firmware-c cleansstate command, Cleansstate won't recover, so the IVT setup should be fine. The modified part is refer to 0001-fip-align-and-mmc-init.patch in AN13750SW-Software for application note AN13750. So there should be other changes in BSP35.0.</description>
    <pubDate>Tue, 15 Oct 2024 02:37:34 GMT</pubDate>
    <dc:creator>sdx111</dc:creator>
    <dc:date>2024-10-15T02:37:34Z</dc:date>
    <item>
      <title>s32G274RDB2 using BSP ATF</title>
      <link>https://community.nxp.com/t5/S32G/s32G274RDB2-using-BSP-ATF/m-p/1963576#M10958</link>
      <description>&lt;P&gt;I am using the construction method of BSP35.0 yocto. The fip.bin and fip.s32 generated here are generated by FIp.s32-qSPI, and I want to be generated by FIp.s32-sdcard instead. Where can I make this change?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="sdx111_0-1727442540029.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/301727i6F2C36E9FD0652CB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sdx111_0-1727442540029.png" alt="sdx111_0-1727442540029.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;sdx111_0-1727442540029.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Sep 2024 13:11:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32G274RDB2-using-BSP-ATF/m-p/1963576#M10958</guid>
      <dc:creator>sdx111</dc:creator>
      <dc:date>2024-09-27T13:11:43Z</dc:date>
    </item>
    <item>
      <title>Re: s32G274RDB2 using BSP ATF</title>
      <link>https://community.nxp.com/t5/S32G/s32G274RDB2-using-BSP-ATF/m-p/1963800#M10965</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231473"&gt;@sdx111&lt;/a&gt;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is no documented way to change the fip.bin/s32 to be the same as the sdcard instead of the qspi. Can you describe more about your problem? What are you traying to solve with this change?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks in advance for the information&lt;/P&gt;</description>
      <pubDate>Sat, 28 Sep 2024 02:51:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32G274RDB2-using-BSP-ATF/m-p/1963800#M10965</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2024-09-28T02:51:42Z</dc:date>
    </item>
    <item>
      <title>Re: s32G274RDB2 using BSP ATF</title>
      <link>https://community.nxp.com/t5/S32G/s32G274RDB2-using-BSP-ATF/m-p/1963859#M10966</link>
      <description>I was debugging the bootloader and starting M7 core and A53 core. I needed to download fip.bin of A53 core to Norflash and fip.s32 to EMMC, but startup errors occurred. NOTICE: Reset status: Power-On Reset&lt;BR /&gt;NOTICE: BL2: v2.5(release):bsp35.0-2.5-dirty&lt;BR /&gt;NOTICE: BL2: Built : 13:21:28, Nov 29 2022&lt;BR /&gt;Warning: Instruction at BL33_ENTRYPOINT (0xffaa0000) is 0x54000100, which is not a B or BL!&lt;BR /&gt;NOTICE: BL2: Booting BL31&lt;BR /&gt;&lt;BR /&gt;I think that this generated fip.s32 does not correspond to the download to EMMC.</description>
      <pubDate>Sun, 29 Sep 2024 01:53:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32G274RDB2-using-BSP-ATF/m-p/1963859#M10966</guid>
      <dc:creator>sdx111</dc:creator>
      <dc:date>2024-09-29T01:53:46Z</dc:date>
    </item>
    <item>
      <title>Re: s32G274RDB2 using BSP ATF</title>
      <link>https://community.nxp.com/t5/S32G/s32G274RDB2-using-BSP-ATF/m-p/1964828#M10997</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231473"&gt;@sdx111&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You can flash the file with the &lt;STRONG&gt;sdcard&amp;nbsp;&lt;/STRONG&gt;suffix with no problem or rename it yourself with no issues. If you require an multicore application I can recommend checking&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN13750" target="_blank"&gt;AN13750: Enabling Multicore Application&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;If you keep having problems please share more details about the complete process you are following, this is: Bootloader configuration, Changes to ATF/u-boot code, building commands, flashing commands and dip switch configuration when booting.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if this information was useful.&lt;/P&gt;</description>
      <pubDate>Mon, 30 Sep 2024 23:21:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32G274RDB2-using-BSP-ATF/m-p/1964828#M10997</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2024-09-30T23:21:33Z</dc:date>
    </item>
    <item>
      <title>Re: s32G274RDB2 using BSP ATF</title>
      <link>https://community.nxp.com/t5/S32G/s32G274RDB2-using-BSP-ATF/m-p/1973322#M11211</link>
      <description>&lt;P&gt;With reference to AN13750, modify the patch shown in the following figure to build bitbake arm-trusted- firmfirmware -C compile and bitbake fsl-image-auto. During boot, the DIP code is Norflash startup, and dual-core startup is shown in the figure below.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would like to know what other programs in BSP35.0 need to be changed?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="sdx111_0-1728907094433.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/304543i307FCB0ABE16BB08/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sdx111_0-1728907094433.png" alt="sdx111_0-1728907094433.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;sdx111_0-1728907094433.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="sdx111_1-1728907109749.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/304544i264906CDD81EDC31/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sdx111_1-1728907109749.png" alt="sdx111_1-1728907109749.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;sdx111_1-1728907109749.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Oct 2024 11:59:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32G274RDB2-using-BSP-ATF/m-p/1973322#M11211</guid>
      <dc:creator>sdx111</dc:creator>
      <dc:date>2024-10-14T11:59:15Z</dc:date>
    </item>
    <item>
      <title>Re: s32G274RDB2 using BSP ATF</title>
      <link>https://community.nxp.com/t5/S32G/s32G274RDB2-using-BSP-ATF/m-p/1973659#M11220</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231473"&gt;@sdx111&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;All the steps related to change files are present in the application note I mentioned, it is useful to have previous IVT configuration experience. If this is your first time configuring an IVT image I strongly recommend checking&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=S32G-VNP-RDB2-SW-UG" target="_blank"&gt;S32G-VNP-RDB2 Software Enablement Guide&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Please be aware that you will need to download the following package&amp;nbsp;&lt;A id="relatedDocsClickPDF_1" class="dtmcustomrulelink" href="https://www.nxp.com/docs/en/application-note-software/AN13750SW.zip" target="_blank" rel="noopener" data-dtmaction="Documentation Section - Results Link Click" data-dtmsubaction="AN13750SW - Software for application note AN13750 - NXP - Application Note Software - English"&gt;&lt;SPAN&gt;AN&lt;SPAN class="highlight"&gt;13750&lt;/SPAN&gt;SW - Software for application note AN&lt;SPAN class="highlight"&gt;13750&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/A&gt;&amp;nbsp;to be able to complete the application note.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if this information was useful.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Oct 2024 23:10:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32G274RDB2-using-BSP-ATF/m-p/1973659#M11220</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2024-10-14T23:10:31Z</dc:date>
    </item>
    <item>
      <title>Re: s32G274RDB2 using BSP ATF</title>
      <link>https://community.nxp.com/t5/S32G/s32G274RDB2-using-BSP-ATF/m-p/1973744#M11225</link>
      <description>I was able to start both core A and core M, but once executing the bitbake arm-trusted- firmware-c cleansstate command, Cleansstate won't recover, so the IVT setup should be fine. The modified part is refer to 0001-fip-align-and-mmc-init.patch in AN13750SW-Software for application note AN13750. So there should be other changes in BSP35.0.</description>
      <pubDate>Tue, 15 Oct 2024 02:37:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32G274RDB2-using-BSP-ATF/m-p/1973744#M11225</guid>
      <dc:creator>sdx111</dc:creator>
      <dc:date>2024-10-15T02:37:34Z</dc:date>
    </item>
    <item>
      <title>Re: s32G274RDB2 using BSP ATF</title>
      <link>https://community.nxp.com/t5/S32G/s32G274RDB2-using-BSP-ATF/m-p/1974525#M11253</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231473"&gt;@sdx111&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could you elaborate more on how you added the patches to your yocto build? what steps did you follow to add the mentioned modifications?&lt;/P&gt;
&lt;P&gt;Are there any log errors when you try to run the&amp;nbsp;&lt;STRONG&gt;&lt;SPAN&gt;bitbake arm-trusted- firmware-c cleansstate&lt;/SPAN&gt;&lt;/STRONG&gt;&amp;nbsp;command? can you share them with me?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks in advance for the information.&lt;/P&gt;</description>
      <pubDate>Tue, 15 Oct 2024 18:26:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/s32G274RDB2-using-BSP-ATF/m-p/1974525#M11253</guid>
      <dc:creator>alejandro_e</dc:creator>
      <dc:date>2024-10-15T18:26:11Z</dc:date>
    </item>
  </channel>
</rss>