<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Re: An error occurs when compiling the IPCF_Example_multi_instance_S32G274_M7_0 project</title>
    <link>https://community.nxp.com/t5/S32G/An-error-occurs-when-compiling-the-IPCF-Example-multi-instance/m-p/1972050#M11145</link>
    <description>&lt;P&gt;Hello&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;很高兴听到你的问题解决了。目前没有关于 S32G3 的双核启动的类似 AN13750.pdf 的文档，并且也没有发布此类文档的计划。这是因为 S32G3 的 GoldVIP 里面已经有双核启动了。我认为 AN13750 对你仍具有一定的参考价值，因为思路是一致的。以下这个案例可能会对你有所帮助：&lt;A href="https://community.nxp.com/t5/S32G/S32G399A-RDB3-Multi-core-boot-failed-following-AN13750/m-p/1753196" target="_self"&gt;Solved: S32G399A-RDB3-Multi-core-boot-failed-following-AN13750&lt;/A&gt;&amp;nbsp;。&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;</description>
    <pubDate>Fri, 01 Nov 2024 07:50:45 GMT</pubDate>
    <dc:creator>Celeste_Liu</dc:creator>
    <dc:date>2024-11-01T07:50:45Z</dc:date>
    <item>
      <title>An error occurs when compiling the IPCF_Example_multi_instance_S32G274_M7_0 project</title>
      <link>https://community.nxp.com/t5/S32G/An-error-occurs-when-compiling-the-IPCF-Example-multi-instance/m-p/1971039#M11123</link>
      <description>&lt;P&gt;Hi nxp,&lt;/P&gt;&lt;P&gt;我正在使用&amp;nbsp;S32 Design Studio for S32 Platform 3.5 编译“IPCF_Example_multi_instance_S32G274_M7_0” 例程，出现报错如下：&lt;/P&gt;&lt;P&gt;14:35:25 **** Incremental Build of configuration Debug_RAM for project IPCF_Example_multi_instance_S32G274_M7_1 ****&lt;BR /&gt;make -j20 all&lt;BR /&gt;Building file: ../generate/src/OsIf_Cfg.c&lt;BR /&gt;Building file: ../src/main.c&lt;BR /&gt;Building file: ../board/Siul2_Port_Ip_Cfg.c&lt;BR /&gt;Building file: ../src/sample.c&lt;BR /&gt;Building file: ../generate/src/Mpu_M7_Ip_Cfg.c&lt;BR /&gt;Invoking: Standard S32DS C Compiler&lt;BR /&gt;Invoking: Standard S32DS C Compiler&lt;BR /&gt;arm-none-eabi-gcc "@src/main.args" -MMD -MP -MF"src/main.d" -MT"src/main.o" -o "src/main.o" "../src/main.c"&lt;BR /&gt;Invoking: Standard S32DS C Compiler&lt;BR /&gt;Invoking: Standard S32DS C Compiler&lt;BR /&gt;arm-none-eabi-gcc "@src/main.args" -MMD -MP -MF"src/sample.d" -MT"src/sample.o" -o "src/sample.o" "../src/sample.c"&lt;BR /&gt;arm-none-eabi-gcc "@generate/src/Mpu_M7_Ip_Cfg.args" -MMD -MP -MF"generate/src/OsIf_Cfg.d" -MT"generate/src/OsIf_Cfg.o" -o "generate/src/OsIf_Cfg.o" "../generate/src/OsIf_Cfg.c"&lt;BR /&gt;Invoking: Standard S32DS C Compiler&lt;BR /&gt;arm-none-eabi-gcc "@board/Siul2_Port_Ip_Cfg.args" -MMD -MP -MF"board/Siul2_Port_Ip_Cfg.d" -MT"board/Siul2_Port_Ip_Cfg.o" -o "board/Siul2_Port_Ip_Cfg.o" "../board/Siul2_Port_Ip_Cfg.c"&lt;BR /&gt;arm-none-eabi-gcc "@generate/src/Mpu_M7_Ip_Cfg.args" -MMD -MP -MF"generate/src/Mpu_M7_Ip_Cfg.d" -MT"generate/src/Mpu_M7_Ip_Cfg.o" -o "generate/src/Mpu_M7_Ip_Cfg.o" "../generate/src/Mpu_M7_Ip_Cfg.c"&lt;BR /&gt;../src/main.c:20:10: fatal error: Clock_Ip.h: No such file or directory&lt;BR /&gt;20 | #include "Clock_Ip.h"&lt;BR /&gt;| ^~~~~~~~~~~~&lt;BR /&gt;compilation terminated.&lt;BR /&gt;In file included from ../generate/src/Mpu_M7_Ip_Cfg.c:46:&lt;BR /&gt;D:/nxp/workspaceS32DS.3.5/IPCF_Example_multi_instance_S32G274_M7_1/generate/include/Mpu_M7_Ip_Cfg.h:39:10: fatal error: Mpu_M7_Ip_Types.h: No such file or directory&lt;BR /&gt;39 | #include "Mpu_M7_Ip_Types.h"&lt;BR /&gt;| ^~~~~~~~~~~~~~~~~~~&lt;BR /&gt;compilation terminated.&lt;BR /&gt;In file included from ../board/Siul2_Port_Ip_Cfg.c:43:&lt;BR /&gt;../board/Siul2_Port_Ip_Cfg.h:47:10: fatal error: Siul2_Port_Ip_Types.h: No such file or directory&lt;BR /&gt;47 | #include "Siul2_Port_Ip_Types.h"&lt;BR /&gt;| ^~~~~~~~~~~~~~~~~~~~~~~&lt;BR /&gt;compilation terminated.&lt;BR /&gt;../src/sample.c:24:10: fatal error: ipcf_Ip_Cfg.h: No such file or directory&lt;BR /&gt;24 | #include "ipcf_Ip_Cfg.h"&lt;BR /&gt;| ^~~~~~~~~~~~~~~&lt;BR /&gt;In file included from ../generate/src/OsIf_Cfg.c:44:&lt;BR /&gt;D:/nxp/S32DS.3.5/S32DS/software/PlatformSDK_S32XX_2022_03/SW32_RTD_4_4_3_0_2_D2203/Base_TS_T40D11M30I2R0/include/OsIf_Cfg_TypesDef.h:87:6: error: #error "Software Version Numbers of OsIf_Cfg_TypesDef.h and OsIf_Cfg.h are different"&lt;BR /&gt;87 | #error "Software Version Numbers of OsIf_Cfg_TypesDef.h and OsIf_Cfg.h are different"&lt;BR /&gt;| ^~~~~&lt;BR /&gt;compilation terminated.&lt;BR /&gt;../generate/src/OsIf_Cfg.c:93:6: error: #error "Software Version Numbers of OsIf_Cfg.c and OsIf_Cfg_TypesDef.h are different"&lt;BR /&gt;93 | #error "Software Version Numbers of OsIf_Cfg.c and OsIf_Cfg_TypesDef.h are different"&lt;BR /&gt;| ^~~~~&lt;BR /&gt;make: *** [generate/src/subdir.mk:23: generate/src/Mpu_M7_Ip_Cfg.o] Error 1&lt;BR /&gt;make: *** Waiting for unfinished jobs....&lt;BR /&gt;make: *** [src/subdir.mk:23: src/sample.o] Error 1&lt;BR /&gt;make: *** [board/subdir.mk:20: board/Siul2_Port_Ip_Cfg.o] Error 1&lt;BR /&gt;make: *** [src/subdir.mk:23: src/main.o] Error 1&lt;BR /&gt;make: *** [generate/src/subdir.mk:23: generate/src/OsIf_Cfg.o] Error 1&lt;BR /&gt;"make -j20 all" terminated with exit code 2. Build might be incomplete.&lt;/P&gt;&lt;P&gt;14:35:26 Build Failed. 12 errors, 0 warnings. (took 552ms)&lt;/P&gt;&lt;P&gt;打开 Peripherals 配置出现问题显示如下：&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="DRAVE_0-1728542282150.png" style="width: 792px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/303944i36935ABDCE8FF15A/image-dimensions/792x298?v=v2" width="792" height="298" role="button" title="DRAVE_0-1728542282150.png" alt="DRAVE_0-1728542282150.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;已安装软件包如下：&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="DRAVE_2-1728542432284.png" style="width: 769px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/303946iAE23DAB68D58E1F3/image-dimensions/769x178?v=v2" width="769" height="178" role="button" title="DRAVE_2-1728542432284.png" alt="DRAVE_2-1728542432284.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;麻烦可以帮忙看看什么原因不？谢谢！&lt;/P&gt;</description>
      <pubDate>Thu, 10 Oct 2024 06:41:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/An-error-occurs-when-compiling-the-IPCF-Example-multi-instance/m-p/1971039#M11123</guid>
      <dc:creator>DRAVE</dc:creator>
      <dc:date>2024-10-10T06:41:05Z</dc:date>
    </item>
    <item>
      <title>Re: An error occurs when compiling the IPCF_Example_multi_instance_S32G274_M7_0 project</title>
      <link>https://community.nxp.com/t5/S32G/An-error-occurs-when-compiling-the-IPCF-Example-multi-instance/m-p/1971053#M11125</link>
      <description>&lt;P&gt;Hi nxp,&lt;/P&gt;&lt;P&gt;下面三个例程运行都出现一样的现象&lt;/P&gt;&lt;P&gt;IPCF_Example_multi_instance_S32G274_M7_0&lt;/P&gt;&lt;P&gt;IPCF_Example_multi_instance_S32G274_M7_1&lt;/P&gt;&lt;P&gt;IPCF_Example_multi_instance_S32G274_M7_2&lt;/P&gt;</description>
      <pubDate>Thu, 10 Oct 2024 06:48:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/An-error-occurs-when-compiling-the-IPCF-Example-multi-instance/m-p/1971053#M11125</guid>
      <dc:creator>DRAVE</dc:creator>
      <dc:date>2024-10-10T06:48:15Z</dc:date>
    </item>
    <item>
      <title>Re: An error occurs when compiling the IPCF_Example_multi_instance_S32G274_M7_0 project</title>
      <link>https://community.nxp.com/t5/S32G/An-error-occurs-when-compiling-the-IPCF-Example-multi-instance/m-p/1971228#M11129</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211314"&gt;@DRAVE&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;感谢你的提问。&lt;SPAN&gt;在编译项目之前，你似乎没有使用配置工具生成代码。&lt;/SPAN&gt;请点击标记处的绿色按钮”更新源代码“，它会向项目中添加缺失的模块以使其正常工作。我们建议再次导入示例（删除之前的）并使用配置工具生成代码。&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_0-1728551462510.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/303983i5FF7FFB15075442B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Celeste_Liu_0-1728551462510.png" alt="Celeste_Liu_0-1728551462510.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;</description>
      <pubDate>Thu, 10 Oct 2024 09:14:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/An-error-occurs-when-compiling-the-IPCF-Example-multi-instance/m-p/1971228#M11129</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2024-10-10T09:14:52Z</dc:date>
    </item>
    <item>
      <title>Re: An error occurs when compiling the IPCF_Example_multi_instance_S32G274_M7_0 project</title>
      <link>https://community.nxp.com/t5/S32G/An-error-occurs-when-compiling-the-IPCF-Example-multi-instance/m-p/1972006#M11143</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/237877"&gt;@Celeste_Liu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;貌似是我装多一个 RTD 包导致的，我重装软件后就可以了，谢谢！问下，是否有关于&amp;nbsp;S32G-VNP-RDB3 类似&amp;nbsp;AN13750.pdf 的文档？就是能在&amp;nbsp;&amp;nbsp;S32G-VNP-RDB3 上实现 A 核和 M 核同时工作的状态？&lt;/P&gt;</description>
      <pubDate>Fri, 11 Oct 2024 08:34:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/An-error-occurs-when-compiling-the-IPCF-Example-multi-instance/m-p/1972006#M11143</guid>
      <dc:creator>DRAVE</dc:creator>
      <dc:date>2024-10-11T08:34:29Z</dc:date>
    </item>
    <item>
      <title>Re: An error occurs when compiling the IPCF_Example_multi_instance_S32G274_M7_0 project</title>
      <link>https://community.nxp.com/t5/S32G/An-error-occurs-when-compiling-the-IPCF-Example-multi-instance/m-p/1972050#M11145</link>
      <description>&lt;P&gt;Hello&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;很高兴听到你的问题解决了。目前没有关于 S32G3 的双核启动的类似 AN13750.pdf 的文档，并且也没有发布此类文档的计划。这是因为 S32G3 的 GoldVIP 里面已经有双核启动了。我认为 AN13750 对你仍具有一定的参考价值，因为思路是一致的。以下这个案例可能会对你有所帮助：&lt;A href="https://community.nxp.com/t5/S32G/S32G399A-RDB3-Multi-core-boot-failed-following-AN13750/m-p/1753196" target="_self"&gt;Solved: S32G399A-RDB3-Multi-core-boot-failed-following-AN13750&lt;/A&gt;&amp;nbsp;。&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;</description>
      <pubDate>Fri, 01 Nov 2024 07:50:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/An-error-occurs-when-compiling-the-IPCF-Example-multi-instance/m-p/1972050#M11145</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2024-11-01T07:50:45Z</dc:date>
    </item>
    <item>
      <title>Re: An error occurs when compiling the IPCF_Example_multi_instance_S32G274_M7_0 project</title>
      <link>https://community.nxp.com/t5/S32G/An-error-occurs-when-compiling-the-IPCF-Example-multi-instance/m-p/1972444#M11164</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/237877"&gt;@Celeste_Liu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;好的，我参考一下，谢谢！&lt;/P&gt;</description>
      <pubDate>Sat, 12 Oct 2024 01:41:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/An-error-occurs-when-compiling-the-IPCF-Example-multi-instance/m-p/1972444#M11164</guid>
      <dc:creator>DRAVE</dc:creator>
      <dc:date>2024-10-12T01:41:48Z</dc:date>
    </item>
  </channel>
</rss>