<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32G中的主题 Re: pfeng: Version magic is inconsistent</title>
    <link>https://community.nxp.com/t5/S32G/pfeng-Version-magic-is-inconsistent/m-p/1499633#M1089</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The kernel you are using is not part of the S32G standard bsp so please use the standard bsp that is not tested with PREEMP_RT.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Tue, 02 Aug 2022 13:51:13 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2022-08-02T13:51:13Z</dc:date>
    <item>
      <title>pfeng: Version magic is inconsistent</title>
      <link>https://community.nxp.com/t5/S32G/pfeng-Version-magic-is-inconsistent/m-p/1499267#M1087</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;I used menuconig to change PREEMPT_RT to y, i.e &lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;The Preemption Model is Fully Preemptible Kernel (real-time).&lt;/SPAN&gt;&lt;SPAN class=""&gt; After compiling and booting the kernel, the boot log displays:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;[ 1.504617] pfeng: version magic '5.10.90-rt60+g47a49b91d4d4 SMP preempt mod_ unload aarch64' should be '5.10.90-rt60+g47a49b91d4d4 SMP preempt_rt mod_unload aarch64'&lt;BR /&gt;[ 1.756999] sja1110: version magic '5.10.90-rt60+g47a49b91d4d4 SMP preempt mo d_unload aarch64' should be '5.10.90-rt60+g47a49b91d4d4 SMP preempt_rt mod_unloa d aarch64'&lt;BR /&gt;[ 1.757136] sja1110: version magic '5.10.90-rt60+g47a49b91d4d4 SMP preempt mo d_unload aarch64' should be '5.10.90-rt60+g47a49b91d4d4 SMP preempt_rt mod_unloa d aarch64'&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;Symptom NIC PFE2 cannot be identified after the system starts.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;How should I modify to normally identify the network card device PFE?&lt;/P&gt;</description>
      <pubDate>Tue, 02 Aug 2022 06:11:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/pfeng-Version-magic-is-inconsistent/m-p/1499267#M1087</guid>
      <dc:creator>972276616</dc:creator>
      <dc:date>2022-08-02T06:11:16Z</dc:date>
    </item>
    <item>
      <title>Re: pfeng: Version magic is inconsistent</title>
      <link>https://community.nxp.com/t5/S32G/pfeng-Version-magic-is-inconsistent/m-p/1499633#M1089</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The kernel you are using is not part of the S32G standard bsp so please use the standard bsp that is not tested with PREEMP_RT.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 02 Aug 2022 13:51:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32G/pfeng-Version-magic-is-inconsistent/m-p/1499633#M1089</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2022-08-02T13:51:13Z</dc:date>
    </item>
  </channel>
</rss>